Data Fields

IVIDDEC1_Params Struct Reference
[IVIDDEC1 - XDM Video Decoder Interface]

Defines the creation time parameters for all IVIDDEC1 instance objects. More...

#include <ividdec1.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxFrameRate
XDAS_Int32 maxBitRate
XDAS_Int32 dataEndianness
XDAS_Int32 forceChromaFormat

Detailed Description

Defines the creation time parameters for all IVIDDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Maximum video height in pixels.

Maximum video width in pixels.

Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.

Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000

Endianness of output data.

See also:
XDM_DataFormat

Chroma formats.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
See also:
XDM_ChromaFormat

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated