Data Fields

IAUDDEC_Params Struct Reference
[IAUDDEC - XDM Audio Decoder Interface]

Defines the creation time parameters for all IAUDDEC instance objects. More...

#include <iauddec.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 maxSampleRate
XDAS_Int32 maxBitrate
XDAS_Int32 maxNoOfCh
XDAS_Int32 dataEndianness

Detailed Description

Defines the creation time parameters for all IAUDDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Maximum sampling frequency in Hz. For example, if the maximum sampling frequency is 44.1 kHz, this field should be 44100.

Maximum bit rate in bits per second. For example, if the maximum bit rate is 128 kbps, set this field to 128000.

Maximum Channels. See IAUDIO_ChannelId.

Endianness of input data.

See also:
XDM_DataFormat

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated