Data Fields

IVIDENC1_CodecClassConfig Struct Reference
[VIDENC1 - Video Encoder Interface]

Definition of IVIDENC1 codec class configurable parameters. More...

#include <videnc1.h>

Data Fields

Bool manageInBufsCache [16]
Bool manageOutBufsCache [16]

Detailed Description

Definition of IVIDENC1 codec class configurable parameters.

See also:
VISA_getCodecClassConfig()

Field Documentation


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated