Data Fields

IIMGENC_DynamicParams Struct Reference
[IIMGENC - XDM Image Encoder Interface]

This structure defines the algorithm parameters that can be modified after creation via control() calls. More...

#include <iimgenc.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 numAU
XDAS_Int32 inputChromaFormat
XDAS_Int32 inputHeight
XDAS_Int32 inputWidth
XDAS_Int32 captureWidth
XDAS_Int32 generateHeader
XDAS_Int32 qValue

Detailed Description

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of Access unit to encode. Set to XDM_DEFAULT to encode the entire frame.

Input chroma format.

See also:
XDM_ChromaFormat

Input frame height.

Input frame width.

Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.

Header generation mode.

See also:
XDM_EncMode

Quality factor for encoder. Set to a value between 0 (lowest quality) and 100 (highest quality).


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated