Data Fields

IVIDDEC_OutArgs Struct Reference
[IVIDDEC - XDM Video Decoder Interface]

Defines the run time output arguments for all IVIDDEC instance objects. More...

#include <ividdec.h>

Collaboration diagram for IVIDDEC_OutArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDAS_Int32 bytesConsumed
XDAS_Int32 decodedFrameType
XDAS_Int32 outputID
IVIDEO_BufDesc displayBufs

Detailed Description

Defines the run time output arguments for all IVIDDEC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
.

Bytes consumed.

Decoded frame type. See IVIDEO_FrameType.

Output ID. Refer to comment IVIDDEC_InArgs::inputID.

The decoder fills this structure to denote the buffer pointers for current displayable frames. In case of sequences having I & P frames only, these values are identical to outBufs passed in process().


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated