Data Fields

IVIDENC_DynamicParams Struct Reference
[IVIDENC - XDM Video Encoder Interface]

This structure defines the codec parameters that can be modified after creation via control() calls. More...

#include <ividenc.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 inputHeight
XDAS_Int32 inputWidth
XDAS_Int32 refFrameRate
XDAS_Int32 targetFrameRate
XDAS_Int32 targetBitRate
XDAS_Int32 intraFrameInterval
XDAS_Int32 generateHeader
XDAS_Int32 captureWidth
XDAS_Int32 forceIFrame

Detailed Description

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Input frame height.

Input frame width.

Reference or input frame rate * 1000.

Target frame rate * 1000.

Target bit rate in bits per second.

I frame interval. For example, 30.

Encode entire access unit or only header.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
See also:
XDM_EncMode

DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.

Force the current frame to be encoded as an I-frame.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated