Data Fields

ISPHDEC1_InArgs Struct Reference
[ISPHDEC1 - XDM Speech Decoder Interface]

Defines the input arguments for all ISPHDEC1 instance process function. More...

#include <isphdec1.h>

Collaboration diagram for ISPHDEC1_InArgs:
Collaboration graph
[legend]

Data Fields

XDAS_Int16 size
XDAS_Int16 frameType
XDM1_SingleBufDesc data

Detailed Description

Defines the input arguments for all ISPHDEC1 instance process function.


Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Frame type of this buffer.

See also:
ISPHDEC1_FrameType

Raw data output for data transmission.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated