AM273x MCU+ SDK  08.06.00

Introduction

This module contains APIs to program and use the GPADC module.

Files

file  gpadc/v0/gpadc.h
 This file contains the prototypes of the APIs present in the device abstraction layer file of GPADC.
 

Data Structures

struct  GPADC_ChannelConfigType
 GPADC Config Type data structure for the mode, trigger source and channel configuration for all the available external sources <0-8> More...
 
struct  GPADC_ConfigType
 GPADC Config Type data structure for the mode, trigger source and channel configuration for all the available external sources <0-8> More...
 
union  GPADC_ParamInfoType
 Configuration Parameters for GPADC in IFM mode ParamValue : Value to be programmed in one hot reg CollectSamples : Number of samples to collect @625KHz SkipSamples : Number of samples to skip @10MHz Time = Mantissa[3:0] * 2^(Exponent[6:4]) / 10M. More...
 
union  GPADC_channelsGroupSelectType
 Available <0-8> external sources/channels could be selected by using bitmap of 9 bits in LSB. Ex: 0x01F is the bitmap for conversion of <0-4> external sources. More...
 
struct  GPADC_DriverChannelConfigType
 GPADC Driver Channel configuration. More...
 
struct  GPADC_DriverObjectType
 GPADC Driver Object configuration. More...
 
struct  GPADC_EfuseTempTrimType
 The Temperature sensor trim parameters structure. More...
 
struct  GPADC_TempSensTrimType
 The Temperature sensor trim parameters structure. More...
 
struct  GPADC_TempSensMuxType
 Temperature sensors mux values. More...
 
struct  GPADC_TempSensValueType
 The Temperature sensor values structure. More...
 
struct  MSS_GPADC_RST_CTRL_REG
 GPADC Reset Control register. More...
 
struct  MSS_GPADC_CLK_DIV_VAL_REG
 GPADC Clock Divider Value register. More...
 
struct  MSS_GPADC_CLK_GATE_REG
 GPADC Clock Gate register. More...
 
struct  MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_REG
 Analog Mux Control Registers. More...
 
struct  MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_REG
 Analog Refsys spare Registers. More...
 
struct  U_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_REG
 RCM Analog register TW Control Registers. More...
 
struct  GPADCREG_REG0
 Register Offset 0x000. More...
 
struct  GPADCREG_REG1
 Register1 Offset 0x004. More...
 
struct  GPADCREG_REG2
 Register2 Offset 0x008. More...
 
union  U_GPADCREG_REG3
 Register3 Offset 0x00C. More...
 
union  U_GPADCREG_REG4
 Register4 Offset 0x010. More...
 
struct  GPADCREG_REG5
 Register5 Offset 0x014. More...
 
struct  GPADCREG_REG6
 Register6 Offset 0x018. More...
 
struct  GPADCREG_REG7
 Register7 Offset 0x01C. More...
 
struct  GPADCREG_REG8
 Register8 Offset 0x020. More...
 
struct  GPADCREG_REG9
 Register9 Offset 0x024. More...
 
struct  GPADCREG_REG10
 Register10 Offset 0x028. More...
 
struct  GPADCREG_REG11
 Register11 Offset 0x02C. More...
 
struct  GPADCREG_REG12
 Register12 Offset 0x030. More...
 
struct  GPADCREG_REG13
 Register13 Offset 0x034. More...
 
struct  GPADCREG_REG14
 Register14 Offset 0x038. More...
 
struct  GPADCREG_REG15
 Register15 Offset 0x03C. More...
 
struct  GPADCREG_REG16
 Register16 Offset 0x040. More...
 
struct  GPADCREG_REG17
 Register17 Offset 0x044. More...
 
struct  GPADCREG_REG18
 Register19 Offset 0x048. More...
 
struct  GPADCREG_REG19
 Register20 Offset 0x04C. More...
 
struct  GPADCREG_REG20
 Register21 Offset 0x050. More...
 
struct  GPADCREG_REG21
 Register22 Offset 0x054. More...
 
struct  GPADCREG_REG22
 Register22 Offset 0x058. More...
 
struct  T_GPADC_REGS
 MSS_GPADC_REG_REGS. More...
 
struct  MSS_CTRL_MSS_GPADC_MEM_INIT_REG
 GPADC Memory initialize registers. More...
 
struct  GPADC_CfgAndParamValuesType
 Configuration Parameters for GPADC LUT in IFM mode 32 bits: ConfigValue 32 bits: ParamInfo. More...
 
struct  GPADC_ResultType
 GPADC returning min, avg, max and sum. More...
 

Functions

void GPADC_init (void)
 This function initializes the GPADC module. More...
 
void GPADC_deinit (void)
 This function de-initializes the GPADC module. More...
 
int32_t GPADC_open (GPADC_ConfigType *CfgPtr)
 Initializes the GPADC Driver with the channels configuration. More...
 
int32_t GPADC_close (void)
 This function closes the GPADC module. More...
 
GPADC_ConvResultType GPADC_startGroupConversion (GPADC_channelsGroupSelectType channels, uint8_t numChannels)
 Starts and triggers the multi channel ADC conversion. More...
 
GPADC_ConvResultType GPADC_startSingleChannelConversion (GPADC_MeasExtSrcType channelID, uint16_t *gpadcValue)
 Starts and triggers the single channel conversion. Pass the channelID and result address to the driver and the result will be stored in the address passed. More...
 
int32_t GPADC_stopConversion (void)
 Stops the GPADC conversion. More...
 
int32_t GPADC_setupResultBuffer (uint16_t *ResBufferPtr)
 Initializes GPADC driver with the group specific result buffer start address where the conversion results will be stored. More...
 
int32_t GPADC_readResultBuffer (uint16_t *ResBufferPtr)
 The function is used to read the result buffer from the GPADC Driver. More...
 
GPADC_StatusType GPADC_getStatus (void)
 Gets the status of GPADC Driver HW unit. More...
 
int32_t GPADC_readTemperature (uint8_t numAverages, uint8_t numChannels, GPADC_TempSensValueType *tempValuesPtr)
 Read the temperature sensor value. More...
 
void GPADC_initTempMeasurement (void)
 Initialize GPADC efuse temperature parameters. More...
 

Enumerations

enum  GPADC_CtmTrigSrcType {
  GPADC_TRIG_SRC_GPIO_0 = 0, GPADC_TRIG_SRC_GPIO_1, GPADC_TRIG_SRC_GPIO_2, GPADC_TRIG_SRC_GPIO_3,
  GPADC_TRIG_SRC_RSS_CSI2A_EOL_INT, GPADC_TRIG_SRC_RSS_CSI2A_SOF_INT0, GPADC_TRIG_SRC_RSS_CSI2A_SOF_INT1, GPADC_TRIG_SRC_RSS_CSI2A_SOF_INT,
  GPADC_TRIG_SRC_RSS_CSI2B_SOF_INT, GPADC_TRIG_SRC_HW_Sync_FE1, GPADC_TRIG_SRC_HW_Sync_FE2, GPADC_TRIG_SRC_DSS_RTIA_1,
  GPADC_TRIG_SRC_DSS_RTIB_1, GPADC_TRIG_SRC_MSS_RTIA_INT1, GPADC_TRIG_SRC_MSS_RTIB_INT1, GPADC_TRIG_SRC_MMR_Based_SW_Trigger
}
 Enumeration which describes the trigger sources for GPADC CTM mode conversion. More...
 
enum  GPADC_ChannelConvModeType { GPADC_ONESHOT_CONV_MODE = 0, GPADC_CONTINUOUS_CONV_MODE }
 Enumeration which lists the conversion modes supported for AM273x GPADC conversion. More...
 
enum  GPADC_TriggerSourceType { GPADC_TRIGG_SRC_SW = 0, GPADC_TRIGG_SRC_HW }
 Enumeration which describes the trigger sources for GPADC CTM mode conversion. More...
 
enum  GPADC_MeasExtSrcType {
  GPADC_MEAS_EXT_CH1 = 0, GPADC_MEAS_EXT_CH2, GPADC_MEAS_EXT_CH3, GPADC_MEAS_EXT_CH4,
  GPADC_MEAS_EXT_CH5, GPADC_MEAS_EXT_CH6, GPADC_MEAS_EXT_CH7, GPADC_MEAS_EXT_CH8,
  GPADC_MEAS_EXT_CH9, MAX_GPADC_MEAS_SOURCES
}
 Enumeration which describes the external sources available for GPADC conversion. More...
 
enum  GPADC_ConvResultType { GPADC_CONV_ERROR = 0, GPADC_CONV_DONE, GPADC_CONV_CHANNEL_CONFIG_MISSING }
 Enumeration which describes the error types of GPADC conversion. More...
 
enum  GPADC_StatusType { GPADC_IDLE, GPADC_BUSY, GPADC_COMPLETED }
 Current status of the conversion of the requested GPADC HW unit. More...
 
enum  GPADC_TempSensorSrcType { GPADC_DIG_DSP_TEMP_SENSOR = 0, GPADC_DIG_HWA_TEMP_SENSOR, GPADC_DIG_HSM_TEMP_SENSOR, MAX_GPADC_TEMP_SENSORS }
 Enumeration which describes the temperature sensors available for GPADC measurement. More...
 

Macros

#define MAX_CTM_GPADC_PARAMS   (1U)
 Number of measurement parameters for GPADC in CTM mode
More...
 
#define GPADC_TIMEOUT_MAX   (200000U)
 GPADC TIMEOUT Max Number of Sample collect : 256 Max Time for 256 samples collection : 256 * 16/10MHz = 409.6us Add 10 % margin : 450us Add 550us for skip samples Total timeout: 1ms Timout in terms of pmu count = 1ms/5ns = 200,000. More...
 
#define EFUSE_TRIM_TEMPERATURE_CONST   523
 Efuse Trime Constant Temperature. More...
 
#define EFUSE_TRIM_TEMPERATURE_DIV_CONST   10
 Efuse Trime Constant Temperature Divider. More...
 
#define ZERO_PT_TRIM_FIXED_TRIM_TEMP   110
 Zero point TRIM Fixed Temperature. More...
 
#define ZERO_PT_TRIM_FIXED_DIG_TEMP_SENSOR_TRIM_30C   305U
 Zero point TRIM Fixed Digital Temperature. More...
 
#define ZERO   0
 Zero Value. More...
 
#define ZERO_PT_TRIM_FIXED_SLOPE   -1.05
 Zero point TRIM Fixed Slope. More...
 
#define ONE_PT_TRIM_FIXED_SLOPE   -1.05
 One point TRIM Fixed Slope. More...
 
#define EFUSE1_ROW_14_FUSEROM_VER_START_BIT   20U
 Efuse Version Start Bit. More...
 
#define EFUSE1_ROW_14_FUSEROM_VER_STOP_BIT   24U
 Efuse Version Stop Bit. More...
 
#define EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_START_BIT   15U
 Efuse Trim Temperature 30C Start Bit. More...
 
#define EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_STOP_BIT   25U
 Efuse Trim Temperature 30C Stop Bit. More...
 
#define EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_START_BIT   0U
 Efuse Trim Temperature 125C Start Bit. More...
 
#define EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_STOP_BIT   10U
 Efuse Trim Temperature 125C Stop Bit. More...
 
#define EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_START_BIT   5U
 Efuse Digital DSP Temperature 30C Sensor Start Bit. More...
 
#define EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_STOP_BIT   14U
 Efuse Digital DSP Temperature 30C Sensor Stop Bit. More...
 
#define EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_START_BIT   15U
 Efuse Digital HWA Temperature 30C Sensor Start Bit. More...
 
#define EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_STOP_BIT   24U
 Efuse Digital HWA Temperature 30C Sensor Stop Bit. More...
 
#define EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_START_BIT   0U
 Efuse Digital HSM Temperature 30C Sensor Start Bit. More...
 
#define EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_STOP_BIT   9U
 Efuse Digital HSM Temperature 30C Sensor Stop Bit. More...
 
#define EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_START_BIT   5U
 Efuse Digital DSP Temperature 125C Sensor Start Bit. More...
 
#define EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_STOP_BIT   14U
 Efuse Digital DSP Temperature 125C Sensor Stop Bit. More...
 
#define EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_START_BIT   15U
 Efuse Digital HWA Temperature 125C Sensor Start Bit. More...
 
#define EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_STOP_BIT   24U
 Efuse Digital HWA Temperature 125C Sensor Stop Bit. More...
 
#define EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_START_BIT   0U
 Efuse Digital HSM Temperature 125C Sensor Start Bit. More...
 
#define EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_STOP_BIT   9U
 Efuse Digital HSM Temperature 125C Sensor Stop Bit. More...
 
#define GPADC_REGS_PTR   ((T_GPADC_REGS*)CSL_MSS_GPADC_REG_U_BASE)
 GPADC Register Base Address. More...
 
#define GPADCPKTRAM_REGS_PTR   ((T_GPADCPKTRAM_REGS*)CSL_MSS_GPADC_PKT_RAM_U_BASE)
 GPADCPKTRAM Register Base Address. More...
 
#define GPADCOUT_RAM_PTR   ((T_GPADCOUT_RAM*)CSL_MSS_GPADC_DATA_RAM_U_BASE)
 GPADCPKTRAM Data RAM Base Address. More...
 
#define MSS_GPADC_RST_CTRL_ADDR   (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_RST_CTRL)
 GPADC Reset Control Address. More...
 
#define MSS_GPADC_RST_CTRL_PTR   ((MSS_GPADC_RST_CTRL_REG*)MSS_GPADC_RST_CTRL_ADDR)
 GPADC Reset Control Pointer. More...
 
#define MSS_GPADC_CLK_DIV_VAL_ADDR   (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_DIV_VAL)
 GPADC Clock Divider value Address. More...
 
#define MSS_GPADC_CLK_DIV_VAL_PTR   ((MSS_GPADC_CLK_DIV_VAL_REG*)MSS_GPADC_CLK_DIV_VAL_ADDR)
 GPADC Clock Divider value pointer. More...
 
#define MSS_GPADC_CLK_GATE_ADDR   (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_GATE)
 GPADC Clock Gate Address. More...
 
#define MSS_GPADC_CLK_GATE_PTR   ((MSS_GPADC_CLK_GATE_REG*)MSS_GPADC_CLK_GATE_ADDR)
 GPADC Clock Gate Pointer. More...
 
#define MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR   (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV)
 RCM TW Analog TMUX Contol Address. More...
 
#define MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_PTR   ((MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR)
 RCM TW Analog TMUX Contol Poniter. More...
 
#define MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR   (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV)
 RCM Analog Refsys Spare register Address. More...
 
#define MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_PTR   ((MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR)
 RCM Analog Refsys Spare register Pointer. More...
 
#define MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR   (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV)
 RCM Analog TW Control register Address. More...
 
#define MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_PTR   ((U_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR)
 RCM Analog TW Control register pointer. More...
 
#define MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR   (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_MSS_GPADC_MEM_INIT)
 GPADC Memomory Init Address. More...
 
#define MSS_CTRL_MSS_GPADC_MEM_INIT_PTR   ((MSS_CTRL_MSS_GPADC_MEM_INIT_REG*)MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR)
 GPADC Memomory Init poniter. More...
 
#define REG_STRUCT_SWRITE(w_hwRegStruct, w_regVal, w_regWrSts)
 Register Structure member write and compare macro. More...
 
#define REG32_SCOMPARE(w_hwVal, w_swVal, w_regWrSts)
 32 bit register compare macro More...
 
#define REG_STRUCT_SCLEAR(w_hwRegStruct, w_regVal, w_regWrSts)
 Register Structure member CLEAR and compare macro. More...
 

GPADC Macros

#define GPADC_DISABLE   (0U)
 Disable GPADC. More...
 
#define GPADC_ENABLE   (1U)
 Enable GPADC. More...
 
#define GPADC_ASSERT_RESET   (1U)
 Reset GPADC. More...
 
#define GPADC_DEASSERT_RESET   (0U)
 Release GPADC Reset. More...
 
#define GPADC_FSM_ASSERT_RESET   (0x7U)
 Reset GPADC for digital FSM. More...
 
#define GPADC_FSM_DEASSERT_RESET   (0U)
 Release Reset GPADC for digital FSM. More...
 

GPADC Modes

#define GPADC_MODE_DISABLE   (0U)
 GPADC Disable mode. More...
 
#define GPADC_MODE_IFM   (1U)
 GPADC IFM Operation mode. More...
 
#define GPADC_MODE_CTM   (2U)
 GPADC CTM Operation mode. More...
 

Instruction RAM Index

MON CTM INSTRUCTION RAM Index

#define GPADC_MON_INSTR_RAM_ST_IND   (224U)
 GPADC RAM Instruction Index. More...
 
#define GPADC_MAX_MON_INSTR_RAM   (32U)
 GPADC MAX RAM Instruction. More...
 

Macro Definition Documentation

◆ GPADC_DISABLE

#define GPADC_DISABLE   (0U)

Disable GPADC.

◆ GPADC_ENABLE

#define GPADC_ENABLE   (1U)

Enable GPADC.

◆ GPADC_ASSERT_RESET

#define GPADC_ASSERT_RESET   (1U)

Reset GPADC.

◆ GPADC_DEASSERT_RESET

#define GPADC_DEASSERT_RESET   (0U)

Release GPADC Reset.

◆ GPADC_FSM_ASSERT_RESET

#define GPADC_FSM_ASSERT_RESET   (0x7U)

Reset GPADC for digital FSM.

◆ GPADC_FSM_DEASSERT_RESET

#define GPADC_FSM_DEASSERT_RESET   (0U)

Release Reset GPADC for digital FSM.

◆ GPADC_MODE_DISABLE

#define GPADC_MODE_DISABLE   (0U)

GPADC Disable mode.

◆ GPADC_MODE_IFM

#define GPADC_MODE_IFM   (1U)

GPADC IFM Operation mode.

◆ GPADC_MODE_CTM

#define GPADC_MODE_CTM   (2U)

GPADC CTM Operation mode.

◆ GPADC_MON_INSTR_RAM_ST_IND

#define GPADC_MON_INSTR_RAM_ST_IND   (224U)

GPADC RAM Instruction Index.

◆ GPADC_MAX_MON_INSTR_RAM

#define GPADC_MAX_MON_INSTR_RAM   (32U)

GPADC MAX RAM Instruction.

◆ MAX_CTM_GPADC_PARAMS

#define MAX_CTM_GPADC_PARAMS   (1U)

Number of measurement parameters for GPADC in CTM mode

◆ GPADC_TIMEOUT_MAX

#define GPADC_TIMEOUT_MAX   (200000U)

GPADC TIMEOUT Max Number of Sample collect : 256 Max Time for 256 samples collection : 256 * 16/10MHz = 409.6us Add 10 % margin : 450us Add 550us for skip samples Total timeout: 1ms Timout in terms of pmu count = 1ms/5ns = 200,000.

◆ EFUSE_TRIM_TEMPERATURE_CONST

#define EFUSE_TRIM_TEMPERATURE_CONST   523

Efuse Trime Constant Temperature.

◆ EFUSE_TRIM_TEMPERATURE_DIV_CONST

#define EFUSE_TRIM_TEMPERATURE_DIV_CONST   10

Efuse Trime Constant Temperature Divider.

◆ ZERO_PT_TRIM_FIXED_TRIM_TEMP

#define ZERO_PT_TRIM_FIXED_TRIM_TEMP   110

Zero point TRIM Fixed Temperature.

◆ ZERO_PT_TRIM_FIXED_DIG_TEMP_SENSOR_TRIM_30C

#define ZERO_PT_TRIM_FIXED_DIG_TEMP_SENSOR_TRIM_30C   305U

Zero point TRIM Fixed Digital Temperature.

◆ ZERO

#define ZERO   0

Zero Value.

◆ ZERO_PT_TRIM_FIXED_SLOPE

#define ZERO_PT_TRIM_FIXED_SLOPE   -1.05

Zero point TRIM Fixed Slope.

◆ ONE_PT_TRIM_FIXED_SLOPE

#define ONE_PT_TRIM_FIXED_SLOPE   -1.05

One point TRIM Fixed Slope.

◆ EFUSE1_ROW_14_FUSEROM_VER_START_BIT

#define EFUSE1_ROW_14_FUSEROM_VER_START_BIT   20U

Efuse Version Start Bit.

◆ EFUSE1_ROW_14_FUSEROM_VER_STOP_BIT

#define EFUSE1_ROW_14_FUSEROM_VER_STOP_BIT   24U

Efuse Version Stop Bit.

◆ EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_START_BIT

#define EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_START_BIT   15U

Efuse Trim Temperature 30C Start Bit.

◆ EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_STOP_BIT

#define EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_STOP_BIT   25U

Efuse Trim Temperature 30C Stop Bit.

◆ EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_START_BIT

#define EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_START_BIT   0U

Efuse Trim Temperature 125C Start Bit.

◆ EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_STOP_BIT

#define EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_STOP_BIT   10U

Efuse Trim Temperature 125C Stop Bit.

◆ EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_START_BIT

#define EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_START_BIT   5U

Efuse Digital DSP Temperature 30C Sensor Start Bit.

◆ EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_STOP_BIT

#define EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_STOP_BIT   14U

Efuse Digital DSP Temperature 30C Sensor Stop Bit.

◆ EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_START_BIT

#define EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_START_BIT   15U

Efuse Digital HWA Temperature 30C Sensor Start Bit.

◆ EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_STOP_BIT

#define EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_STOP_BIT   24U

Efuse Digital HWA Temperature 30C Sensor Stop Bit.

◆ EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_START_BIT

#define EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_START_BIT   0U

Efuse Digital HSM Temperature 30C Sensor Start Bit.

◆ EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_STOP_BIT

#define EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_STOP_BIT   9U

Efuse Digital HSM Temperature 30C Sensor Stop Bit.

◆ EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_START_BIT

#define EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_START_BIT   5U

Efuse Digital DSP Temperature 125C Sensor Start Bit.

◆ EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_STOP_BIT

#define EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_STOP_BIT   14U

Efuse Digital DSP Temperature 125C Sensor Stop Bit.

◆ EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_START_BIT

#define EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_START_BIT   15U

Efuse Digital HWA Temperature 125C Sensor Start Bit.

◆ EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_STOP_BIT

#define EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_STOP_BIT   24U

Efuse Digital HWA Temperature 125C Sensor Stop Bit.

◆ EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_START_BIT

#define EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_START_BIT   0U

Efuse Digital HSM Temperature 125C Sensor Start Bit.

◆ EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_STOP_BIT

#define EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_STOP_BIT   9U

Efuse Digital HSM Temperature 125C Sensor Stop Bit.

◆ GPADC_REGS_PTR

#define GPADC_REGS_PTR   ((T_GPADC_REGS*)CSL_MSS_GPADC_REG_U_BASE)

GPADC Register Base Address.

◆ GPADCPKTRAM_REGS_PTR

#define GPADCPKTRAM_REGS_PTR   ((T_GPADCPKTRAM_REGS*)CSL_MSS_GPADC_PKT_RAM_U_BASE)

GPADCPKTRAM Register Base Address.

◆ GPADCOUT_RAM_PTR

#define GPADCOUT_RAM_PTR   ((T_GPADCOUT_RAM*)CSL_MSS_GPADC_DATA_RAM_U_BASE)

GPADCPKTRAM Data RAM Base Address.

◆ MSS_GPADC_RST_CTRL_ADDR

#define MSS_GPADC_RST_CTRL_ADDR   (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_RST_CTRL)

GPADC Reset Control Address.

◆ MSS_GPADC_RST_CTRL_PTR

#define MSS_GPADC_RST_CTRL_PTR   ((MSS_GPADC_RST_CTRL_REG*)MSS_GPADC_RST_CTRL_ADDR)

GPADC Reset Control Pointer.

◆ MSS_GPADC_CLK_DIV_VAL_ADDR

#define MSS_GPADC_CLK_DIV_VAL_ADDR   (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_DIV_VAL)

GPADC Clock Divider value Address.

◆ MSS_GPADC_CLK_DIV_VAL_PTR

#define MSS_GPADC_CLK_DIV_VAL_PTR   ((MSS_GPADC_CLK_DIV_VAL_REG*)MSS_GPADC_CLK_DIV_VAL_ADDR)

GPADC Clock Divider value pointer.

◆ MSS_GPADC_CLK_GATE_ADDR

#define MSS_GPADC_CLK_GATE_ADDR   (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_GATE)

GPADC Clock Gate Address.

◆ MSS_GPADC_CLK_GATE_PTR

#define MSS_GPADC_CLK_GATE_PTR   ((MSS_GPADC_CLK_GATE_REG*)MSS_GPADC_CLK_GATE_ADDR)

GPADC Clock Gate Pointer.

◆ MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR

#define MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR   (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV)

RCM TW Analog TMUX Contol Address.

◆ MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_PTR

#define MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_PTR   ((MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR)

RCM TW Analog TMUX Contol Poniter.

◆ MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR

#define MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR   (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV)

RCM Analog Refsys Spare register Address.

◆ MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_PTR

#define MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_PTR   ((MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR)

RCM Analog Refsys Spare register Pointer.

◆ MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR

#define MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR   (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV)

RCM Analog TW Control register Address.

◆ MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_PTR

#define MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_PTR   ((U_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR)

RCM Analog TW Control register pointer.

◆ MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR

#define MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR   (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_MSS_GPADC_MEM_INIT)

GPADC Memomory Init Address.

◆ MSS_CTRL_MSS_GPADC_MEM_INIT_PTR

#define MSS_CTRL_MSS_GPADC_MEM_INIT_PTR   ((MSS_CTRL_MSS_GPADC_MEM_INIT_REG*)MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR)

GPADC Memomory Init poniter.

◆ REG_STRUCT_SWRITE

#define REG_STRUCT_SWRITE (   w_hwRegStruct,
  w_regVal,
  w_regWrSts 
)
Value:
do { (w_hwRegStruct) = (w_regVal); \
REG32_SCOMPARE((w_hwRegStruct), (w_regVal), (w_regWrSts)); \
} while (0)

Register Structure member write and compare macro.

◆ REG32_SCOMPARE

#define REG32_SCOMPARE (   w_hwVal,
  w_swVal,
  w_regWrSts 
)
Value:
do { \
(w_regWrSts) |= (((uint32_t)(w_swVal)) ^ ((uint32_t)(w_hwVal))); \
} while (0)

32 bit register compare macro

◆ REG_STRUCT_SCLEAR

#define REG_STRUCT_SCLEAR (   w_hwRegStruct,
  w_regVal,
  w_regWrSts 
)
Value:
do { (w_hwRegStruct) = (w_regVal); \
(w_regWrSts) |= ((((uint32_t)(w_hwRegStruct)) & (uint32_t)(w_regVal))); \
} while (0)

Register Structure member CLEAR and compare macro.

Enumeration Type Documentation

◆ GPADC_CtmTrigSrcType

Enumeration which describes the trigger sources for GPADC CTM mode conversion.

Note: Only GPADC_TRIGG_SRC_SW is supported in the AM273x GPADC Driver. GPADC_TRIG_SRC_MMR_Based_SW_Trigger will be default trigger if CTM mode is configured

Enumerator
GPADC_TRIG_SRC_GPIO_0 

0x00 - GPIO_0

GPADC_TRIG_SRC_GPIO_1 

0x01 - GPIO_1

GPADC_TRIG_SRC_GPIO_2 

0x02 - GPIO_2

GPADC_TRIG_SRC_GPIO_3 

0x03 - GPIO_3

GPADC_TRIG_SRC_RSS_CSI2A_EOL_INT 

0x04 - RSS_CSI2A_EOL_INT

GPADC_TRIG_SRC_RSS_CSI2A_SOF_INT0 

0x05 - RSS_CSI2A_SOF_INT0

GPADC_TRIG_SRC_RSS_CSI2A_SOF_INT1 

0x06 - RSS_CSI2A_SOF_INT1

GPADC_TRIG_SRC_RSS_CSI2A_SOF_INT 

0x07 - RSS_CSI2A_SOF_INT

GPADC_TRIG_SRC_RSS_CSI2B_SOF_INT 

0x08 - RSS_CSI2B_SOF_INT

GPADC_TRIG_SRC_HW_Sync_FE1 

0x09 - HW_Sync_FE1

GPADC_TRIG_SRC_HW_Sync_FE2 

0x0A - HW_Sync_FE2

GPADC_TRIG_SRC_DSS_RTIA_1 

0x0B - DSS_RTIA_1

GPADC_TRIG_SRC_DSS_RTIB_1 

0x0C - DSS_RTIB_1

GPADC_TRIG_SRC_MSS_RTIA_INT1 

0x0D - MSS_RTIA_INT1

GPADC_TRIG_SRC_MSS_RTIB_INT1 

0x0E - MSS_RTIB_INT1

GPADC_TRIG_SRC_MMR_Based_SW_Trigger 

0x0F - MMR_Based_SW_Trigger

◆ GPADC_ChannelConvModeType

Enumeration which lists the conversion modes supported for AM273x GPADC conversion.

Note: Only GPADC_ONESHOT_CONV_MODE is supported in the AM273x GPADC Driver.

Enumerator
GPADC_ONESHOT_CONV_MODE 

0x00 - IFM - Inter Frame Monitoring/One Shot Conversion Mode

GPADC_CONTINUOUS_CONV_MODE 

0x01 - CTM - Continuous Time Monitoring/ Continuous conversion Mode

◆ GPADC_TriggerSourceType

Enumeration which describes the trigger sources for GPADC CTM mode conversion.

Note: Only GPADC_TRIGG_SRC_SW is supported in the AM273x GPADC Driver.

Enumerator
GPADC_TRIGG_SRC_SW 

Conversion is triggered by a software API call.

GPADC_TRIGG_SRC_HW 

Conversion is triggered by a hardware event.

◆ GPADC_MeasExtSrcType

Enumeration which describes the external sources available for GPADC conversion.

Enumerator
GPADC_MEAS_EXT_CH1 

0x0 - Channel 1

GPADC_MEAS_EXT_CH2 

0x1 - Channel 2

GPADC_MEAS_EXT_CH3 

0x2 - Channel 3

GPADC_MEAS_EXT_CH4 

0x3 - Channel 4

GPADC_MEAS_EXT_CH5 

0x4 - Channel 5

GPADC_MEAS_EXT_CH6 

0x5 - Channel 6

GPADC_MEAS_EXT_CH7 

0x6 - Channel 7

GPADC_MEAS_EXT_CH8 

0x7 - Channel 8

GPADC_MEAS_EXT_CH9 

0x8 - Channel 9

MAX_GPADC_MEAS_SOURCES 

0x9 - MAX_CHANNELS

◆ GPADC_ConvResultType

Enumeration which describes the error types of GPADC conversion.

Enumerator
GPADC_CONV_ERROR 

GPADC conversion error.

GPADC_CONV_DONE 

GPADC conversion done.

GPADC_CONV_CHANNEL_CONFIG_MISSING 

GPADC requested channel through the channel bitmap or index is not configured during the initialization.

◆ GPADC_StatusType

Current status of the conversion of the requested GPADC HW unit.

Enumerator
GPADC_IDLE 

The conversion of the specified group has not been started. No result is available.

GPADC_BUSY 

The conversion of the specified group has been started and is still going on. So far no result is available.

GPADC_COMPLETED 

A conversion round of the specified group has been finished. A result is available for all specified channels of the group.

◆ GPADC_TempSensorSrcType

Enumeration which describes the temperature sensors available for GPADC measurement.

Enumerator
GPADC_DIG_DSP_TEMP_SENSOR 

0x0 - DIG_DSP_TEMP_SENSOR

GPADC_DIG_HWA_TEMP_SENSOR 

0x1 - DIG_HWA_TEMP_SENSOR

GPADC_DIG_HSM_TEMP_SENSOR 

0x2 - DIG_HSM_TEMP_SENSOR

MAX_GPADC_TEMP_SENSORS 

0x3 - MAX_TEMP_SENSORS

Function Documentation

◆ GPADC_init()

void GPADC_init ( void  )

This function initializes the GPADC module.

◆ GPADC_deinit()

void GPADC_deinit ( void  )

This function de-initializes the GPADC module.

◆ GPADC_open()

int32_t GPADC_open ( GPADC_ConfigType CfgPtr)

Initializes the GPADC Driver with the channels configuration.

Parameters
[in]CfgPtrPointer to the GPADC configuration

◆ GPADC_close()

int32_t GPADC_close ( void  )

This function closes the GPADC module.

◆ GPADC_startGroupConversion()

GPADC_ConvResultType GPADC_startGroupConversion ( GPADC_channelsGroupSelectType  channels,
uint8_t  numChannels 
)

Starts and triggers the multi channel ADC conversion.

        Pass the channel selection bitmap for group conversion to the GPADC Driver and
        check the result buffer passed to the driver using GPADC_SetupResultBuffer()
        for conversion results of all configured channels.

        Conversion happens based on the parameters provided through GPADC_Init()
        for GPADC HW unit and each channel config like sampling parameters, buffered/ unbuffered.

        GPADC_Init() should be done before starting conversion
        Channel bitmap selected shouldn't be zero
        Result buffer should be setup before starting conversion using GPADC_SetupResultBuffer().
Parameters
[in]channelsChannel selection bitmap to start conversion together
[in]numChannels
number of channels
Returns
GPADC_CONV_ERROR: GPADC Conversion Error GPADC_CONV_DONE: GPADC Conversion Successfully Done GPADC_CONV_CHANNEL_CONFIG_MISSING: One or more of the bitmap selected channel group is missing configuration during initialization

◆ GPADC_startSingleChannelConversion()

GPADC_ConvResultType GPADC_startSingleChannelConversion ( GPADC_MeasExtSrcType  channelID,
uint16_t *  gpadcValue 
)

Starts and triggers the single channel conversion. Pass the channelID and result address to the driver and the result will be stored in the address passed.

Parameters
[in]channelIDChannel index from <0-8> available external sources
[out]gpadcValuePointer to the address where the result shall be stored.
Returns
GPADC_CONV_ERROR: GPADC Conversion Error GPADC_CONV_DONE: GPADC Conversion Successfully Done GPADC_CONV_CHANNEL_CONFIG_MISSING: The specified channel channel is not configured using GPADC_Init()

◆ GPADC_stopConversion()

int32_t GPADC_stopConversion ( void  )

Stops the GPADC conversion.

        This API should not be called before initialization.\n
        This API should not be called before starting group/single channel start conversion\n
        To be used when the mode of conversion is chosen as GPADC_CONTINUOUS_CONV_MODE.

return If stop conversion is successful returns SystemP_SUCCESS, else error on failure

◆ GPADC_setupResultBuffer()

int32_t GPADC_setupResultBuffer ( uint16_t *  ResBufferPtr)

Initializes GPADC driver with the group specific result buffer start address where the conversion results will be stored.

The application has to ensure that the application buffer, where ResBufferPtr points to, can hold all the conversion results of the specified group. The initialization with GPADC_SetupResultBuffer is required after GPADC_Init(), before a group conversion can be started.

Parameters
[in]ResBufferPtr
Returns
If Result Buffer Setup is successful returns SystemP_SUCCESS, else error on failure

◆ GPADC_readResultBuffer()

int32_t GPADC_readResultBuffer ( uint16_t *  ResBufferPtr)

The function is used to read the result buffer from the GPADC Driver.

        Reads the group conversion result of the last completed conversion round
        of the requested group and stores the channel values starting at the
        ResBufferPtr address.
Parameters
[out]ResBufferPtr
Returns
On Read Result Buffer is successful returns SystemP_SUCCESS , else error on failure

◆ GPADC_getStatus()

GPADC_StatusType GPADC_getStatus ( void  )

Gets the status of GPADC Driver HW unit.

Returns
GPADC_IDLE: The conversion of the specified group has not been started. No result is available. GPADC_BUSY: The conversion of the specified group has been started and is still going on. So far no result is available. GPADC_COMPLETED: A conversion round of the specified group has been finished. A result is available for all specified channels of the group.

◆ GPADC_readTemperature()

int32_t GPADC_readTemperature ( uint8_t  numAverages,
uint8_t  numChannels,
GPADC_TempSensValueType tempValuesPtr 
)

Read the temperature sensor value.

Parameters
[in]numAveragesnumber of average samples
[in]numChannelsnumber of channels
[out]tempValuesPtrPointer to store the temperature values
Returns
If temperature read is successful returns SystemP_SUCCESS, else error on failure

◆ GPADC_initTempMeasurement()

void GPADC_initTempMeasurement ( void  )

Initialize GPADC efuse temperature parameters.