GPADC Driver Object configuration.
The structure holds the channel confiiguration structure,operation mode structure
Data Fields | |
GPADC_ChannelConvModeType | convMode |
Operation mode of the group. More... | |
GPADC_TriggerSourceType | triggSrc |
Trigger Source Type. More... | |
GPADC_StatusType | driverStatus |
Driver Status. More... | |
GPADC_DriverChannelConfigType | driverChannelConfig [MAX_GPADC_MEAS_SOURCES] |
Channel configurations. More... | |
uint16_t * | ResultBufferPtr |
Pointer to store conversion results. More... | |
GPADC_ChannelConvModeType GPADC_DriverObjectType::convMode |
Operation mode of the group.
GPADC_TriggerSourceType GPADC_DriverObjectType::triggSrc |
Trigger Source Type.
GPADC_StatusType GPADC_DriverObjectType::driverStatus |
Driver Status.
GPADC_DriverChannelConfigType GPADC_DriverObjectType::driverChannelConfig[MAX_GPADC_MEAS_SOURCES] |
Channel configurations.
uint16_t* GPADC_DriverObjectType::ResultBufferPtr |
Pointer to store conversion results.