|
static void | RDC_setAdcSocWidth (uint32_t base, uint8_t socWidth) |
| sets the Start of Conversion Width for the ADC conversion More...
|
|
static void | RDC_setAdcBurstCount (uint32_t base, uint8_t burstCount) |
| sets the ADC Burst count, samples to be averaged. More...
|
|
static void | RDC_enableAdcSingleEndedMode (uint32_t base) |
| Enable Single Ended Mode of operation. More...
|
|
static void | RDC_disableAdcSingleEndedMode (uint32_t base) |
| Disable Single Ended Mode of operation. More...
|
|
static uint32_t | RDC_getAdcSequencerOperationalMode (uint32_t base) |
| returns Sequencer Operational Mode Valid values are RDC_SEQUENCER_MODE_0 - ADC0 SAMPLES SIN AND ADC1 SAMPLES COSINE PARALLELLY FOR CORE 0 RDC_SEQUENCER_MODE_1 - ADC0 SAMPLES SIN AND COSINE SEQUENTIALLY FOR CORE 0 RDC_SEQUENCER_MODE_2 - ADC0 SAMPLES SIN0, COS0, COS1, SIN1 SEQUENTIALLY, TO BE AVERAGED FOR CORE 0 RDC_SEQUENCER_MODE_3 - ADC0 SAMPLES SIN AND ADC1 SAMPLES COS PARALLELLY FOR CORE 0 FOLLOWED BY ADC0 SAMPLES SIN AND ADC1 SAMPLES COS PARALLELLY FOR CORE 1 RDC_SEQUENCER_MODE_4 - ADC0 SAMPLES SIN FOR CORE 0 AND ADC1 SAMPLES SIN FOR CORE 1 PARALLELLY FOLLOWED BY ADC0 SAMPLES COS FOR CORE 0 AND ADC1 SAMPLES COS FOR CORE 2 RDC_SEQUENCER_MODE_5 - ADC0/1 PARALLELLY SAMPLE SIN0, COS0, COS1, SIN1 SAMPLES SEQUENTIALLY FOR CORE0/1. BOTH SIN(COS) SAMPLES FOR EACH CORE WILL BE AVERAGED. More...
|
|
static void | RDC_setAdcSequencerOperationalMode (uint32_t base, uint8_t operationalMode) |
| sets Sequencer Operational Mode Valid values are RDC_SEQUENCER_MODE_0 - ADC0 SAMPLES SIN AND ADC1 SAMPLES COSINE PARALLELLY FOR CORE 0 RDC_SEQUENCER_MODE_1 - ADC0 SAMPLES SIN AND COSINE SEQUENTIALLY FOR CORE 0 RDC_SEQUENCER_MODE_2 - ADC0 SAMPLES SIN0, COS0, COS1, SIN1 SEQUENTIALLY, TO BE AVERAGED FOR CORE 0 RDC_SEQUENCER_MODE_3 - ADC0 SAMPLES SIN AND ADC1 SAMPLES COS PARALLELLY FOR CORE 0 FOLLOWED BY ADC0 SAMPLES SIN AND ADC1 SAMPLES COS PARALLELLY FOR CORE 1 RDC_SEQUENCER_MODE_4 - ADC0 SAMPLES SIN FOR CORE 0 AND ADC1 SAMPLES SIN FOR CORE 1 PARALLELLY FOLLOWED BY ADC0 SAMPLES COS FOR CORE 0 AND ADC1 SAMPLES COS FOR CORE 2 RDC_SEQUENCER_MODE_5 - ADC0/1 PARALLELLY SAMPLE SIN0, COS0, COS1, SIN1 SAMPLES SEQUENTIALLY FOR CORE0/1. BOTH SIN(COS) SAMPLES FOR EACH CORE WILL BE AVERAGED. More...
|
|
static void | RDC_enableResolver (uint32_t base) |
| Enables the Resolver Operation. More...
|
|
static void | RDC_disableResolver (uint32_t base) |
| Disables the Resolver Operation. More...
|
|
static void | RDC_setExcitationSignalPhase (uint32_t base, uint16_t phase) |
| Sets the Phase value for the Excitation Signal. Phase values in the range [RDC_EXCITATION_FREQUENCY_MIN_PHASE, RDC_EXCITATION_FREQUENCY_MAX_PHASE] can be mapped to 0-360 deg. More...
|
|
static uint32_t | RDC_getExcitationSignalPhase (uint32_t base) |
| Returns the Phase Value programmed for Excitation signal. More...
|
|
static void | RDC_setExcitationSignalFrequencySelect (uint32_t base, uint8_t FrequencySel) |
| Sets the Excitation frequency value from the selected values. More...
|
|
static uint32_t | RDC_getExcitationSignalFrequencySelect (uint32_t base) |
| Returns the selected Excitation Signal Frequency select. More...
|
|
static uint32_t | RDC_getAdcSampleRate (uint32_t base) |
| Gets the ADC Sampling Ratio. More...
|
|
static void | RDC_enableExcitationSignalSyncIn (uint32_t base) |
| Enables the Excitation Signal Sync In. More...
|
|
static void | RDC_disableExcitationSignalSyncIn (uint32_t base) |
| Disables the Excitation Signal Sync In. More...
|
|
static uint32_t | RDC_getExcitationSignalEventStatus (uint32_t base) |
| returns if there is a sync in event after the RDC_enableResolver() has been called once this returns non-zero, RDC_clearExcitationSignalEventStatus(), RDC_disableResolver(), RDC_enableResolver() needs to be called to rearm. More...
|
|
static void | RDC_clearExcitationSignalEventStatus (uint32_t base) |
| Clears SyncIn event status. More...
|
|
static uint32_t | RDC_getExcitationSignalPhaseInfo (uint32_t base) |
| Returns the latched value of the last pwm_sync_in rise event of the pwm phase. this is updated on every pwm_sync_in event. More...
|
|
static void | RDC_setExcitationSignalSocDelay (uint32_t base, uint16_t socDelay) |
| Sets the SOC Delay from the PWM Exciation Signal. More...
|
|
static void | RDC_setExcitationSignalAmplitudeControl (uint32_t base, uint8_t amplitude) |
| set the Amplitude control for the excitation signal More...
|
|
static uint32_t | RDC_getExcitationSignalAmplitudeControl (uint32_t base) |
| returns the Amplitude control for the excitation signal More...
|
|
static void | RDC_enableSequencerInterrupt (uint32_t base) |
| Enable Sequencer Error Interrupt. More...
|
|
static void | RDC_disableSequencerInterrupt (uint32_t base) |
| Disable Sequencer Error Interrupt. More...
|
|
static void | RDC_clearSequencerInterrupt (uint32_t base) |
| Clear the Sequencer Error Interrupt status. More...
|
|
static void | RDC_forceSequencerInterrupt (uint32_t base) |
| Force the Sequencer Error Interrupt. More...
|
|
static uint32_t | RDC_getSequencerInterruptStatus (uint32_t base) |
| Returns Sequencer interrupt Status. More...
|
|
static void | RDC_enableCoreInterrupt (uint32_t base, uint32_t ResolverCore, uint32_t interruptSource) |
| enable Core Interrupt More...
|
|
static uint32_t | RDC_getCoreEnabledInterruptSources (uint32_t base, uint8_t ResolverCore) |
| returns enabled Interrupt Sources More...
|
|
static void | RDC_disableCoreInterrupt (uint32_t base, uint32_t ResolverCore, uint32_t interruptSource) |
| Disable Core Interrupt. More...
|
|
static void | RDC_clearCoreInterrupt (uint32_t base, uint32_t ResolverCore, uint32_t interruptSource) |
| Clear the Core Interrupt status. More...
|
|
static void | RDC_forceCoreInterrupt (uint32_t base, uint32_t ResolverCore, uint32_t interruptSource) |
| Force the Core Interrupt. More...
|
|
static uint32_t | RDC_getCoreInterruptStatus (uint32_t base, uint32_t ResolverCore) |
| Returns Core interrupt Status. More...
|
|
static bool | RDC_getCalibrationStatus (uint32_t base) |
| Returns the Calibration Status. More...
|
|
static void | RDC_clearCalibrationStatus (uint32_t base) |
| Clears Calibration Status for re-enabling Calibration Sequence. More...
|
|
static void | RDC_selectCalibrationChannel (uint32_t base, uint8_t calChannel) |
| Selects Calibration Channel for Cal sequence. More...
|
|
static void | RDC_enableCalibration (uint32_t base) |
| Enables ADC Calibration. More...
|
|
static uint32_t | RDC_getCalibrationData (uint32_t base, uint8_t CalAdc) |
| Returns the CAL ADC data for given ADC, if the mode permits. More...
|
|
static void | RDC_setDcOffsetCalCoef (uint32_t base, uint8_t core, uint8_t coef1, uint8_t coef2) |
| Sets the DC Offset Coefficients coef1, coef2. More...
|
|
static void | RDC_enableBPF (uint32_t base, uint8_t core) |
| enables Band Pass Filter before DC Offset logic. More...
|
|
static void | RDC_disableBPF (uint32_t base, uint8_t core) |
| Disables Band Pass Filter Logic before DC Offset logic. More...
|
|
static void | RDC_disableDcOffsetAutoCorrection (uint32_t base, uint8_t core) |
| Disbales Auto Offset correction from the estimated values Enables DC Offset Manual Correction logic. More...
|
|
static void | RDC_enableDcOffsetAutoCorrection (uint32_t base, uint8_t core) |
| Enables Auto DC Offset Correction from the estimated values Disables DC Offset Manual Correction logic and enabled the Auto correction logic. More...
|
|
static void | RDC_setDcOffsetManualCorrectionValue (uint32_t base, uint8_t core, int16_t sin, int16_t cos) |
| Sets the Sin, Cosine Manual Correction values for the Dc Offset block in the given resolver core. More...
|
|
static int16_t | RDC_getDcOffsetEstimatedValues (uint32_t base, uint8_t core, uint8_t sinCosValue) |
| returns DC OFFSET estimation values More...
|
|
static void | RDC_overrideIdealSampleTime (uint32_t base, uint8_t core, uint8_t overrideValue) |
| sets the Override value for the Ideal Sample Time selection. More...
|
|
static uint8_t | RDC_getIdealSampleTime (uint32_t base, uint8_t core) |
| Returns the Ideal Sample Time esitimated by the resolver core. More...
|
|
static void | RDC_setIdealSampleDetectionThreshold (uint32_t base, uint8_t core, uint16_t absThresholdValue) |
| sets Ideal Sample Detetction Threshold. validates the sample for the Ideal Sample time detection computation More...
|
|
static void | RDC_setIdealSampleBpfAdjust (uint32_t base, uint8_t core, uint8_t sampleAdjustCount) |
| the BPF sample adjust when the BPF is turned on. This configuration takes effect only on the auto mode, and doesn't take effect on the manual mode More...
|
|
static bool | RDC_getIdealSamplePeakAvgLimitStatus (uint32_t base, uint8_t core) |
| Gets the status if the Peak Averaging Limit is reached. More...
|
|
static void | RDC_setIdealSampleMode (uint32_t base, uint8_t core, uint8_t mode) |
| Ideal Sample Time Computation Mode selection. More...
|
|
static void | RDC_enableIdealSampleBottomSampling (uint32_t base, uint8_t core) |
| Enables bottom Sampling. twice the sampling rate than disabled. the track2 loop runs twice the speed so, the velocity output needs to be converted to respective rotations per second accordingly. More...
|
|
static void | RDC_disableIdealSampleBottomSampling (uint32_t base, uint8_t core) |
| Disables Bottom Sampling. More...
|
|
static bool | RDC_getPhaseGainEstimationStatus (uint32_t base, uint8_t core) |
| Gets status if the Phase Gain Estimation is complete. More...
|
|
static void | RDC_setPhaseGainEstimationTrainLimit (uint32_t base, uint8_t core, uint8_t pgEstimationLimit) |
| Sets the Phase Gain Estimation train limit. if the programmed value is x, 2^x rotations are considered for the train limit. More...
|
|
static void | RDC_setCosPhaseBypass (uint32_t base, uint8_t core, uint16_t cosPhaseBypass) |
| sets the Cos Phase Manual Bypass Value More...
|
|
static void | RDC_enablePhaseGainEstimation (uint32_t base, uint8_t core) |
| Enables Phase Gain Estimation in the background. More...
|
|
static void | RDC_disablePhaseGainEstimation (uint32_t base, uint8_t core) |
| Disbales Phase Gain Estimation in the background. More...
|
|
static void | RDC_enablePhaseAutoCorrection (uint32_t base, uint8_t core) |
| Enables Phase Auto Correction. More...
|
|
static void | RDC_disablePhaseAutoCorrection (uint32_t base, uint8_t core) |
| Disables Phase Auto Correction. More...
|
|
static void | RDC_enableGainAutoCorrection (uint32_t base, uint8_t core) |
| Enable Gain Auto correction. More...
|
|
static void | RDC_disableGainAutoCorrection (uint32_t base, uint8_t core) |
| Disable Gain Auto Correction. More...
|
|
static void | RDC_setGainBypassValue (uint32_t base, uint8_t core, int16_t sinGainBypass, int16_t cosGainBypass) |
| Sets the Manual Gain Correction values for Sin and Cos. More...
|
|
static int16_t | RDC_getPhaseEstimation (uint32_t base, uint8_t core) |
| returns the Cos Phase Offset Estimation this can be used only if the RDC_getPhaseGainEstimationStatus() returns true More...
|
|
static void | RDC_getGainEstimation (uint32_t base, uint8_t core, int16_t *sinGainEstimate, int16_t *cosGainEstimate) |
| returns the Gain estimates for sin and cosine gain values More...
|
|
static void | RDC_setTrack2Constants (uint32_t base, uint8_t core, Track2Constants_t *track2Constants) |
| sets up the Track2 loop constants the following are the constants that can be setup using this API More...
|
|
static void | RDC_enableTrack2Boost (uint32_t base, uint8_t core) |
| enables the track2 Boost More...
|
|
static void | RDC_disableTrack2Boost (uint32_t base, uint8_t core) |
| disables the track2 Boost More...
|
|
static int16_t | RDC_getArcTanAngle (uint32_t base, uint8_t core) |
| Returns signed 16bit angle data from ArcTan. the data corresponds to -180 to +180 degrees angle in degrees : ((16b signed int)) * 360 / 2^16. More...
|
|
static int16_t | RDC_getTrack2Angle (uint32_t base, uint8_t core) |
| Returns Signed 16 bit angle data from Track2 Loop. the data corresponds to -180 to 180 degrees angle in degrees : ((16b signed int)) * 360 / 2^16. More...
|
|
static int32_t | RDC_getTrack2Velocity (uint32_t base, uint8_t core) |
| Returns Signed 32 bit Velocity data from Track2 Loop. More...
|
|
static void | RDC_getDiagnosticsSinCosOffsetDriftData (uint32_t base, uint8_t resolverCore, Diag_Mon_SinCos_Offset_drift_data *monitorData) |
| Returns the Monitor Sin or Cos Offset Drift (DOS) diagnostics data int16_t offset_drift_threshold_hi - the configured offset drift threshold hi value int16_t offset_drift_threshold_lo - the configured offset drift threshold lo value bool offset_drift_cos_hi - the status of the flag in the Interrupt status bool offset_drift_cos_lo - the status of the flag in the Interrupt status bool offset_drift_sin_hi - the status of the flag in the Interrupt status bool offset_drift_sin_lo - the status of the flag in the Interrupt status bool offset_drift_en - if the interrupt is enabled for any of the error status. More...
|
|
static void | RDC_setDiagnosticsSinCosOffsetDriftData (uint32_t base, uint8_t resolverCore, Diag_Mon_SinCos_Offset_drift_data *monitorData) |
| Sets the Monitor Sin or Cos Offset Drift (DOS) diagnostics controls int16_t offset_drift_threshold_hi - the offset drift threshold hi value to be configured int16_t offset_drift_threshold_lo - the offset drift threshold lo value to be configured bool offset_drift_cos_hi - enables interrupt on this flag if set and offset_drift_en is set bool offset_drift_cos_lo - enables interrupt on this flag if set and offset_drift_en is set bool offset_drift_sin_hi - enables interrupt on this flag if set and offset_drift_en is set bool offset_drift_sin_lo - enables interrupt on this flag if set and offset_drift_en is set bool offset_drift_en - enables interrupt on the errors. More...
|
|
static void | RDC_getDiagnosticsSinCosGainDriftData (uint32_t base, uint8_t resolverCore, Diag_Mon_SinCos_Gain_drift_data *monitorData) |
| Returns the Monitor Sin or Cos Gain drift (DOS) diagnostics data int16_t gain_drift_threshold_hi - the configured gain drift threshold hi value int16_t gain_drift_threshold_lo - the configured gain drift threshold lo value uint8_t gain_drift_glitch_count - the configured gain drift glitch count value bool gain_drift_cos_hi - the status of the flag in the Interrupt status bool gain_drift_cos_lo - the status of the flag in the Interrupt status bool gain_drift_sin_hi - the status of the flag in the Interrupt status bool gain_drift_sin_lo - the status of the flag in the Interrupt status bool gain_drift_en - if the interrupt is enabled for any of the error status. More...
|
|
static void | RDC_setDiagnosticsSinCosGainDriftData (uint32_t base, uint8_t resolverCore, Diag_Mon_SinCos_Gain_drift_data *monitorData) |
| Sets the Monitor Sin or Cos Gain drift (DOS) diagnostics Controls int16_t gain_drift_threshold_hi - the gain drift threshold hi value to be configured int16_t gain_drift_threshold_lo - the gain drift threshold lo value to be configured uint8_t gain_drift_glitch_count - the gain drift glitch count value to be configured bool gain_drift_cos_hi - enables interrupt on this flag if set and gain_drift_en is set bool gain_drift_cos_lo - enables interrupt on this flag if set and gain_drift_en is set bool gain_drift_sin_hi - enables interrupt on this flag if set and gain_drift_en is set bool gain_drift_sin_lo - enables interrupt on this flag if set and gain_drift_en is set bool gain_drift_en - enables interrupt on the errors. More...
|
|
static void | RDC_getDiagnosticsCosPhaseDriftData (uint32_t base, uint8_t resolverCore, Diag_Mon_Cos_Phase_drift_data *monitorData) |
| Returns the Monitor Cos Phase drift (DOS) diagnostics data int16_t phase_drift_threshold_hi - the configured phase drift threshold hi value int16_t phase_drift_threshold_lo - the configured phase drift threshold lo value uint8_t phase_drift_glitch_count - the configured phase drift glitch count value bool phase_drift_cos_hi - the status of the flag in the Interrupt status bool phase_drift_cos_lo - the status of the flag in the Interrupt status bool phase_drift_en - if the interrupt is enabled for any of the error status. More...
|
|
static void | RDC_setDiagnosticsCosPhaseDriftData (uint32_t base, uint8_t resolverCore, Diag_Mon_Cos_Phase_drift_data *monitorData) |
| Sets the Monitor Cos Phase drift (DOS) diagnostics Controls int16_t phase_drift_threshold_hi - the phase drift threshold hi value to be configured int16_t phase_drift_threshold_lo - the phase drift threshold lo value to be configured uint8_t phase_drift_glitch_count - the phase drift glitch count value to be configured bool phase_drift_cos_hi - enables interrupt on this flag if set and phase_drift_en is set bool phase_drift_cos_lo - enables interrupt on this flag if set and phase_drift_en is set bool phase_drift_en - enables interrupt on the errors. More...
|
|
static void | RDC_getDiagnosticsExcFreqDegradationData (uint32_t base, uint8_t resolverCore, Diag_Mon_ExcFreq_Degradataion_data *monitorData) |
| Returns the Monitor excitation frequency degradation or loss (DOS) diagnostics data uint16_t excfreqdetected_sin - the counts detected between ZCS for sin excitation frequency uint16_t excfreqdetected_cos - the counts detected between ZCS for cos excitation frequency uint16_t excfreqdrift_threshold_hi - the configured excfreqdrift threshold hi value uint16_t excfreqdrift_threshold_lo - the configured excfreqdrift threshold lo value uint16_t excfreq_level - the configured threshold on ADC to detect sin or cos zero crossings uint8_t excfreqdrift_glitchcount - the configured excfreqdrift glitch count value bool excfreqdrift_hi - the status of the flag in the Interrupt status bool excfreqdrift_cos_lo - the status of the flag in the Interrupt status bool excfreqdrift_sin_lo - the status of the flag in the Interrupt status bool excfreqdrift_en - if the interrupt is enabled for any of the error status. More...
|
|
static void | RDC_setDiagnosticsExcFreqDegradationData (uint32_t base, uint8_t resolverCore, Diag_Mon_ExcFreq_Degradataion_data *monitorData) |
| Sets the Monitor excitation frequency degradation or loss (DOS) diagnostics Controls uint16_t excfreqdetected_sin - no action uint16_t excfreqdetected_cos - no action uint16_t excfreqdrift_threshold_hi - the excfreqdrift threshold hi value to be configured uint16_t excfreqdrift_threshold_lo - the excfreqdrift threshold lo value to be configured uint16_t excfreq_level - the threshold on ADC to detect sin or cos zero crossings to be configured uint8_t excfreqdrift_glitchcount - the excfreqdrift glitch count value to be configured bool excfreqdrift_hi - enables interrupt on this flag if set and excfreqdrift_en is set bool excfreqdrift_cos_lo - enables interrupt on this flag if set and excfreqdrift_en is set bool excfreqdrift_sin_lo - enables interrupt on this flag if set and excfreqdrift_en is set bool excfreqdrift_en - enables interrupt on the errors. More...
|
|
static void | RDC_getDiagnosticsRotationalSignalIntegrityData (uint32_t base, uint8_t resolverCore, Diag_Mon_Rotational_Signal_Integrity_data *monitorData) |
| Returns the Monitor rotational signal integrity (DOS) diagnostics data bool cos_neg_zc_peak_mismatch_err - the status of the flag in the Interrupt status bool cos_pos_zc_peak_mismatch_err - the status of the flag in the Interrupt status bool sin_neg_zc_peak_mismatch_err - the status of the flag in the Interrupt status bool sin_pos_zc_peak_mismatch_err - the status of the flag in the Interrupt status bool sin_multi_zc_error_err - the status of the flag in the Interrupt status bool cos_multi_zc_error_err - the status of the flag in the Interrupt status uint8_t cos_multi_zc_error_count - status of cos capture number of faulty ZCS uint8_t sin_multi_zc_error_count - status of sin capture number of faulty ZCS uint16_t rotpeak_level - the configured "peak level" of rotational Sin/Cos when other signal is zero crossing uint16_t rotfreq_level - the configured "zero crossing detection level" of rotational sin/cos bool zero_cross_rot_en - if the interrupt is enabled for any of the error status. More...
|
|
static void | RDC_setDiagnosticsRotationalSignalIntegrityData (uint32_t base, uint8_t resolverCore, Diag_Mon_Rotational_Signal_Integrity_data *monitorData) |
| Sets the Monitor rotational signal integrity (DOS) diagnostics Controls bool cos_neg_zc_peak_mismatch_err - enables interrupt on this flag if set and zero_cross_rot_en is set bool cos_pos_zc_peak_mismatch_err - enables interrupt on this flag if set and zero_cross_rot_en is set bool sin_neg_zc_peak_mismatch_err - enables interrupt on this flag if set and zero_cross_rot_en is set bool sin_pos_zc_peak_mismatch_err - enables interrupt on this flag if set and zero_cross_rot_en is set bool sin_multi_zc_error_err - enables interrupt on this flag if set and zero_cross_rot_en is set bool cos_multi_zc_error_err - enables interrupt on this flag if set and zero_cross_rot_en is set uint8_t cos_multi_zc_error_count - no action uint8_t sin_multi_zc_error_count - no action uint16_t rotpeak_level - the "peak level" of rotational Sin/Cos when other signal is zero crossing to be configured uint16_t rotfreq_level - the "zero crossing detection level" of rotational sin/cos to be configured bool zero_cross_rot_en - enables interrupt on the errors. More...
|
|
static void | RDC_getDiagnosticsSignalIntegritySquareSumData (uint32_t base, uint32_t resolverCore, Diag_Mon_Signal_Integrity_SinSq_CosSq *monitorData) |
| Returns the Monitor signal integrity by checking Sin2+Cos2=Constant (DOS) diagnostics data uint16_t sinsqcossq_threshold_hi - the configured threshold hi for sinsq + cossq uint16_t sinsqcossq_threshold_lo - the configured threshold lo for sinsq + cossq uint8_t sinsqcossq_glitchcount - the configured glitchcount for sinsq + cossq error uint16_t sinsqcossq_cossq - actual cossq value on error trigger either lo of hi, first event uint16_t sinsqcossq_sinsq - actual sinsq value on error trigger either lo of hi, first event bool sinsqcossq_hi - the status of the flag in the Interrupt status bool sinsqcossq_lo - the status of the flag in the Interrupt status. More...
|
|
static void | RDC_setDiagnosticsSignalIntegritySquareSumData (uint32_t base, uint32_t resolverCore, Diag_Mon_Signal_Integrity_SinSq_CosSq *monitorData) |
| Sets the Monitor signal integrity by checking Sin2+Cos2=Constant (DOS) diagnostics Controls uint16_t sinsqcossq_threshold_hi - the threshold hi for sinsq + cossq to be configured uint16_t sinsqcossq_threshold_lo - the threshold lo for sinsq + cossq to be configured uint8_t sinsqcossq_glitchcount - the glitchcount for sinsq + cossq error to be configured uint16_t sinsqcossq_cossq - no action uint16_t sinsqcossq_sinsq - no action bool sinsqcossq_hi - enable interrupt on this error if set bool sinsqcossq_lo - enable interrupt on this error if set. More...
|
|
static void | RDC_getDiagnosticsHighAmplitudeData (uint32_t base, uint8_t resolverCore, Diag_Mon_Sin_Cos_High_Amplitude *monitorData) |
| Returns the Monitor Sin or Cos saturation or very high amplitude (DOS) diagnostics data uint16_t highAmplitude_threshold - the configured threshold for highAmplitude error uint8_t highAmplitude_glitchcount - the configured glitch count for highAmplitude error int16_t highAmplitude_sin_value - value of sin channel at the error trigger instant int16_t highAmplitude_cos_value - value of cos channel at the error trigger instant bool highAmplitude_sin_error - status of the error flag in the interrupt register bool highAmplitude_cos_error - status of the error flag in the interrupt register. More...
|
|
static void | RDC_setDiagnosticsHighAmplitudeData (uint32_t base, uint8_t resolverCore, Diag_Mon_Sin_Cos_High_Amplitude *monitorData) |
| Sets the Monitor Sin or Cos saturation or very high amplitude (DOS) diagnostics Controls uint16_t highAmplitude_threshold - the threshold for highAmplitude error to be configured uint8_t highAmplitude_glitchcount - the glitch count for highAmplitude error to be configured int16_t highAmplitude_sin_value - no action int16_t highAmplitude_cos_value - no action bool highAmplitude_sin_error - enabled interrupt on this error if set bool highAmplitude_cos_error - enabled interrupt on this error if set. More...
|
|
static void | RDC_getDiagnosticsWeakAmplitudeData (uint32_t base, uint8_t resolverCore, Diag_Mon_Sin_Cos_Weak_Amplitude *monitorData) |
| Returns the Monitor weak Sin or Cos signal below a threshold (LOS) diagnostics data uint16_t lowAmplitude_threshold - the configured threshold for the lowAmplitude error uint8_t lowAmplitude_glitchcount - the configured glitch count for the lowAmplitude error bool lowAmplitude_error - status of the error flag in the interrupt register int16_t lowAmplitude_sin_value - value of sin channel at the trigger instant int16_t lowAmplitude_cos_value - value of cos channel at the trigger instant. More...
|
|
static void | RDC_setDiagnosticsWeakAmplitudeData (uint32_t base, uint8_t resolverCore, Diag_Mon_Sin_Cos_Weak_Amplitude *monitorData) |
| Sets the Monitor weak Sin or Cos signal below a threshold (LOS) diagnostics Controls uint16_t lowAmplitude_threshold - the threshold for the lowAmplitude error to be configured uint8_t lowAmplitude_glitchcount - the glitch count for the lowAmplitude error to be configured bool lowAmplitude_error - enabled interrupt on the error if set int16_t lowAmplitude_sin_value - no action int16_t lowAmplitude_cos_value - no action. More...
|
|
static void | RDC_getAdcObservationalData (uint32_t base, uint8_t resolverCore, ADC_observationalData *AdcData) |
| Returns the Observational ADC data to struct type ADC_observationalData int16_t cos_adc - SW Observational ADC data post latch and Averaged if enabled int16_t sin_adc - SW Observational ADC data post latch and Averaged if enabled int16_t cos_rec - SW Observational ADC data post recovered int16_t sin_rec - SW Observational ADC data post recovered int16_t cos_dc - SW Observational ADC data post DC offset Correction int16_t sin_dc - SW Observational ADC data post DC offset Correction int16_t cos_pgc - SW Observational ADC data post Phase Gain Correction int16_t sin_pgc - SW Observational ADC data post Phase Gain Correction. More...
|
|
static void | RDC_getPeakHistogramObservationalData (uint32_t base, uint8_t resolverCore, PeakHistogram_observationalData *histogram) |
| Returns the Peak Histogram Bucket data. More...
|
|
void | RDC_coreParamsInit (Core_config_t *coreParams) |
| Inits the Core Parameters for the resolver core. More...
|
|
void | RDC_paramsInit (RDC_configParams *params) |
| Inits the resolver Configuration parameters. More...
|
|
void | RDC_init (uint32_t base, RDC_configParams *params) |
| Configures the RDC based on the parameter values. More...
|
|
void | RDC_BaselineParametersInit (uint32_t base) |
| Inits Baseline Parameter configurations. More...
|
|