Structure to hold the control/status data for Diagnostics mentioned under Monitor rotational signal integrity (DOS)
Values that can be passed to RDC_getDiagnosticsRotationalSignalIntegrityData(), RDC_setDiagnosticsRotationalSignalIntegrityData() as Diag_Mon_Rotational_Signal_Integrity_data parameter
◆ cos_neg_zc_peak_mismatch_err
bool Diag_Mon_Rotational_Signal_Integrity_data::cos_neg_zc_peak_mismatch_err |
◆ cos_pos_zc_peak_mismatch_err
bool Diag_Mon_Rotational_Signal_Integrity_data::cos_pos_zc_peak_mismatch_err |
◆ sin_neg_zc_peak_mismatch_err
bool Diag_Mon_Rotational_Signal_Integrity_data::sin_neg_zc_peak_mismatch_err |
◆ sin_pos_zc_peak_mismatch_err
bool Diag_Mon_Rotational_Signal_Integrity_data::sin_pos_zc_peak_mismatch_err |
◆ sin_multi_zc_error_err
bool Diag_Mon_Rotational_Signal_Integrity_data::sin_multi_zc_error_err |
◆ cos_multi_zc_error_err
bool Diag_Mon_Rotational_Signal_Integrity_data::cos_multi_zc_error_err |
◆ cos_multi_zc_error_count
uint8_t Diag_Mon_Rotational_Signal_Integrity_data::cos_multi_zc_error_count |
◆ sin_multi_zc_error_count
uint8_t Diag_Mon_Rotational_Signal_Integrity_data::sin_multi_zc_error_count |
◆ rotpeak_level
uint16_t Diag_Mon_Rotational_Signal_Integrity_data::rotpeak_level |
◆ rotfreq_level
uint16_t Diag_Mon_Rotational_Signal_Integrity_data::rotfreq_level |
◆ zero_cross_rot_en
bool Diag_Mon_Rotational_Signal_Integrity_data::zero_cross_rot_en |