Structure to hold the control/status data for Diagnostics mentioned under Monitor weak Sin or Cos signal below a threshold (LOS)
Values that can be passed to RDC_getDiagnosticsWeakAmplitudeData(), RDC_setDiagnosticsWeakAmplitudeData() as Diag_Mon_Sin_Cos_Weak_Amplitude parameter
◆ lowAmplitude_threshold
uint16_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_threshold |
◆ lowAmplitude_glitchcount
uint8_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_glitchcount |
◆ lowAmplitude_error
bool Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_error |
◆ lowAmplitude_sin_value
int16_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_sin_value |
◆ lowAmplitude_cos_value
int16_t Diag_Mon_Sin_Cos_Weak_Amplitude::lowAmplitude_cos_value |