7.9.8.95. OnFileLoaded()¶
GEL callback function called after a program is loaded.
Syntax
OnFileLoaded( int nErrorCode, int bSymbolsOnly );
Parameters
nErrorCode: 0 (zero) indicates success.
bSymbolsOnlyBoolean indicates if only symbols were loaded.
Description
If defined in a loaded GEL file, OnFileLoaded() is called after a program is loaded.
Example
OnFileLoaded(int nErrorCode, int bSymbolsOnly)
{
if (nErrorCode)
GEL_TextOut(“An error occurred while loading a file. -%d-n”,,,,,
ErrorCode);
else
GEL_TextOut(“File was loaded successfully. -%d-n”,,,,, nErrorCode);
if (bSymbolsOnly)
GEL_TextOut(“Only symbols were loaded.n”);
else
GEL_TextOut(“Full load.n”);
}