7.9.8.83. GEL_SyncStepIntoΒΆ

Performs a StepInto operation on every target that is in the same group as the current target.

Format

GEL_SyncStepInto([iterations**]);**

Parameters

iterations(optional) specifies the number of times the command is to be repeated. If iterations is not specified, executes a single assembly instruction.

Description

Performs a StepInto operation on every target that is in the same group as the current target. The operation performed is the same as the Lock Step option selected from the PDM debug menu. The step operation is context sensitive. If stepping through source and source symbolic information is available, a source step-into will be performed. If source symbolic information is not available, an assembly step into will be performed.

As with the other synchronous operations, the operation is performed on all targets simultaneously.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_SyncStepInto(10);

GEL_SyncStepInto( );

Related Topics

GEL_SyncStepOver

GEL_SyncStepOut

GEL_SyncRun

GEL_SyncHalt