7.9.8.10. GEL_CancelTimerΒΆ

Cancels a previously set GEL timer.

Format

GEL_CancelTimer(timer_id);

Parameters

timer_id specifies the same timer_id that was used to set the timer.

Description

Cancels a timer that was previously set with GEL_SetTimer. The timer_id specified in the second parameter of GEL_SetTimer uniquely identifies the timer, and that same value used in this function cancels that specific timer.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_CancelTimer(1);

Related Topics

GEL_SetTimer