7.9.8.79. GEL_SymbolRemove()

Removes symbol information.

Syntax

GEL_SymbolRemove( “fileName” [, “cpuName” [, “boardName”]] );

Parameters

fileNamenames the symbol file containing the symbol information. The fileName must be enclosed in quotation marks. The symbol file can be a standard COFF output file (*.out) or a specific symbol file obtained during the build process.

cpuName(optional) names the CPU from which to remove the symbolic information (useful in a multiprocessor environment). The cpuName must be enclosed in quotation marks.

boardName(optional) names the board from which to remove the symbolic information. If not specified, uses the board name of the processor on which this GEL function is executed. The boardName must be enclosed in quotation marks.

Description

This function removes the loaded symbols that are defined in the specified symbol file.

If the file is not in the current directory, provide a full path name within the string. A double backslash escape sequence is required to ensure that you get a backslash into the fileName entry.

The cpuName and boardName must match the Processor Name and Board Name as configured in the multiprocessor setup. In a single processor system, you do not need to fill these fields.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_SymbolRemove(“c:\mydir\myfile.out”, “cpu_a”, “Emulator”);

Related Topics

GEL_Load()

GEL_SymbolAdd()

GEL_SymbolAddRel()

GEL_SymbolLoad()

GEL_SymbolLoadRel()

GEL_SymbolAddRel()

GEL_SymbolShowSection()

GEL_UnloadAllSymbols()