7.9.8.70. GEL_SrcStepOver()¶
Step over source code.
Syntax
GEL_SrcStepOver()
Parameters
count(optional) specifies the number of times the command is to be repeated. If no count is specified, executes a single assembly instruction.
Description
Execute the next available instruction in C or assembly source without following function calls then halt. If an action brings you into an area with no source code, the debugger continues stepping until source code (somewhere) is reached. Repeats count times.
The source file can be viewed entirely in C or displayed at the same time as the assembly instructions. In C source mode, this command steps over an entire C instruction. Otherwise, it steps over a single assembly instruction. However, to protect the processor’s pipeline, several instructions following a delayed branch or call may be considered part of the same statement. In this case, the command may execute more than one instruction at a time.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Related Topics