7.9.8.23. GEL_HWBreakPtAdd()¶
Adds a hardware breakpoint.
Syntax
GEL_HWBreakPtAdd(address [,count]);
Parameters
address is the location of the breakpoint. If the address is a string Parameters, a symbolic breakpoint will be set at that location and re-evaluated whenever symbols change. Otherwise, a breakpoint will be set at the specified address.
count(optional) is the number of times to execute before breakpoint is triggered. The default value is 1.
Description
This function adds a new, enabled type 1 hardware breakpoint at the specified address, if the target supports it.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_HWBreakPtAdd( 0x2000 );
GEL_HWBreakPtAdd( PC + 100 );
GEL_HWBreakPtAdd( “main” );
GEL_HWBreakPtAdd( 0x2000, 5 );
Related Topics