7.9.8.62. GEL_Run()

Runs code.

Syntax

GEL_Run( [“Condition”] );

Parameters

Condition: (optional) specifies the condition that must be satisfied while the target is executing. Once the execution reaches a breakpoint and the condition is evaluated to be false, the Code Composer Studio debugger stops at that address. The condition must be enclosed in quotation marks.

Description

This function starts executing code on the target. If a condition is specified, the run function becomes a conditional run statement. That is, execution continues while the statement is true. The statement is evaluated at each breakpoint that is encountered.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_Run();
GEL_Run(“A != B”);

Related Topics

GEL_Restart

GEL_Go

GEL_Halt

GEL_RunF