7.9.8.84. GEL_SyncStepIntoΒΆ
Performs a StepInto operation on every target that is in the same group as the current target.
Format
GEL_SyncStepInto([iterations**]);**
Parameters
iterations(optional) specifies the number of times the command is to be repeated. If iterations is not specified, executes a single assembly instruction.
Description
Performs a StepInto operation on every target that is in the same group as the current target. The operation performed is the same as the Lock Step option selected from the PDM debug menu. The step operation is context sensitive. If stepping through source and source symbolic information is available, a source step-into will be performed. If source symbolic information is not available, an assembly step into will be performed.
As with the other synchronous operations, the operation is performed on all targets simultaneously.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_SyncStepInto(10);
GEL_SyncStepInto( );
Related Topics