7.9.8.30. GEL_IsInRealtimeModeΒΆ
Called every time a target is connected. GEL built-in function that can be called at any time to determine if the target is in realtime mode.
Syntax
GEL_IsInRealtimeMode()
Parameters
None
Description
The function returns 0 is the DSP is currently in Stop mode and 1 if it is in Real Time Mode. Some targets cannot enter Real Time mode; for those cases, the function will always return 0. (See real-time mode)
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
OnTargetConnect()
{ if( GEL_IsInRealtimeMode() )
{
// The target was connected in realtime mode
}
else
{
//The target was connected in stop mode
}
Related Topics