7.9.8.38. GEL_MapOn()ΒΆ
Enables memory mapping.
Syntax
GEL_MapOn()
Parameters
None.
Description
This function enables memory mapping. The Code Composer Studio debugger does not attempt to read from a map segment that is not readable or attempt to write to a map segment that is not writeable. When mapping is first turned on, the entire memory range is assumed to have no reading or writing capabilities. You must add memory sections (using the GEL_MapAdd() function) to allow the debugger to access valid sections. On power up, memory mapping is turned off by default.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_MapOn();
Related Topics