7.9.8.66. GEL_SetSemihostingMainArgs¶
Set the arguments that must be forwarded to the target program’s main function in response to a SYS_GET_CMDLINE semihosting call.
GEL_SetSemihostingMainArgs(args);
Parameters
args - String of arguments to be passed
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_SetSemihostingMainArgs(“arg1 arg2 arg3 arg4 arg5”) will pass an array of size 5 containing [arg1,arg2,arg3,arg4,arg5]
GEL_SetSemihostingMainArgs(“arg1 "arg2 with space” arg3 arg4”) will pass an array of size 4 containing [arg1, arg2 with space, arg3, arg4]
Related Topics
This function should be called to set the desired behaviour prior to calling GEL_Load to start a program load