7.9.8.40. GEL_MemoryFill()ΒΆ
Fills a block of memory.
Syntax
GEL_MemoryFill(startAddress, page, length, pattern [, patternSizeType])
Parameters
startAddressis the first address in the block.
page identifies the type of memory to fill: 0 (Program memory), 1 (Data memory) or 2 (I/0 space).
For processors that do not have more than one type of memory, use 0 for this Parameters. For simulated targets, the I/O space Parameters is not supported.
length defines the number of words to fill.
pattern is the value that is placed in each word in the block.
patternSizeType (optional) specifies the size of pattern that CCStudio should interpret. If not provided, pattern size will be interpreted as being the word size on the memory page on which the GEL_MemoryFill operation is taking place. Acceptable values for patternSizeType are as follows:
Target specific types: size of the type depends on the target used
0x00 - Char
0x01 - Unsigned Char
0x02 - Short
0x03 - Unsigned Short
0x04 - Enum
0x06 - Int
0x07 - Unsigned Int
0x08 - Long
0x09 - Unsigned Long
0x0B - Pointer
Target independent signed types
0x0C - 8 bit integer
0x0E - 16 bit integer
0x10 - 24 bit integer
0x12 - 32 bit integer
0x14 - 40 bit integer
0x16 - 48 bit integer
0x18 - 64 bit integer
Target independent unsigned types
0x0D - 8 bit unsigned integer
0x0F - 16 bit unsigned integer
0x11 - 24 bit unsigned integer
0x13 - 32 bit unsigned integer
0x15 - 40 bit unsigned integer
0x17 - 48 bit unsigned integer
0x19 - 64 bit unsigned integer
Large and floating point types
0x1E - long long
0x1F - unsigned long long
0x20 - float
0x22 - 32 bit IEEE single precision float
0x24 - double
0x26 - 64 bit IEEE double precision float
0x28 - long double
Description
This function can be used to fill a block of target memory with a specified pattern.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
// Fill memory 0x1000 on page 0 with 0x1000 instances of 0xa5a5 where 0xa5a5 is interpreted by CCS as a 32-bit unsigned integer.
GEL_MemoryFill(0x1000, 0, 0x100, 0xa5a5, 0x13);
Related Topics