7.9.8.20. GEL_EvalOnTarget()¶
Evaluate a GEL expression on a target
Syntax
GEL_EvalOnTarget( target_path_name, expression, synchronous = true );
Parameters
target_path_name is the path name of the target on which the expression will be evaluated
expression is the expression to be evaluated
synchronous, if true, GEL_EvalOnTarget won’t return until expression has completed. If false, it will start the evaluation and return immediatel
Description
The GEL_EvalOnTarget function evaluates the expression on the target whose path name is target_path_name. If synchronous, it returns the result of the underlying expression. Otherwise zero is returned