7.9.8.51. GEL_PortDisconnect()ΒΆ
For simulator only, disconnects a data file from a memory (port) address.
Syntax
GEL_PinDisconnect(portAddress, page, length, accessType);
Parameters
portAddressspecifies the starting address of a range in memory. This Parameters can be an absolute address, any C expression, the name of a C function, or an assembly language label. If you want to specify a hex address, be sure to prefix the address number with 0x; otherwise, Code Composer Studio treats the number as a decimal address.
pageidentifies the type of memory: 0 (Program memory), 1 (Data memory) or 2 (I/O space)
For processors that do not have more than one type of memory, use 0 for this Parameters.
lengthdefines the length of the range. This Parameters can be any C expression.
accessTypespecifies the type of access allowed. The access type can be any combination of the following values:
Access Type #define GTI_ATTR_PORT_READ #define GTI_ATTR_PORT_NOREWIND #define GTI_ATTR_PORT_UPDATE #define GTI_ATTR_PORT_EXTERN |
Value 0x01 0x02 0x04 0x08 0x10 |
Description
The simulator allows you to read or write data by connecting a data file to a memory (port) address. This function disconnects the currently connected data file from the specified memory address.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_PortDisconnect(0x1000, 0, 0x100,);
Related Topics
Connecting a File to a Memory Address