7.9.8.64. GEL_RunF()ΒΆ
Runs free.
Syntax
GEL_RunF();
Parameters
None.
Description
This function disables breakpoints before it starts executing code on the target. It also disconnects from the target system. This is useful if you need to perform a hardware reset on your target system or if you need to disconnect the JTAG or MPSD cable. The Code Composer Studio debugger reconnects to the target system and enables breakpoints if any access is requested on the target system (e.g., memory read), or if the user halts the processor.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_RunF();
Related Topics