6.13. CDD DMA Module Migration

Migration Approach: Follow sequential migration for clear understanding of changes at each version. Each migration is organized by individual changes with description, old vs new comparison, and migration actions.

6.13.1. v01.01.00 (i.e release v26.00.01) from v01.00.00 (i.e release v26.00.00) Migration

6.13.1.1. Summary

Version v01.01.00 introduces the following changes to the CDD DMA module:

  1. Cdd_Dma_SetTransferSize parameter type widening: BurstSize widened from uint8 to uint16 and TransferSize from uint16 to uint32, also widening the corresponding fields in Cdd_Dma_TransferSizeType

  2. Wrap size parameter type widening: SrcWrapSize and DestWrapSize widened from uint16 to uint32 in Cdd_Dma_SetTransferWrapSrcProperties, Cdd_Dma_SetTransferWrapDestProperties, and the corresponding Cdd_Dma_TransferSrcWrapType / Cdd_Dma_TransferDestWrapType struct fields

6.13.1.2. Change 1: Cdd_Dma_SetTransferSize parameter type widening

6.13.1.2.1. Description

The BurstSize parameter of Cdd_Dma_SetTransferSize has been widened from uint8 to uint16, and TransferSize from uint16 to uint32. The same widening applies to the corresponding fields BurstSize and TransferSize in Cdd_Dma_TransferSizeType, which is embedded in Cdd_Dma_TransferParamsType.

The driver subtracts 1 from each API value before writing to the hardware register. With the old uint8 type for BurstSize, the maximum user input was 255, causing the hardware to receive 254 — leaving the hardware maximum register value of 255 unreachable. The new uint16 type allows the user to input 256, which the driver writes as 255 to the hardware. The same logic applies to TransferSize: widening from uint16 to uint32 allows input 65536, which the driver writes as 65535.

All values previously valid under uint8/uint16 continue to produce identical runtime behavior. The struct layout of Cdd_Dma_TransferSizeType and Cdd_Dma_TransferParamsType is larger due to the wider fields, requiring regeneration of the plugin-generated files.

6.13.1.2.2. Old vs New

Symbol

v01.00.00

v01.01.00

Cdd_Dma_SetTransferSize — BurstSize parameter type

uint8

uint16

Cdd_Dma_SetTransferSize — TransferSize parameter type

uint16

uint32

Cdd_Dma_TransferSizeType.BurstSize field type

uint8

uint16

Cdd_Dma_TransferSizeType.TransferSize field type

uint16

uint32

Note

Existing calls that pass values within the old type range (BurstSize ≤ 255, TransferSize ≤ 65535) continue to compile and behave identically. No runtime change occurs for those values.

6.13.1.2.3. Migration Actions

  1. Update application variable types: In application code that calls Cdd_Dma_SetTransferSize directly, update any uint8 variables holding BurstSize to uint16, and any uint16 variables holding TransferSize to uint32, to match the new parameter types.

  2. Update Cdd_Dma_TransferSizeType initializers: If application code directly initializes a Cdd_Dma_TransferSizeType struct, update uint8 literals or variables assigned to BurstSize to use uint16, and uint16 literals or variables assigned to TransferSize to use uint32.

  3. Regenerate plugin output: Open EB Tresos and regenerate Cdd_Dma_Cfg.c and Cdd_Dma_Cfg.h using the updated plugin to reflect the new struct layout.

  4. Rebuild the project: Recompile all translation units that include Cdd_Dma.h or Cdd_Dma_Cfg.h to pick up the new struct sizes.

6.13.1.3. Change 2: Wrap size parameter type widening

6.13.1.3.1. Description

The SrcWrapSize parameter of Cdd_Dma_SetTransferWrapSrcProperties and the DestWrapSize parameter of Cdd_Dma_SetTransferWrapDestProperties have each been widened from uint16 to uint32. The same widening applies to Cdd_Dma_TransferSrcWrapType.SrcWrapSize and Cdd_Dma_TransferDestWrapType.DestWrapSize, which are embedded in Cdd_Dma_TransferParamsType.

As with Change 1, the driver subtracts 1 from the wrap size before writing to the hardware register. Widening from uint16 to uint32 allows the user to input 65536, causing the driver to write the hardware maximum value of 65535 — previously unreachable with a uint16 input.

All values previously valid under uint16 continue to produce identical runtime behavior. The struct layout of Cdd_Dma_TransferSrcWrapType, Cdd_Dma_TransferDestWrapType, and Cdd_Dma_TransferParamsType is larger, requiring regeneration of the plugin-generated files.

6.13.1.3.2. Old vs New

Symbol

v01.00.00

v01.01.00

Cdd_Dma_SetTransferWrapSrcProperties — SrcWrapSize parameter type

uint16

uint32

Cdd_Dma_SetTransferWrapDestProperties — DestWrapSize parameter type

uint16

uint32

Cdd_Dma_TransferSrcWrapType.SrcWrapSize field type

uint16

uint32

Cdd_Dma_TransferDestWrapType.DestWrapSize field type

uint16

uint32

Note

Existing calls that pass wrap size values within the old uint16 range (≤ 65535) continue to compile and behave identically. No runtime change occurs for those values.

6.13.1.3.3. Migration Actions

  1. Update application variable types: In application code that calls Cdd_Dma_SetTransferWrapSrcProperties or Cdd_Dma_SetTransferWrapDestProperties directly, update any uint16 variables holding the wrap size to uint32 to match the new parameter types.

  2. Update wrap struct initializers: If application code directly initializes Cdd_Dma_TransferSrcWrapType or Cdd_Dma_TransferDestWrapType structs, update uint16 literals or variables assigned to SrcWrapSize or DestWrapSize to use uint32.

  3. Regenerate plugin output: Open EB Tresos and regenerate Cdd_Dma_Cfg.c and Cdd_Dma_Cfg.h using the updated plugin to reflect the new struct layout.

  4. Rebuild the project: Recompile all translation units that include Cdd_Dma.h or Cdd_Dma_Cfg.h to pick up the new struct sizes.