6.3. CAN Module Migration

Migration Approach: Follow sequential migration for clear understanding of changes at each version. Each migration is organized by individual changes with description, old vs new comparison, and migration actions.

6.3.1. v04.01.00 (i.e release v26.00.01) from v04.00.00 (i.e release v26.00.00) Migration

6.3.1.1. Summary

Version v04.01.00 (release v26.00.01) introduces the following change to the CAN module:

  1. CanMultiplexedTransmission Config: The Tx buffer ordering mode is now correctly driven by the CanMultiplexedTransmission configuration parameter.

6.3.1.2. Change 1: Tx Buffer Mode Now Respects CanMultiplexedTransmission Config

6.3.1.2.1. Description

The CanMultiplexedTransmission parameter in CanGeneral controls the Tx buffer ordering mode:

  • CanMultiplexedTransmission = true → Queue mode: priority-order transmission

  • CanMultiplexedTransmission = false → FIFO mode: first-in, first-out transmission

Note

Per AUTOSAR, CanMultiplexedTransmission is a global parameter in CanGeneral and applies to all CAN controller instances. There is no per-controller override.

CanMultiplexedTransmission parameter in EB Tresos

Fig. 6.4 CanMultiplexedTransmission parameter location under Can → General

In earlier versions, the driver unconditionally initialized every controller to operate in Queue mode regardless of the CanMultiplexedTransmission setting. Starting with this release, the driver evaluates the CanMultiplexedTransmission parameter and programs the controller accordingly.

Users who configured CanMultiplexedTransmission = false expecting FIFO-ordered transmission were silently running in Queue mode. After upgrading, these controllers will operate in FIFO mode as configured, which changes the hardware Tx arbitration behaviour.

6.3.1.2.2. Old vs New

CanMultiplexedTransmission

v26.00.00

v26.00.01

false

Queue mode (config ignored)

FIFO mode (config respected)

true

Queue mode

Queue mode (no change)

6.3.1.2.3. Migration Actions

  1. Check your CanMultiplexedTransmission setting: In EB Tresos, open Can → General and locate the CanMultiplexedTransmission parameter.

  2. If CanMultiplexedTransmission = true: No action required — Queue mode was active before and remains active.

  3. If CanMultiplexedTransmission = false: The hardware will now operate in FIFO mode. Review any application logic that depends on Tx message transmission order (e.g., priority-based frame scheduling, latency assumptions). Confirm that FIFO ordering matches the intended design.

  4. Rebuild: After verifying configuration intent, rebuild the project.


6.3.2. v04.00.00 (i.e release v26.00.00) from v03.01.00 (i.e release v01.04.01) Migration

6.3.2.1. Summary

Version v04.00.00 introduces the following changes to the CAN module:

  1. Standard Filter Type Enum Value Renamed: CAN_FILTER_DISABLED renamed to CAN_SFT_FILTER_DISABLED_EFT_RANGE_NO_XIDAM to accurately reflect the dual behavior of filter type 0x03

  2. CanMainFunctionRWPeriodRef Validation Added: CanMainFunctionRWPeriodRef is now required when the associated controller uses POLLING or MIXED processing mode

  3. TDC Parameters Now Interpreted as Nanoseconds: CanControllerTrcvDelayCompensationOffset and CanControllerTrcvDelayCompensationFilter are now correctly treated as nanosecond values and converted to MTQ at code-generation time — configurations with non-zero TDC values must be recalculated

6.3.2.2. Change 1: Standard Filter Type Enum Value Renamed

6.3.2.2.1. Description

The CanStandardFilterType enum value CAN_FILTER_DISABLED (numeric value 0x03) has been renamed to CAN_SFT_FILTER_DISABLED_EFT_RANGE_NO_XIDAM. The new name accurately reflects the dual behavior of this value: for Standard Frame Type (SFT) filters it disables the filter, and for Extended Frame Type (EFT) range filters it applies the range without the XIDAM mask.

6.3.2.2.2. Old vs New

Old (v03.10.00):

Add Hardware Object Instance

Fig. 6.5 Old CAN Filter Types

New (v04.00.00):

Add Hardware Object Instance

Fig. 6.6 New CAN Filter Types

6.3.2.2.3. Migration Actions

  1. Regenerate configuration — EB Tresos will generate the updated enum value name in Can_Cfg.h automatically

  2. Recompile the application to confirm no remaining references to the old name

6.3.2.3. Change 2: CanMainFunctionRWPeriodRef Now Required for POLLING/MIXED Mode due to AUTOSAR requirement

6.3.2.3.1. Description

AUTOSAR requirement enforces that CanMainFunctionRWPeriodRef must be configured for any Hardware Object Handle whose associated controller uses POLLING or MIXED processing mode. Previously this reference was optional and could be left unconfigured; now leaving it unconfigured produces a validation error in EB Tresos at configuration time as prescribed by AUTOSAR.

6.3.2.3.2. Old vs New

Old (v03.01.00):

CanMainFunctionRWPeriodRef had no mandatory validation — it could be left empty even when the controller used POLLING or MIXED mode processing.

New (v04.00.00):

EB Tresos enforces that CanMainFunctionRWPeriodRef must reference a valid CanMainFunctionPeriod entry when:

  • CanObjectType = RECEIVE and the controller’s CanRxProcessing = POLLING or MIXED, or

  • CanObjectType = TRANSMIT and the controller’s CanTxProcessing = POLLING or MIXED

Validation fails with the error:

Add Hardware Object Instance

Fig. 6.7 Validation for CanMainFunctionRWPeriodRef

6.3.2.3.3. Migration Actions

  1. Open EB Tresos and navigate to each CanHardwareObject container

  2. Check processing mode for each Hardware Object Handle, check whether the associated controller uses POLLING or MIXED mode for the corresponding direction (receive or transmit)

  3. Configure the reference CanMainFunctionRWPeriodRef to point to the appropriate CanMainFunctionPeriod entry for any Hardware Object Handle that was previously left unconfigured

  4. Run validation in EB Tresos to confirm the validation check

6.3.2.4. Change 3: TDC Parameters Now Interpreted as Nanoseconds

6.3.2.4.1. Description

The FD baud-rate parameters CanControllerTrcvDelayCompensationOffset and CanControllerTrcvDelayCompensationFilter have always been labeled as nanoseconds in the EB Tresos GUI, but in v03.01.00 the generated code passed the raw config values directly to the hardware register as Minimum Time Quanta (MTQ). This meant users who wanted TDC to function correctly had to enter MTQ values despite the nanosecond label.

In v04.00.00, the code generator now correctly converts these values from nanoseconds to MTQ.

Note

If both CanControllerTrcvDelayCompensationOffset and CanControllerTrcvDelayCompensationFilter are 0, TDC remains disabled and no action is required.

6.3.2.4.2. Old vs New

Old (v03.01.00):

The raw config value was passed directly to the hardware register as MTQ, despite the EB Tresos parameter label showing nanoseconds.

New (v04.00.00):

The value is converted from nanoseconds to MTQ at code-generation time. The comment in the generated file shows the source nanosecond value for traceability.

6.3.2.4.3. Migration Actions

  1. Check your current TDC parameter values — open EB Tresos and locate CanControllerTrcvDelayCompensationOffset and CanControllerTrcvDelayCompensationFilter under each FD baud-rate configuration

  2. If both values are 0: no action required — TDC is disabled and behavior is unchanged

  3. If either value is non-zero, the existing values were being used as MTQ and must now be replaced with nanosecond equivalents:

    • Determine the correct TDC offset and filter values in nanoseconds for your transceiver

    • Update CanControllerTrcvDelayCompensationOffset and CanControllerTrcvDelayCompensationFilter in EB Tresos to the nanosecond values

  4. Regenerate the configuration using EB Tresos

  5. Recompile and confirm the generated Can_PBcfg.c contains the conversion comments and that no code-generation assertion errors are reported


6.3.3. v03.00.00 (i.e release v01.04.00) from v02.00.00 (i.e release v01.03.00) Migration

6.3.3.1. Summary

Version v3.00.00 introduces fundamental architectural changes that shift from direct parameter configuration to centralized resource management:

  1. Resource Allocator Introduction: Resource Allocator becomes mandatory for all CAN module configuration

  2. Controller Name Updates: Controller naming convention changes from numeric (MCAN1, MCAN2) to alphabetic (MCANA, MCANB)

  3. ISR Name Updates: Interrupt Service Routine names updated to match new controller naming pattern

PREREQUISITE: Complete Resource Allocator Setup before proceeding.

6.3.3.2. Change 1: Resource Allocator Introduction

6.3.3.2.1. Description

Resource Allocator becomes a mandatory architectural foundation, replacing direct parameter configuration with centralized resource management. This represents a fundamental shift in how CAN controllers are configured and referenced.

6.3.3.2.2. Old vs New Configuration

Old (v02.00.00):

Open CAN Controller

Fig. 6.8 v02.00.00: Direct controller parameter selection with CanControllerInstance as MCAN1 and CanControllerBaseAddress in hexadecimal format (0x60020000)

New (v03.00.00):

Select CAN Instance

Fig. 6.9 v03.00.00: Select CAN instance from ResourceAllocator reference (MCANA, MCANB, etc.)

6.3.3.2.3. Migration Actions

  1. Setup Resource Allocator: Follow Resource Allocator Setup

  2. Navigate to Context: Navigate to ResourceAllocatorGeneral → Context → Can and add CAN allocator:

Add CAN Allocator

Fig. 6.10 Navigate to Context and add CAN allocator

  1. Add CAN Instance: Add CanAllocatedInstance with new naming convention:

Add CAN Instance

Fig. 6.11 Add CanAllocatedInstance with new naming (MCANA, MCANB, etc.)

  1. Configure CAN Instance: Configure CAN instances with new controller names:

Configure CAN Instance

Fig. 6.12 Configure CAN instances with new controller names

  1. Complete Configuration: Finalize CAN instance allocation:

Final CAN Configuration

Fig. 6.13 Complete CAN instance allocation (MCANA, MCANB, MCANC)

  1. Navigate to CanController: Navigate to Can → CanController and update configurations to reference the CAN instances allocated in Resource Allocator

  2. Open Controller Configuration: Access the CanController configuration that needs to be updated

  3. Set Instance Reference: Set CanControllerInstanceRef to point to the corresponding CanAllocatedInstance in Resource Allocator

  4. Verify Automatic Derivation: Confirm that the CanControllerBaseAddress parameter is now automatically derived from the Resource Allocator reference

6.3.3.3. Change 2: Controller Name Updates

6.3.3.3.1. Description

Controller naming convention changes from numeric identifiers (MCAN1, MCAN2, etc.) to alphabetic identifiers (MCANA, MCANB, etc.) to align with Resource Allocator requirements and improve naming consistency.

6.3.3.3.2. Old vs New Names

Controller Name Mapping:

v02.00.00

v03.00.00

Hardware

MCAN1

MCANA

MCAN_A

MCAN2

MCANB

MCAN_B

MCAN3

MCANC

MCAN_C

MCAN4

MCAND

MCAN_D

MCAN5

MCANE

MCAN_E

MCAN6

MCANF

MCAN_F

6.3.3.3.3. Migration Actions

No additional action required. Controller name updates are automatically handled when following the Resource Allocator setup steps in Change 1. The controller naming convention changes from numeric identifiers (MCAN1, MCAN2) to alphabetic identifiers (MCANA, MCANB) are applied automatically through the Resource Allocator configuration.

If you have used the old controller names in the application code, please change them to match the new naming convention.

6.3.3.4. Change 3: ISR Name Updates

6.3.3.4.1. Description of Change

Interrupt Service Routine (ISR) names are updated to match the new controller naming pattern, changing from numeric-based naming to alphabetic-based naming for consistency.

6.3.3.4.2. Old vs New ISR Names

ISR Name Mapping:

v02.00.00 ISR

v03.00.00 ISR

Type

Can_1_Int1ISR

Can_A_Int1ISR

Interrupt 1

Can_1_WakeUpISR

Can_A_WakeUpISR

Wake-up

Can_2_Int1ISR

Can_B_Int1ISR

Interrupt 1

Can_2_WakeUpISR

Can_B_WakeUpISR

Wake-up

Naming Pattern: Can_{Number}_ → Can_{Letter}_

6.3.3.4.3. Migration Actions

  1. Update Application Code: Search and replace ISR references in your application code following the new naming pattern

  2. Update Interrupt Vector Table: Ensure interrupt vector table references use the new ISR names

  3. Verify ISR Functionality: Test interrupt handling after migration to confirm proper operation

6.3.4. v02.00.00 (i.e release v01.03.00) from v01.01.00 (i.e release v01.02.00) Migration

6.3.4.1. Summary

Version v2.00.00 introduces redefinition of BASIC and FULL hardware object parameters with AUTOSAR-compliant constraints and behavior changes:

  1. Hardware Object Parameter Redefinition: BASIC and FULL hardware object parameters are redefined with enforced AUTOSAR-compliant constraints and new memory limitations

  2. Application Code Update: Configuration structure name change for AUTOSAR TPS_ECUC_08011 compliance

6.3.4.2. Change 1: Hardware Object Parameter Redefinition

6.3.4.2.1. Description

Version v2.00.00 redefines BASIC and FULL hardware object parameters with enforced AUTOSAR-compliant constraints. This change introduces specific hardware utilization patterns and memory constraints that were not enforced in previous versions.

6.3.4.2.2. Old vs New Parameter Definitions

CanHandleType Parameter Changes:

Handle Type

v01.01.00

v02.00.00

FULL

• Not used by driver

• Hardware dedicated buffer is used

BASIC

• Not used by driver

• For TRANSMIT messages, Tx FIFO is used
• For RECEIVE messages, Rx FIFO or FIFO1 is used

CanHwObjectCount Parameter Changes:

Configuration

v01.01.00

v02.00.00

CanHwObjectCount = 1

• Uses hardware dedicated buffer
• Restriction: Not allowed for BASIC objects

• Uses hardware dedicated buffer
• Recommended: Use for FULL objects only
• Warning: Allowed for BASIC objects but not recommended

CanHwObjectCount > 1

• Uses hardware FIFO
• Allowed: For both BASIC and FULL objects
• Represents FIFO depth
• Tx FIFO for TRANSMIT messages
• Rx FIFO for RECEIVE messages
• Combined depth when multiple objects use FIFO

• Uses hardware FIFO
• Allowed: For BASIC objects only
• Represents FIFO depth
• Tx FIFO for TRANSMIT messages
• Rx FIFO for RECEIVE messages
• Combined depth when multiple objects use FIFO

Message RAM Memory Area Constraints:

Constraint

v01.01.00

v02.00.00

Standard filters

No constraint

Maximum 128 (1 word each)

Extended filters

No constraint

Maximum 64 (2 word each)

Dedicated Tx buffers

Maximum 32

Maximum 32 (4/18 word each)

Tx FIFO

No constraint on FIFO count
Maximum 32 entries

Maximum 32 entries (4/18 word each entry)
Combined FIFO and entries: 32 max

Dedicated Rx buffers

Maximum 64

Maximum 64 (4/18 word each)

Rx FIFO

Maximum 64 entries

Maximum 64 entries (4/18 word each)
Maximum 2 Rx FIFOs
Maximum 2 entries per FIFO1

Total RAM area

No constraint

1024 words total for all components

Message size

Size varies

4 words (CanFDMode enabled)
18 words (CanFDMode disabled)

Note

These constraints are added as per hardware capacity per controller so that EB Tresos can give error when wrong configurations are added. This helps to avoid message RAM memory overflow. Refer to TRM for details.

6.3.4.2.3. Migration Actions

  1. Navigate to Hardware Objects: Navigate to Can → CanHardwareObject and add hardware object instances as needed for your application:

Add Hardware Object Instance

Fig. 6.14 Add hardware object instance for BASIC/FULL configuration

  1. Configure CanHandleType: Configure each hardware object with appropriate CanHandleType (BASIC or FULL):

Select BASIC or FULL Type

Fig. 6.15 Select BASIC or FULL object type with new constraint definitions

CanHandleType Configuration Guidelines:

Handle Type

Configuration

Hardware Usage

FULL

Use dedicated buffer in hardware

Individual dedicated buffer per object

BASIC

Use FIFO in hardware

Shared FIFO (1 Tx FIFO, 2 Rx FIFOs available)

Hardware Limitations:

  • Maximum 1 Tx BASIC object

  • Maximum 2 Rx BASIC objects

  1. Set CanHwObjectCount: Configure based on handle type:

Handle Type

CanHwObjectCount

Usage

Limits

FULL

1 (recommended)

Dedicated buffer

-

BASIC

> 1

FIFO depth

Tx FIFO: max 32
Rx FIFO: max 64

FIFO Usage Pattern:

  • TRANSMIT messages: Use Tx FIFO

  • RECEIVE messages: Use Rx FIFO

  • Multiple objects: Share combined FIFO depth

  1. Configure Message Filters: Setup message filters within new RAM constraints:

Add Message Filter

Fig. 6.16 Configure message filters with new RAM constraints

Configure Filter Parameters

Fig. 6.17 Set filter parameters within new limits

Message RAM Memory Constraints to Follow:

Constraint Type

Maximum Limit

Word Size

Action Required

Standard filters

128 filters

1 word each

Configure CanStandardObject within allowed limit. EB Tresos will prompt error if exceeded

Extended filters

64 filters

2 words each

Stay within limit during configuration

Dedicated Tx buffers

32 buffers

4/18 words each

Monitor total usage

Tx FIFO entries

32 entries total

4/18 words each

Combined FIFO and entries max: 32

Dedicated Rx buffers

64 buffers

4/18 words each

Monitor total usage

Rx FIFO entries

64 entries max

4/18 words each

Max 2 Rx FIFOs, Max 2 entries per FIFO1

Total RAM area

1024 words

Combined total

All components together must not exceed 1024 words

Message Size Reference:

  • 4 words if parameter CanFDMode is enabled

  • 18 words if parameter CanFDMode is disabled

  1. Verify All Constraints: Ensure all configurations stay within the new memory limits to avoid EB Tresos configuration errors and message RAM memory overflow. Refer to TRM for additional details.

6.3.4.3. Change 2: Application Code Update

6.3.4.3.1. Description

Version v2.00.00 changes the configuration structure name for AUTOSAR TPS_ECUC_08011 compliance, requiring updates to application code that references the CAN configuration structure.

6.3.4.3.2. Old vs New Configuration Structure

Configuration Structure Name Mapping:

v01.01.00

v02.00.00

Can_CanConfigSet

Can_Config

Code Examples:

// v01.01.00
Can_Init(&Can_CanConfigSet);

// v02.00.00
Can_Init(&Can_Config);

6.3.4.3.3. Migration Actions

  1. Search Application Code: Find all references to Can_CanConfigSet in your application code

  2. Replace Structure Name: Update all references from Can_CanConfigSet to Can_Config

  3. Update Function Calls: Ensure all CAN initialization calls use the new structure name

  4. Verify Compilation: Clean build and verify no compilation errors related to CAN configuration structure

6.3.5. v01.01.00 (i.e release v01.02.00) from v01.00.01 (i.e release v01.01.00) Migration

6.3.5.1. Summary

Version v01.01.00 introduces a clock reference parameter update to remove dependency between CAN and OS modules for timeout calculation:

  1. Clock Reference Parameter Update: CanOsCounterRef parameter replaced with CanSysClockRef to eliminate CAN-OS module dependency

6.3.5.2. Change 1: Clock Reference Parameter Update

6.3.5.2.1. Description

The CanOsCounterRef parameter used as tick reference to calculate CAN_CFG_TIMEOUT_DURATION is replaced with CanSysClockRef. This change removes dependency between CAN and OS modules by referencing the system clock directly from MCU instead of OS counter.

6.3.5.2.2. Old vs New Clock Configuration

Parameter Name Change:

v01.00.01

v01.01.00

CanOsCounterRef

CanSysClockRef

Old (v01.00.01):

Old CAN Clock Config

Fig. 6.18 v01.00.01: CanOsCounterRef parameter used as tick reference for timeout calculation

New (v01.01.00):

New CAN Clock Config

Fig. 6.19 v01.01.00: CanSysClockRef parameter references MCU system clock directly

6.3.5.2.3. Migration Actions

  1. Navigate to CAN Configuration: Open CAN module configuration in EB Tresos

  2. Remove OS Counter Dependency: The CanOsCounterRef parameter is no longer available in the GUI

  3. Configure System Clock Reference: Use the new CanSysClockRef parameter to refer to system clock in MCU module

  4. Verify Clock Frequency: Ensure the clock frequency matches your MCU system clock configuration

  5. Update Timeout Calculation: CAN_CFG_TIMEOUT_DURATION is now calculated based on the MCU system clock frequency

Benefits: This change eliminates dependency between CAN and OS modules, provides more direct and reliable timeout calculation based on system clock, and simplifies configuration by using MCU system clock directly.