7.9.8.82. GEL_SetWaitInResetMode()ΒΆ

Sets or clears the Halt on Reset option.

Syntax

GEL_SetWaitInResetMode("integer");

Parameters

integer:

0 - Will not halt on a reset.

1 - Halts at the beginning of the reset vector once a reset has been set.

Description

This GEL function sets or clears the Halt on Reset menu option, which is used for resets that occur externally to the debugger.

Synchronous

Synchronous from GEL: Yes

Completely Synchronous: Yes

Related Topics

GEL_Reset

GEL_Restart

GEL_Run

GEL_Halt