7.9.8.69. GEL_RemoveOutputFile()ΒΆ

Removes the output file from the breakpoint at the specified address.

Syntax

GEL_RemoveOutputFile(programAddr, "connectFileName");

Removes the output file from the breakpoint in the specified file.

Syntax

GEL_RemoveOutputFile("srcFileName", lineNumber, "connectFileName");

Parameters

programAddr: is an expression specifying the memory location of the breakpoint to be removed. This expression should not be enclosed in quotation marks.

srcFileName: is a string value specifying the filename (without path) of the source file in which the breakpoint to be removed is located. A double backslash escape sequence is required to ensure that a backslash is inserted into the filename; for example: "c:\ti\myprojects\sine.dat"

lineNumber: is a long integer value specifying the line number in said file at which the breakpoint to be removed is located.

connectFileName: is a string value specifying the full path and filename of the file connected with the breakpoint. This connection will be severed and the file closed. A double backslash escape sequence is required to ensure that a backslash is inserted into the filename; for example: "c:\ti\myprojects\sine.dat"

Description

This function disconnects the specified file from the appropriate breakpoint, puts the corresponding output FileI/O object into the Stopped state, closes the output file, and removes the breakpoint (whether or not it was originally added by a call to GEL_AddOutputFile).

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Related Topics

GEL_RemoveInputFile

GEL_AddOutputFile