7.9.8.66. GEL_RefreshWindowsΒΆ

Forces a refresh of all IDE windows

Format

GEL_RefreshWindows();

Parameters

None

Description

This function causes the Disassembly window, Mixed Mode window, Register window, Memory window and the Watch window to refresh their contents with what is on the target. This can be useful if target memory is changing while the target is halted, such as due to a DMA transfer.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_RefreshWindows