7.9.8.111. OnChildRunning()ΒΆ

GEL callback function called on the parent processor when one of its child is running.

Syntax

OnChildRunning();

Parameters

Description

If defined in a loaded GEL file on the parent processor, OnChildRunning() is called when one of its child is running.