7.9.8.118. OnRestart()ΒΆ

GEL callback function called when the program is restarted.

Syntax

OnRestart( int nErrorCode );

Parameters

nErrorCode0 (zero) indicates success.

Description

If defined in a loaded GEL file, OnRestart() is called when the program is restarted.

Example

OnRestart(int nErrorCode)
{
if (nErrorCode)
GEL_TextOut("An error occurred while restarting. -%d-n",,,,, nErrorCode);
else
GEL_TextOut("Restart was successful. -%d-n",,,,, nErrorCode);}