7.9.8.5. GEL_AsmStepInto()ΒΆ

Executes the next assembly instruction.

Syntax

GEL_AsmStepInto([count] );

Parameters

count(optional) specifies the number of times the command is to be repeated. If no count is specified, GEL_ASMStepInto executes a single assembly instruction.

Description

Executes the next assembly instruction, whether source is available or not. Repeats count times. Optionally, you can enable/disable automatic focus change to a Disassembly window, in assembly or mixed mode, to show the current assembly instruction.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_AsmStepInto();

Related Topics

GEL_SrcStepInto

GEL_SrcStepOver

GEL_AsmStepOver