Implements Data path AoA2D processing functionality.
Implements Data path DoA processing functionality.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
Data Structures | |
struct | DPU_Aoa2dProc_InitParams |
dopplerProc DPU initial configuration parameters More... | |
struct | DPU_Aoa2dProc_HWA_Doppler_Fft_Cfg |
Configuration parameters for each HWA param set performing the Doppler FFTs and mappng output into row-col array as input to azimuth/elevation FFTs. More... | |
struct | DPU_Aoa2dProc_HWA_Option_Cfg |
struct | DPU_Aoa2dProc_FFTWindowCfg |
dopplerProc DPU HWA configuration parameters More... | |
struct | DPU_Aoa2dProc_HwaCfg |
dopplerProc DPU HWA configuration parameters More... | |
struct | DPU_Aoa2dProc_HwaMaxOutput |
Maximum peaks filled by HWA statistics block. More... | |
struct | DPU_Aoa2dProc_EdmaCfg |
dopplerProc DPU EDMA configuration parameters More... | |
struct | DPU_Aoa2dProc_HW_Resources |
Aoa2d DPU HW configuration parameters. More... | |
struct | DPU_Aoa2dProc_compRxChannelBiasCfg |
Range Bias and rx channel gain/phase compensation configuration. More... | |
struct | DPU_Aoa2dProc_compRxChannelBiasFloatCfg |
Range Bias and rx channel gain/phase compensation configuration. More... | |
struct | DPU_Aoa2dProc_AoaFovCfg |
Field of view - AoA2d Configuration. More... | |
struct | DPU_Aoa2dProc_detectionCfg |
Holds number of samples to be skipped in detection process from left and right side of the dimension for range, azimuth and elevation dimension. More... | |
struct | DPU_Aoa2dProc_compressCfg |
Compression parameters. More... | |
struct | DPU_Aoa2dProc_StaticConfig |
Doppler DPU static configuration parameters. More... | |
struct | DPU_Aoa2dProc_Config |
aoa2dProc DPU configuration parameters More... | |
struct | DPU_Aoa2dProc_OutParams |
DPU processing output parameters. More... | |
Macros | |
#define | DPU_AOA2DPROC_EINVAL (DP_ERRNO_AOA2D_PROC_BASE-1) |
Error Code: Invalid argument. More... | |
#define | DPU_AOA2DPROC_ENOMEM (DP_ERRNO_AOA2D_PROC_BASE-2) |
Error Code: Out of memory. More... | |
#define | DPU_AOA2DPROC_EINPROGRESS (DP_ERRNO_AOA2D_PROC_BASE-3) |
Error Code: DPU is in progress. More... | |
#define | DPU_AOA2DPROC_EHWARES (DP_ERRNO_AOA2D_PROC_BASE-4) |
Error Code: Out of HWA resources. More... | |
#define | DPU_AOA2DPROC_ESEMA (DP_ERRNO_AOA2D_PROC_BASE-5) |
Error Code: Semaphore creation failed. More... | |
#define | DPU_AOA2DPROC_ESEMASTATUS (DP_ERRNO_AOA2D_PROC_BASE-6) |
Error Code: Bad semaphore status. More... | |
#define | DPU_AOA2DPROC_EEXCEEDHWAMEM (DP_ERRNO_AOA2D_PROC_BASE-7) |
Error Code: Configure parameters exceed HWA memory bank size. More... | |
#define | DPU_AOA2DPROC_ECUBEFORMAT (DP_ERRNO_AOA2D_PROC_BASE-8) |
Error Code: Unsupported radar cube format. More... | |
#define | DPU_AOA2DPROC_EDETMFORMAT (DP_ERRNO_AOA2D_PROC_BASE-9) |
Error Code: Unsupported detection matrix format. More... | |
#define | DPU_AOA2DPROC_EDETMSIZE (DP_ERRNO_AOA2D_PROC_BASE-10) |
Error Code: Insufficient detection matrix size. More... | |
#define | DPU_AOA2DPROC_EWINDSIZE (DP_ERRNO_AOA2D_PROC_BASE-11) |
Error Code: Wrong window size. More... | |
#define | DPU_AOA2DPROC_E_NOTSUPPORTED_ANGLE_DIM_ONE_AND_CPU_LOOP_CTRL (DP_ERRNO_AOA2D_PROC_BASE-12) |
Error Code: Not supported angle dim 1 (no elevation) and. More... | |
#define | DPU_AOA2DPROC_E_EXCEEDED_MAX_NUM_DOPPLER_BINS (DP_ERRNO_AOA2D_PROC_BASE-13) |
Error Code: Doppler FFT size exceeded the limit. Maximum Doppler index is stored in array of type uint8_t. More... | |
#define | DPU_AOA2DPROC_HWA_NUM_REGS_PER_PARAM_SET 8 |
Number of registers per HWA param set. More... | |
#define | DPU_AOA2DPROC_MAX_NUM_HWA_PARAMSET 6 |
Maximum number of HWA paramsets used by DPU. More... | |
#define | DPU_AOA2DPROC_NUM_HWA_MEMBANKS 4 |
Number of HWA memory banks needed. More... | |
#define | DPU_AOA2DPROC_FIRST_SCALING_DISABLED ((uint8_t)0U) |
Disables first butterfly stage scaling. More... | |
#define | DPU_AOA2DPROC_FIRST_SCALING_ENABLED ((uint8_t)1U) |
Enables first butterfly stage scaling. More... | |
#define | DPU_AOA2DPROC_SHIFT_Q8 8 |
scale for side-lobe threshold More... | |
#define | DPU_AOA2DPROC_ONE_Q8 (1<<DPU_CFARPROCHWA_SHIFT_Q8) |
#define | DPU_AOA2D_PROC_MAX_NUM_DOP_FFFT_PARAMS 5 |
Maximum nuber of Doppler FFT params. More... | |
#define | DPU_AOA2D_PROC_MAX_2D_ANT_ARRAY_ELEMENTS 16 |
Maximum number of antenna elements in 2D virtual antenna array (maximum value of the product numRows*numCol) More... | |
Typedefs | |
typedef void * | DPU_Aoa2dProc_Handle |
Handle for Aoa2d Processing DPU. More... | |
Functions | |
DPU_Aoa2dProc_Handle | DPU_Aoa2dProc_init (DPU_Aoa2dProc_InitParams *initCfg, int32_t *errCode) |
int32_t | DPU_Aoa2dProc_process (DPU_Aoa2dProc_Handle handle, DPIF_RadarCube *radarCubeSrc, DPIF_CFARRngDopDetListElement *detRngDopList, uint32_t numDetPoints, DPIF_DetectedRangeGates *detectedRangeGates, DPIF_DetMatrix *detMatrix, DPU_Aoa2dProc_OutParams *outParams) |
int32_t | DPU_Aoa2dProc_deinit (DPU_Aoa2dProc_Handle handle) |
int32_t | DPU_Aoa2dProc_config (DPU_Aoa2dProc_Handle handle, DPU_Aoa2dProc_Config *cfg) |
int32_t | DPU_Aoa2dProc_GetNumUsedHwaParamSets (DPU_Aoa2dProc_Handle handle, uint8_t *numUsedHwaParamSets) |
#define DPU_AOA2DPROC_HWA_NUM_REGS_PER_PARAM_SET 8 |
Number of registers per HWA param set.
#define DPU_AOA2DPROC_MAX_NUM_HWA_PARAMSET 6 |
Maximum number of HWA paramsets used by DPU.
#define DPU_AOA2DPROC_NUM_HWA_MEMBANKS 4 |
Number of HWA memory banks needed.
#define DPU_AOA2DPROC_FIRST_SCALING_DISABLED ((uint8_t)0U) |
Disables first butterfly stage scaling.
#define DPU_AOA2DPROC_FIRST_SCALING_ENABLED ((uint8_t)1U) |
Enables first butterfly stage scaling.
#define DPU_AOA2DPROC_SHIFT_Q8 8 |
scale for side-lobe threshold
#define DPU_AOA2DPROC_ONE_Q8 (1<<DPU_CFARPROCHWA_SHIFT_Q8) |
#define DPU_AOA2D_PROC_MAX_NUM_DOP_FFFT_PARAMS 5 |
Maximum nuber of Doppler FFT params.
#define DPU_AOA2D_PROC_MAX_2D_ANT_ARRAY_ELEMENTS 16 |
Maximum number of antenna elements in 2D virtual antenna array (maximum value of the product numRows*numCol)
typedef void* DPU_Aoa2dProc_Handle |
Handle for Aoa2d Processing DPU.
DPU_Aoa2dProc_Handle DPU_Aoa2dProc_init | ( | DPU_Aoa2dProc_InitParams * | initCfg, |
int32_t * | errCode | ||
) |
int32_t DPU_Aoa2dProc_process | ( | DPU_Aoa2dProc_Handle | handle, |
DPIF_RadarCube * | radarCubeSrc, | ||
DPIF_CFARRngDopDetListElement * | detRngDopList, | ||
uint32_t | numDetPoints, | ||
DPIF_DetectedRangeGates * | detectedRangeGates, | ||
DPIF_DetMatrix * | detMatrix, | ||
DPU_Aoa2dProc_OutParams * | outParams | ||
) |
int32_t DPU_Aoa2dProc_deinit | ( | DPU_Aoa2dProc_Handle | handle | ) |
int32_t DPU_Aoa2dProc_config | ( | DPU_Aoa2dProc_Handle | handle, |
DPU_Aoa2dProc_Config * | cfg | ||
) |
int32_t DPU_Aoa2dProc_GetNumUsedHwaParamSets | ( | DPU_Aoa2dProc_Handle | handle, |
uint8_t * | numUsedHwaParamSets | ||
) |