![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.02.00
|
|
Go to the documentation of this file.
77 #include <drivers/hw_include/csl_complex_math_types.h>
79 #include <drivers/hw_include/cslr_hwa.h>
90 #define HWADRV_ADDR_TRANSLATE_CPU_TO_HWA(x) (uint32_t)((uint32_t)(x) & 0x000FFFFFU)
99 #define HWA_ERRNO_BASE (-2800)
101 #define HWA_EINVAL (HWA_ERRNO_BASE-1)
103 #define HWA_ENOINIT (HWA_ERRNO_BASE-2)
105 #define HWA_EOUTOFRANGE (HWA_ERRNO_BASE-3)
107 #define HWA_EOUTOFMEM (HWA_ERRNO_BASE-4)
109 #define HWA_ENOTSUPP (HWA_ERRNO_BASE-5)
111 #define HWA_EINUSE (HWA_ERRNO_BASE-6)
113 #define HWA_ENOTALIGNED (HWA_ERRNO_BASE-7)
115 #define HWA_EINVAL_COMMON_REGISTER_PARAMSET (HWA_ERRNO_BASE-8)
117 #define HWA_EINVAL_COMMON_REGISTER_PARAMSET_ALT (HWA_ERRNO_BASE-9)
119 #define HWA_EINVAL_COMMON_REGISTER_FFTCONFIG (HWA_ERRNO_BASE-10)
121 #define HWA_EINVAL_COMMON_REGISTER_DCEST (HWA_ERRNO_BASE-11)
123 #define HWA_EINVAL_COMMON_REGISTER_CFAR (HWA_ERRNO_BASE-12)
125 #define HWA_EINVAL_COMMON_REGISTER_INTERFERENCE (HWA_ERRNO_BASE-13)
127 #define HWA_EINVAL_COMMON_REGISTER_COMPLEXMULT (HWA_ERRNO_BASE-14)
129 #define HWA_EINVAL_COMMON_REGISTER_CHANCOMB (HWA_ERRNO_BASE-15)
131 #define HWA_EINVAL_COMMON_REGISTER_ZEROINSERT (HWA_ERRNO_BASE-16)
133 #define HWA_EINVAL_COMMON_REGISTER_ADVSTAT (HWA_ERRNO_BASE-17)
135 #define HWA_EINVAL_COMMON_REGISTER_COMPRESS (HWA_ERRNO_BASE-18)
137 #define HWA_EINVAL_COMMON_REGISTER_LOCALMAXIMUM (HWA_ERRNO_BASE-19)
139 #define HWA_EINVAL_PARAMSET_GENERALCONFIG (HWA_ERRNO_BASE - 20)
141 #define HWA_EINVAL_PARAMSET_SOURCE (HWA_ERRNO_BASE - 21)
143 #define HWA_EINVAL_PARAMSET_DEST (HWA_ERRNO_BASE - 22)
145 #define HWA_EINVAL_PARAMSET_SRCDST_ADDRESS (HWA_ERRNO_BASE - 23)
147 #define HWA_EINVAL_PARAMSET_FFTMODE_GENERALCONFIG (HWA_ERRNO_BASE - 24)
149 #define HWA_EINVAL_PARAMSET_FFTMODE_SIZE (HWA_ERRNO_BASE - 25)
151 #define HWA_EINVAL_PARAMSET_FFTMODE_POSTPROC (HWA_ERRNO_BASE - 26)
153 #define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC (HWA_ERRNO_BASE - 27)
155 #define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_INTERF (HWA_ERRNO_BASE - 28)
157 #define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_COMPLEXMULT (HWA_ERRNO_BASE - 29)
159 #define HWA_EINVAL_PARAMSET_CFARMODE_GENERALCONFIG (HWA_ERRNO_BASE - 30)
161 #define HWA_EINVAL_PARAMSET_CFARMODE_OSCONFIG (HWA_ERRNO_BASE - 31)
163 #define HWA_EINVAL_PARAMSET_CFARMODE_CACONFIG (HWA_ERRNO_BASE - 32)
165 #define HWA_EINVAL_PARAMSET_COMPRESSMODE (HWA_ERRNO_BASE - 33)
167 #define HWA_EINVAL_PARAMSET_LOCALMAXMODE (HWA_ERRNO_BASE - 34)
169 #define HWA_PARAMSET_POLLINGNOTALLOWED (HWA_ERRNO_BASE - 35)
173 #define HWA_NUM_RXCHANNELS (12U)
175 #define HWA_NUM_INTERFMITG_WINARRAY (5U)
177 #define HWA_BPMPATTERN_LENGTH_INWORDS (8U)
179 #define HWA_CHANCOMB_LENGTH_INWORDS (8U)
181 #define HWA_ZEROINSERT_LENGTH_INWORDS (8U)
183 #define HWA_NUM_RAMS (10U)
185 #define HWA_MAXNUM_LOOPS (4095U)
187 #define HWA_CMP_K_ARR_LEN (8U)
202 #define HWA_DONE_INTERRUPT_PRIORITY (1U)
204 #define HWA_ALTDONE_INTERRUPT_PRIORITY (1U)
206 #define HWA_PARAMSETDONE_INTERRUPT1_PRIORITY (1U)
208 #define HWA_PARAMSETDONE_INTERRUPT2_PRIORITY (1U)
216 #define HWA_FEATURE_BIT_ENABLE ((uint8_t)1U)
217 #define HWA_FEATURE_BIT_DISABLE ((uint8_t)0U)
225 #define HWA_SAMPLES_WIDTH_16BIT ((uint8_t)0U)
226 #define HWA_SAMPLES_WIDTH_32BIT ((uint8_t)1U)
234 #define HWA_SAMPLES_FORMAT_COMPLEX ((uint8_t)0U)
235 #define HWA_SAMPLES_FORMAT_REAL ((uint8_t)1U)
243 #define HWA_SAMPLES_UNSIGNED ((uint8_t)0U)
244 #define HWA_SAMPLES_SIGNED ((uint8_t)1U)
252 #define HWA_FFT_WINDOW_NONSYMMETRIC ((uint8_t)0U)
253 #define HWA_FFT_WINDOW_SYMMETRIC ((uint8_t)1U)
265 #define HWA_FFT_WINDOW_INTERPOLATE_MODE_NONE ((uint8_t)0U)
266 #define HWA_FFT_WINDOW_INTERPOLATE_MODE_4K ((uint8_t)2U)
267 #define HWA_FFT_WINDOW_INTERPOLATE_MODE_8K ((uint8_t)1U)
275 #define HWA_FFT_MODE_MAGNITUDE_LOG2_DISABLED ((uint8_t)0U)
276 #define HWA_FFT_MODE_MAGNITUDE_ONLY_ENABLED ((uint8_t)2U)
277 #define HWA_FFT_MODE_MAGNITUDE_LOG2_ENABLED ((uint8_t)3U)
285 #define HWA_FFT_MODE_OUTPUT_DEFAULT ((uint8_t)0U)
286 #define HWA_FFT_MODE_OUTPUT_MAX_STATS ((uint8_t)2U)
287 #define HWA_FFT_MODE_OUTPUT_SUM_STATS ((uint8_t)3U)
295 #define HWA_NOISE_AVG_MODE_CFAR_CA ((uint8_t)0U)
296 #define HWA_NOISE_AVG_MODE_CFAR_CAGO ((uint8_t)1U)
297 #define HWA_NOISE_AVG_MODE_CFAR_CASO ((uint8_t)2U)
298 #define HWA_NOISE_AVG_MODE_CFAR_OS ((uint8_t)3U)
306 #define HWA_TRIG_MODE_IMMEDIATE ((uint8_t)0U)
307 #define HWA_TRIG_MODE_SOFTWARE ((uint8_t)1U)
308 #define HWA_TRIG_MODE_RESERVED1 ((uint8_t)2U)
309 #define HWA_TRIG_MODE_DMA ((uint8_t)3U)
310 #define HWA_TRIG_MODE_HARDWARE ((uint8_t)4U)
311 #define HWA_TRIG_MODE_RESERVED2 ((uint8_t)5U)
312 #define HWA_TRIG_MODE_RESERVED3 ((uint8_t)6U)
313 #define HWA_TRIG_MODE_M4CONTROL ((uint8_t)7U)
321 #define HWA_CONTEXTSWITCH_TRIG_MODE_DMA ((uint8_t)3U)
322 #define HWA_CONTEXTSWITCH_TRIG_MODE_HARDWARE ((uint8_t)4U)
323 #define HWA_CONTEXTSWITCH_TRIG_MODE_SOFTWARE ((uint8_t)5U)
331 #define HWA_THREAD_BACKGROUNDCONTEXT ((uint8_t)0U)
332 #define HWA_THREAD_ALTCONTEXT ((uint8_t)1U)
340 #define HWA_ACCELMODE_FFT ((uint8_t)0U)
341 #define HWA_ACCELMODE_CFAR ((uint8_t)1U)
342 #define HWA_ACCELMODE_COMPRESS ((uint8_t)2U)
343 #define HWA_ACCELMODE_LOCALMAX ((uint8_t)3U)
344 #define HWA_ACCELMODE_NONE ((uint8_t)7U)
364 #define HWA_CFAR_OPER_MODE_LOG_INPUT_REAL 0U
365 #define HWA_CFAR_OPER_MODE_LOG_INPUT_COMPLEX 1U
366 #define HWA_CFAR_OPER_MODE_MAG_INPUT_REAL 2U
367 #define HWA_CFAR_OPER_MODE_MAG_INPUT_COMPLEX 3U
368 #define HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_REAL 4U
369 #define HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_COMPLEX 5U
370 #define HWA_CFAR_OPER_MODE_LOG_INPUT_COMPLEX_LINEARCFAR 6U
388 #define HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_CUT ((uint8_t)0U)
390 #define HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_DET_FLAG ((uint8_t)1U)
392 #define HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_NEIGHBOR_NOISE_VAL ((uint8_t)2U)
394 #define HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_CUT ((uint8_t)3U)
396 #define HWA_CFAR_OUTPUT_MODE_FILTER_LARGE_PEAK ((uint8_t)4U)
405 #define HWA_RAM_TYPE_WINDOW_RAM ((uint8_t)0U)
406 #define HWA_RAM_TYPE_VECTORMULTIPLY_RAM ((uint8_t)1U)
407 #define HWA_RAM_TYPE_LUT_FREQ_DEROTATE_RAM ((uint8_t)2U)
408 #define HWA_RAM_TYPE_SHUFFLE_RAM ((uint8_t)3U)
409 #define HWA_RAM_TYPE_HIST_THRESH_RAM ((uint8_t)4U)
410 #define HWA_RAM_TYPE_2DSTAT_ITER_VAL ((uint8_t)5U)
411 #define HWA_RAM_TYPE_2DSTAT_ITER_IDX ((uint8_t)6U)
412 #define HWA_RAM_TYPE_2DSTAT_SAMPLE_VAL ((uint8_t)7U)
413 #define HWA_RAM_TYPE_2DSTAT_SAMPLE_IDX ((uint8_t)8U)
414 #define HWA_RAM_TYPE_HISTOGRAM_RAM ((uint8_t)9U)
422 #define HWA_CLIPREG_TYPE_DCACC ((uint8_t)0U)
423 #define HWA_CLIPREG_TYPE_DCEST ((uint8_t)1U)
424 #define HWA_CLIPREG_TYPE_DCSUB ((uint8_t)2U)
425 #define HWA_CLIPREG_TYPE_INTFSTATS_MAGACC ((uint8_t)3U)
426 #define HWA_CLIPREG_TYPE_INTFSTATS_MAGDIFFACC ((uint8_t)4U)
427 #define HWA_CLIPREG_TYPE_INTFSTATS_MAGTHRESHOLD ((uint8_t)5U)
428 #define HWA_CLIPREG_TYPE_INTFSTATS_MAGDIFFTHRESHOLD ((uint8_t)6U)
429 #define HWA_CLIPREG_TYPE_INTFSTATS_MAGSUM ((uint8_t)7U)
430 #define HWA_CLIPREG_TYPE_INTFSTATS_MAGDIFFSUM ((uint8_t)8U)
431 #define HWA_CLIPREG_TYPE_TWIDINCR_DELTAFRAC ((uint8_t)9U)
432 #define HWA_CLIPREG_TYPE_CHANCOMB ((uint8_t)10U)
433 #define HWA_CLIPREG_TYPE_FFT ((uint8_t)11U)
434 #define HWA_CLIPREG_TYPE_INPUTFORMAT ((uint8_t)12U)
435 #define HWA_CLIPREG_TYPE_OUTPUTFORMAT ((uint8_t)13U)
443 #define HWA_ACCUMULATORREG_TYPE_DC ((uint8_t)0U)
444 #define HWA_ACCUMULATORREG_TYPE_INTERF_MAG ((uint8_t)1U)
445 #define HWA_ACCUMULATORREG_TYPE_INTERF_MAGDIFF ((uint8_t)2U)
446 #define HWA_ACCUMULATORREG_TYPE_INTERF ((uint8_t)3U)
454 #define HWA_INTERFERENCE_THRESHOLD_TYPE_MAG ((uint8_t)0U)
455 #define HWA_INTERFERENCE_THRESHOLD_TYPE_MAGDIFF ((uint8_t)1U)
465 #define HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR1 ((uint8_t)1U)
466 #define HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR2 ((uint8_t)2U)
467 #define HWA_PARAMDONE_INTERRUPT_TYPE_DMA ((uint8_t)4U)
476 #define HWA_COMMONCONFIG_MASK_STATEMACHINE_CFG ((uint64_t)0x00000001U)
477 #define HWA_COMMONCONFIG_MASK_STATEMACHINE_CFG_ALT ((uint64_t)0x00000002U)
478 #define HWA_COMMONCONFIG_CONTEXTSWITCH_TRIG_CFG ((uint64_t)0x00000004U)
479 #define HWA_COMMONCONFIG_MASK_BPMCFG ((uint64_t)0x00000008U)
480 #define HWA_COMMONCONFIG_MASK_TWIDDITHERENABLE ((uint64_t)0x00000010U)
481 #define HWA_COMMONCONFIG_MASK_LFSRSEED ((uint64_t)0x00000020U)
482 #define HWA_COMMONCONFIG_MASK_FFTSUMDIV ((uint64_t)0x00000040U)
483 #define HWA_COMMONCONFIG_MASK_CFARTHRESHOLDSCALE ((uint64_t)0x00000080U)
484 #define HWA_COMMONCONFIG_MASK_DCEST_SCALESHIFT ((uint64_t)0x00000100U)
485 #define HWA_COMMONCONFIG_MASK_DCSUB_SWVAL ((uint64_t)0x00000200U)
486 #define HWA_COMMONCONFIG_MASK_INTERFMAG_THRESHOLD ((uint64_t)0x00000400U)
487 #define HWA_COMMONCONFIG_MASK_INTERFMAGDIFF_THRESHOLD ((uint64_t)0x00000800U)
488 #define HWA_COMMONCONFIG_MASK_INTERFSUM_MAG ((uint64_t)0x00001000U)
489 #define HWA_COMMONCONFIG_MASK_INTERFSUM_MAGDIFF ((uint64_t)0x00002000U)
490 #define HWA_COMMONCONFIG_MASK_COMPLEXMULT_SCALEARRAY ((uint64_t)0x00004000U)
493 #define HWA_COMMONCONFIG_MASK_COMPLEXMULT_SCALECONST ((uint64_t)0x00008000U)
496 #define HWA_COMMONCONFIG_MASK_RECWIN_RESET ((uint64_t)0x00010000U)
497 #define HWA_COMMONCONFIG_MASK_TWIDINCR_DELTA_FRAC ((uint64_t)0x00020000U)
499 #define HWA_COMMONCONFIG_MASK_CHANCOMB_VEC_SIZE ((uint64_t)0x00400000U)
500 #define HWA_COMMONCONFIG_MASK_ZEROINSERT_NUM_MASK ((uint64_t)0x00800000U)
501 #define HWA_COMMONCONFIG_MASK_MAX2D_OFFSETBOTHDIM ((uint64_t)0x01000000U)
502 #define HWA_COMMONCONFIG_MASK_CDFCNT_THRESHOLD ((uint64_t)0x02000000U)
503 #define HWA_COMMONCONFIG_MASK_LOCALMAXDIMB_THRESHOLDSW ((uint64_t)0x04000000U)
504 #define HWA_COMMONCONFIG_MASK_LOCALMAXDIMC_THRESHOLDSW ((uint64_t)0x08000000U)
505 #define HWA_COMMONCONFIG_MASK_LOCALMAXDIMBTHRESH_OFFSET ((uint64_t)0x10000000U)
506 #define HWA_COMMONCONFIG_MASK_LOCALMAXDIMCTHRESH_OFFSET ((uint64_t)0x20000000U)
507 #define HWA_COMMONCONFIG_MASK_INTERF_MITG_WINDOW_PARAM ((uint64_t)0x40000000U)
508 #define HWA_COMMONCONFIG_MASK_EGECOMRESS_KPARAM ((uint64_t)0x80000000U)
516 #define HWA_SRC_SHUFFLE_AB_MODE_DISABLE ((uint8_t)0U)
517 #define HWA_SRC_SHUFFLE_AB_MODE_ADIM ((uint8_t)1U)
518 #define HWA_SRC_SHUFFLE_AB_MODE_BDIM ((uint8_t)2U)
526 #define HWA_COMPLEX_MULTIPLY_MODE_DISABLE ((uint8_t)0U)
527 #define HWA_COMPLEX_MULTIPLY_MODE_FREQ_SHIFTER ((uint8_t)1U)
528 #define HWA_COMPLEX_MULTIPLY_MODE_SLOW_DFT ((uint8_t)2U)
529 #define HWA_COMPLEX_MULTIPLY_MODE_FFT_STITCHING ((uint8_t)3U)
530 #define HWA_COMPLEX_MULTIPLY_MODE_MAG_SQUARED ((uint8_t)4U)
531 #define HWA_COMPLEX_MULTIPLY_MODE_SCALAR_MULT ((uint8_t)5U)
532 #define HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT ((uint8_t)6U)
533 #define HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT_2 ((uint8_t)7U)
534 #define HWA_COMPLEX_MULTIPLY_MODE_RECURSIVE_WIN ((uint8_t)8U)
535 #define HWA_COMPLEX_MULTIPLY_MODE_LUT_FREQ_DEROTATE ((uint8_t)9U)
536 #define HWA_COMPLEX_MULTIPLY_MODE_FREQSHIFT_FREQINCREMENT ((uint8_t)10U)
545 #define HWA_FFT_STITCHING_TWID_PATTERN_4K ((uint8_t)1U)
546 #define HWA_FFT_STITCHING_TWID_PATTERN_8K ((uint8_t)2U)
555 #define HWA_RECURSIVE_WIN_MODE_SELECT_ITERATION_COUNT ((uint8_t)0U)
556 #define HWA_FFT_STITCHING_TWID_PATTERN_EXE_COUNT ((uint8_t)1U)
564 #define HWA_WINDOW_MODE_18BITREAL ((uint8_t)0U)
566 #define HWA_WINDOW_MODE_16BITREAL ((uint8_t)1U)
568 #define HWA_WINDOW_MODE_COMPLEX ((uint8_t)2U)
577 #define HWA_FFT3x_BFLY_SCALING_MSBSATURATED ((uint8_t)0U)
578 #define HWA_FFT3x_BFLY_SCALING_MSBSATLSBRND ((uint8_t)1U)
580 #define HWA_FFT3x_BFLY_SCALING_LSBROUNDED ((uint8_t)2U)
589 #define HWA_DCEST_INTERFSUM_RESET_MODE_NOUPDATE ((uint8_t)0U)
590 #define HWA_DCEST_INTERFSUM_RESET_MODE_SOFTWARERESET ((uint8_t)1U)
591 #define HWA_DCEST_INTERFSUM_RESET_MODE_PARAMRESET ((uint8_t)2U)
592 #define HWA_DCEST_INTERFSUM_RESET_MODE_PARAMRESET_ZEROLPCONT ((uint8_t)3U)
600 #define HWA_INTERFTHRESH_MODE_MAG_OR_MAGDIF ((uint8_t)0U)
601 #define HWA_INTERFTHRESH_MODE_MAGDIFF ((uint8_t)1U)
602 #define HWA_INTERFTHRESH_MODE_MAG ((uint8_t)2U)
603 #define HWA_INTERFTHRESH_MODE_MAG_AND_MAGDIFF ((uint8_t)3U)
611 #define HWA_DCSUB_SELECT_DCSW ((uint8_t)0U)
612 #define HWA_DCSUB_SELECT_DCEST ((uint8_t)1U)
620 #define HWA_INTERFTHRESH_SELECT_SW ((uint8_t)0U)
622 #define HWA_INTERFTHRESH_SELECT_EST_AVERAGE ((uint8_t)1U)
624 #define HWA_INTERFTHRESH_SELECT_EST_INDIVIDUAL ((uint8_t)2U)
633 #define HWA_INTERFMITIGATION_PATH_ZEROOUT ((uint8_t)0U)
634 #define HWA_INTERFMITIGATION_PATH_WINDOWZEROOUT ((uint8_t)1U)
635 #define HWA_INTERFMITIGATION_PATH_LINEARINTERPOLATION ((uint8_t)2U)
636 #define HWA_INTERFMITIGATION_PATH_UNUSED ((uint8_t)3U)
647 #define HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_WRAPAROUND ((uint8_t)0U)
648 #define HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_SATURATED ((uint8_t)1U)
649 #define HWA_LUT_FREQ_DEROTATE_RAMIDX_NONINCR ((uint8_t)2U)
657 #define HWA_HISTOGRAM_MODE_DISABLED ((uint8_t)0U)
658 #define HWA_HISTOGRAM_MODE_HISTOGRAM ((uint8_t)1U)
659 #define HWA_HISTOGRAM_MODE_CDF ((uint8_t)2U)
660 #define HWA_HISTOGRAM_MODE_CDF_THRESHOLD ((uint8_t)3U)
668 #define HWA_LOCALMAX_THRESH_BITMASK_BOTH_EN ((uint8_t)0U)
669 #define HWA_LOCALMAX_THRESH_BITMASK_CDIM_EN ((uint8_t)1U)
670 #define HWA_LOCALMAX_THRESH_BITMASK_BDIM_EN ((uint8_t)2U)
671 #define HWA_LOCALMAX_THRESH_BITMASK_BOTH_DIS ((uint8_t)3U)
679 #define HWA_LOCALMAX_THRESH_SELECT_DIMBREG_DIMCREG ((uint8_t)0U)
680 #define HWA_LOCALMAX_THRESH_SELECT_DIMBRAM_DIMCREG ((uint8_t)1U)
681 #define HWA_LOCALMAX_THRESH_SELECT_DIMBREG_DIMCRAM ((uint8_t)2U)
682 #define HWA_LOCALMAX_THRESH_SELECT_DIMBRAM_DIMCRAM ((uint8_t)3U)
690 #define HWA_COMPRESS_METHOD_EGE ((uint8_t)0U)
698 #define HWA_CMP_DCMP_COMPRESS ((uint8_t)0U)
699 #define HWA_CMP_DCMP_DECOMPRESS ((uint8_t)1U)
707 #define HWA_COMPRESS_PATHSELECT_BOTHPASSES ((uint8_t)3U)
708 #define HWA_COMPRESS_PATHSELECT_SECONDPASS ((uint8_t)1U)
720 #define HWA_PARAMSET_CONTEXTSWITCH_DISABLE (0U)
722 #define HWA_PARAMSET_CONTEXTSWITCH_NONFORCE_ENABLE (1U)
725 #define HWA_PARAMSET_CONTEXTSWITCH_FORCE_ENABLE (2U)
759 typedef struct HWA_Attrs_t {
760 uint32_t instanceNum;
761 volatile uint32_t ctrlBaseAddr;
762 volatile uint32_t paramBaseAddr;
763 volatile uint32_t ramBaseAddr;
764 volatile uint32_t dssBaseAddr;
765 uint32_t numHwaParamSets;
766 uint32_t intNum1ParamSet;
767 uint32_t intNum2ParamSet;
769 uint32_t intNumDoneALT;
770 uint32_t numDmaChannels;
771 volatile uint32_t accelMemBaseAddr;
772 uint32_t accelMemSize;
773 bool isConcurrentAccessAllowed;
783 typedef struct HWA_RAMAttrs_t
785 uint32_t ramBaseAddress;
786 uint32_t ramSizeInBytes;
800 typedef struct HWA_SrcDMAConfig_t {
814 typedef struct HWA_CommonConfig_t {
822 uint16_t paramStartIdx;
825 uint16_t paramStopIdx;
828 uint16_t numLoopsALT;
831 uint16_t paramStartIdxALT;
834 uint16_t paramStopIdxALT;
837 uint8_t contextswitchTriggerMode;
840 uint8_t contextswitchTriggerSrc;
856 uint8_t twidDitherEnable;
929 uint8_t sumMagDiffScale;
934 int8_t sumMagDiffShift;
962 int16_t twiddleDeltaFrac;
970 uint8_t recWindowReset;
973 } complexMultiplyConfig;
1008 uint32_t thresholdScale;
1019 int32_t max2DoffsetDim1;
1023 int32_t max2DoffsetDim2;
1028 uint16_t cdfCntThresh;
1038 uint16_t dimBThreshold;
1043 uint16_t dimCThreshold;
1048 uint16_t dimBBaseAddress;
1053 uint16_t dimCBaseAddress;
1076 typedef struct HWA_SourceConfig_t {
1101 uint16_t srcAcircShift;
1105 uint8_t srcAcircShiftWrap;
1112 uint16_t srcBcircShift;
1115 uint8_t srcBcircShiftWrap;
1122 uint16_t srcCcircShift;
1126 uint8_t srcCcircShiftWrap;
1133 uint8_t srcCircShiftWrap3;
1137 uint8_t shuffleMode ;
1140 uint8_t srcRealComplex;
1153 uint8_t srcConjugate;
1176 uint8_t shuffleStart;
1187 typedef struct HWA_DestConfig_t {
1208 uint8_t dstRealComplex;
1223 uint8_t dstConjugate;
1235 uint16_t dstSkipInit;
1251 typedef struct HWA_PostProcStat_t {
1266 uint8_t max2Denable;
1270 uint8_t histogramMode;
1275 uint8_t histogramScaleSelect;
1280 uint8_t histogramSizeSelect;
1292 typedef struct HWA_ComplexMultiply_t {
1302 uint16_t freqShiftTwiddleIncr;
1318 uint16_t twiddlePattern;
1323 uint8_t winInterpolateMode;
1333 uint8_t scaleCmultScaleEn;
1347 uint8_t cmultScaleEn;
1354 uint16_t vecMultiMode1RamAddrOffset;
1356 } vectorMultiplyMode1;
1360 uint16_t vecMultiMode2RamAddrOffset;
1364 } vectorMultiplyMode2;
1368 uint8_t recwinModeSel;
1375 uint16_t ramAddrOffset;
1377 uint8_t ramIdxIncrMode;
1384 uint16_t twiddleIncr;
1387 } freqShiftWithFreIncrement;
1397 typedef struct HWA_PreProcessing_t {
1399 uint8_t dcEstResetMode;
1404 uint8_t dcSubEnable;
1408 uint8_t dcSubSelect;
1412 uint8_t thresholdEnable;
1416 uint8_t thresholdMode;
1420 uint8_t thresholdSelect;
1441 uint8_t countThreshold;
1450 uint8_t leftHystOrder;
1454 uint8_t rightHystOrder;
1465 uint8_t zeroInsertEn;
1480 typedef struct HWA_AccelModeFFT_t{
1493 uint16_t butterflyScaling;
1504 uint16_t windowStart;
1517 uint8_t fftSize3xEn;
1522 uint8_t fftSizeDim2;
1527 uint8_t butterflyScalingFFT3x;
1552 typedef struct HWA_AccelModeCFAR_t{
1553 uint8_t numNoiseSamplesLeft;
1559 uint8_t numNoiseSamplesRight;
1564 uint8_t numGuardCells;
1566 uint8_t nAvgDivFactor;
1576 uint8_t cfarOsKvalue;
1579 uint8_t cfarOsEdgeKScaleEn;
1590 uint8_t cfarAdvOutMode;
1595 uint8_t peakGroupEn;
1604 uint8_t cyclicModeEn;
1617 typedef struct HWA_AccelModeLocalMax_t{
1619 uint8_t neighbourBitmask;
1623 uint8_t thresholdBitMask;
1627 uint8_t thresholdMode;
1630 uint8_t dimBNonCyclic;
1632 uint8_t dimCNonCyclic;
1642 typedef struct HWA_AccelModeCompress_t {
1646 uint8_t EGEKarrayLength;
1649 uint8_t scaleFactorBW;
1656 uint8_t headerEnable;
1663 uint8_t compressDecompress;
1665 uint8_t ditherEnable;
1675 typedef struct HWA_ParamConfig_t {
1676 uint8_t triggerMode;
1699 uint8_t contextswitchCfg;
1709 typedef struct HWA_InterruptConfig_t {
1710 uint8_t interruptTypeFlag;
1732 typedef struct HWA_Stats_t {
1745 typedef struct HWA_AccmulatorVal_t {
1756 typedef struct HWA_DebugStats_t {
1757 uint8_t currentParamSet;
1762 uint8_t paramSetIdxCpuIntr0;
1763 uint8_t paramSetIdxCpuIntr1;
1764 uint16_t currentLoopCount;
1766 uint16_t otherThreadLoopCount;
1767 uint32_t trigStatus[2];
1776 typedef struct HWA_MemInfo_t {
1777 uint32_t baseAddress;
1788 typedef struct HWA_CdfThreshold_t {
1790 uint32_t pdfValue : 12;
1791 uint32_t cdfValue : 12;
1792 uint32_t binNumber : 6;
1793 uint32_t reserved : 2;
1801 typedef struct HWA_InterruptPriority_t {
1803 uint32_t backgroundDone;
1805 uint32_t paramsetDone1;
1806 uint32_t paramsetDone2;
1814 typedef struct HWA_OpenConfig_t {
1845 typedef struct HWA_InterruptCtx_t {
1858 typedef struct HWA_DoneInterruptCtx_t {
1867 typedef struct HWA_Driver_t {
1871 uint32_t instanceNum;
1880 uint8_t configInProgress;
1886 uint16_t paramSetMapInProgress;
1921 uint64_t interrupt1ParamSetMask;
1926 uint64_t interrupt2ParamSetMask;
2146 extern int32_t
HWA_configRam(
HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx);
2179 extern int32_t
HWA_readRam(
HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx);
#define HWA_CHANCOMB_LENGTH_INWORDS
The length of channel combining vector in words.
Definition: hwa/v0/hwa.h:179
HWA Paramset Config for Input Formatter/Source block.
Definition: hwa/v0/hwa.h:1073
HWA Accumulator register value data structure.
Definition: hwa/v0/hwa.h:1742
int32_t HWA_readInterfThreshReg(HWA_Handle handle, uint32_t *pbuf, uint8_t startIdx, uint8_t size, uint8_t type)
Function to read the interference statistics INTF_LOC_THRESH_MAG_VAL or INTF_LOC_THRESH_MAG_VAL regis...
int32_t HWA_enable(HWA_Handle handle, uint8_t flagEnDis)
Function to enable the state machine of the HWA. This should be called after paramset and RAM have be...
int32_t HWA_disableDoneInterrupt(HWA_Handle handle, uint8_t threadIdx)
Function to disable the CPU interrupt after all programmed paramSets have been completed.
int32_t HWA_reset(HWA_Handle handle)
Function to reset the internal state machine of the HWA.
int32_t HWA_clearHistogramRAM(HWA_Handle handle)
Function to clear the Histogram RAM in HWA.
HWA Paramset Config for FFT block.
Definition: hwa/v0/hwa.h:1477
int32_t HWA_setDMA2ACCManualTrig(HWA_Handle handle, uint8_t idx)
Function to manually trigger the execution of the state machine waiting on DMA via software.
int32_t HWA_clearDebugReg(HWA_Handle handle)
Function to clear the debug registers (acc_trig_in_clr)
HWA Local memory Information.
Definition: hwa/v0/hwa.h:1773
uint32_t gHwaConfigNum
Externally defined driver configuration array size.
int32_t HWA_paramSetDonePolling(HWA_Handle handle, uint8_t numParamSets, uint8_t *paramsetsArray)
Function to poll the PARAM_DONE_SET_STATUS_0 and PARAM_DONE_SET_STATUS_1 registers to check if the sp...
HWA_Handle HWA_open(uint32_t index, HWA_OpenConfig *hwaCfg, int32_t *errCode)
Function to initialize HWA specified by the particular index value.
int32_t HWA_getDMAChanIndex(HWA_Handle handle, uint8_t edmaChanId, uint8_t *hwaDestChan)
Function to get the dma destination index with a given EDMA channel number This function assumes the ...
int32_t HWA_enableParamSetInterrupt(HWA_Handle handle, uint8_t paramsetIdx, HWA_InterruptConfig *intrConfig)
Function to enable the CPU and/or DMA interrupt after a paramSet completion. The CPU interrupt for ev...
HWA Paramset Config for ComplexMultiply block.
Definition: hwa/v0/hwa.h:1289
void(* HWA_ParamDone_IntHandlerFuncPTR)(uint32_t intrIdx, uint32_t paramSet, void *arg)
HWA Interrupt callback function after every paramset completion.
Definition: hwa/v0/hwa.h:740
HWA Paramset Config for CFAR block.
Definition: hwa/v0/hwa.h:1549
void HWA_init(void)
Function to initialize the HWA module.
HWA_Attrs gHwaAttrs[]
Externally defined driver configuration array.
#define HWA_CMP_K_ARR_LEN
The length of EGE compression/decompression K-paramseters array.
Definition: hwa/v0/hwa.h:187
HWA configuration structure, which describes the configuration information, needed for hwa handle ope...
Definition: hwa/v0/hwa.h:1811
int32_t HWA_softwareResetTwidIncrDeltaFrac(HWA_Handle handle)
Function resets the execution counter if complex multiply is configured as frequency shifter mode wit...
int32_t HWA_setContextswitchDMAManualTrigger(HWA_Handle handle, uint8_t idx)
Function to manually trigger the execution of the state machine via DMA trigger in context switch.
#define HWA_ZEROINSERT_LENGTH_INWORDS
The length of zero insert mask in words.
Definition: hwa/v0/hwa.h:181
int32_t HWA_getDMAconfig(HWA_Handle handle, uint8_t dmaTriggerSrc, HWA_SrcDMAConfig *dmaConfig)
Function to get the config to program the DMA for a given DMA Trigger channel. Application should use...
HWA Debug statistics.
Definition: hwa/v0/hwa.h:1753
int32_t HWA_readInterfFrameCountReg(HWA_Handle handle, uint32_t *numInterfSamplesFrame)
Function to read the number of samples that exceeded the threshold in a frame.
int32_t HWA_close(HWA_Handle handle)
Function to close a HWA peripheral specified by the HWA handle.
int32_t HWA_readHistThresholdRam(HWA_Handle handle, HWA_CdfThreshold *cdfThresholdResult, uint8_t numSampleIndices, uint8_t startSampleIdx)
Function to read the HWA HWA_RAM_TYPE_HIST_THRESH_RAM RAM.
int32_t HWA_enableContextSwitch(HWA_Handle handle, uint8_t flagEnDis)
Function to enable or disable the context switching in hwa.
int32_t HWA_readCFARPeakCountReg(HWA_Handle handle, uint8_t *pbuf, uint8_t size)
Function to read the PEAKCNT register.
DSSHWACCPARAMRegs * HWA_getParamSetAddr(HWA_Handle handle, uint8_t paramsetIdx)
Function to returns the HWA paramSet base address.
int32_t HWA_readDCAccReg(HWA_Handle handle, cmplx64ImRe_t *accbuf, uint8_t startIdx, uint8_t size)
Function to read the DC estimation accumulator register,.
#define HWA_BPMPATTERN_LENGTH_INWORDS
The length of BPM Pattern sequence in words.
Definition: hwa/v0/hwa.h:177
int32_t HWA_getEDMAChanId(HWA_Handle handle, uint8_t hwaDMAdestChan)
Function to get the edma EDMA channel number from a given HWA paramset destination channel....
int32_t HWA_enableDoneInterrupt(HWA_Handle handle, uint8_t threadIdx, HWA_Done_IntHandlerFuncPTR callbackFn, void *callbackArg)
Function to enable the CPU interrupt after all programmed paramSets have been completed in the backgr...
int32_t HWA_setContextswitchSoftwareTrigger(HWA_Handle handle)
Function to manually trigger the execution of the state machine via software in context switch,...
DSSHWACCRegs * HWA_getCommonCtrlAddr(HWA_Handle handle)
Function to returns the HWA common control base address.
HWA_RAMAttrs gHwaRamCfg[HWA_NUM_RAMS]
Externally defined driver RAM configuration array.
void(* HWA_Done_IntHandlerFuncPTR)(uint32_t threadIdx, void *arg)
HWA Interrupt callback function after all paramsets completion.
Definition: hwa/v0/hwa.h:748
HWA Paramset Config for pre-processing block.
Definition: hwa/v0/hwa.h:1394
uint32_t HWA_getRamAddress(uint8_t ramType)
Function to get the RAM starting address for one specified RAM type.
int32_t HWA_configCommon(HWA_Handle handle, HWA_CommonConfig *commonConfig)
Function to set the common HWA configuration parameters needed for the next operations/iterations/par...
#define HWA_NUM_RXCHANNELS
Number of RX channels in pre-processing block.
Definition: hwa/v0/hwa.h:173
int32_t HWA_getHWAMemInfo(HWA_Handle handle, HWA_MemInfo *memInfo)
Function to get HWA processing Memory information including address, size and number of banks.
HWA_Object gHwaObject[]
Externally defined driver object.
int32_t HWA_configRam(HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx)
Function to set the HWA RAM : HWA_RAM_TYPE_WINDOW_RAM, HWA_RAM_TYPE_VECTORMULTIPLY_RAM,...
HWA Paramset Config for Local maxima block.
Definition: hwa/v0/hwa.h:1614
HWA interrupt priority for HWA background thread done, ALT thread done, paramset done interrupt 1 and...
Definition: hwa/v0/hwa.h:1798
int32_t HWA_readClipStatus(HWA_Handle handle, uint16_t *clipStatusResult, uint8_t type)
Function to read the Clip Status registers.
int32_t HWA_configParamSet(HWA_Handle handle, uint8_t paramsetIdx, HWA_ParamConfig *paramConfig, HWA_SrcDMAConfig *dmaConfig)
Function to set the HWA configuration parameters for a given paramSet.
HWA Interrupt Config.
Definition: hwa/v0/hwa.h:1706
Source trigger DMA parameters.
Definition: hwa/v0/hwa.h:797
HWA Interrupt context structure for done interrupt.
Definition: hwa/v0/hwa.h:1855
HWA Common Config.
Definition: hwa/v0/hwa.h:811
int32_t HWA_disableParamSetInterrupt(HWA_Handle handle, uint8_t paramsetIdx, uint8_t interruptTypeFlag)
Function to disable the CPU and/or DMA interrupt after a paramSet completion.
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:91
HWA Paramset Config.
Definition: hwa/v0/hwa.h:1672
int32_t HWA_readDCEstimateReg(HWA_Handle handle, cmplx32ImRe_t *pbuf, uint8_t startIdx, uint8_t size)
Function to read the DC_EST_I/Q register.
HWA Paramset Config for compression and decompression.
Definition: hwa/v0/hwa.h:1639
int32_t HWA_singleParamSetDonePolling(HWA_Handle handle, uint8_t paramsetIndex)
Function to poll the PARAM_DONE_SET_STATUS_0 or PARAM_DONE_SET_STATUS_1 registers to check if one sin...
#define HWA_NUM_RAMS
The number of RAM types in HWA.
Definition: hwa/v0/hwa.h:183
HWA Histogram Threshold RAM data structure.
Definition: hwa/v0/hwa.h:1785
int32_t HWA_softwareResetRecursiveWinKvalue(HWA_Handle handle)
Function resets the paramset counter used in recurise windowing mode with REC_WIN_MODE_SEL is set to ...
#define HWA_NUM_INTERFMITG_WINARRAY
Number of programmable array of window parameters in interference mitigation block.
Definition: hwa/v0/hwa.h:175
HWA Interrupt context structure for paramset done interrupt.
Definition: hwa/v0/hwa.h:1842
int32_t HWA_clearClipStatus(HWA_Handle handle, uint8_t type)
Function to clear the Clip Status registers.
int32_t HWA_setSoftwareTrigger(HWA_Handle handle)
Function to manually trigger the execution of the state machine via software, the software trigger th...
HWA RAM Parameters.
Definition: hwa/v0/hwa.h:781
int32_t HWA_readDebugReg(HWA_Handle handle, HWA_DebugStats *pStats)
Function to read the debug registers (paramcurr, loopcou, acc_trig_in_stat)
HWA Paramset Config for post-processing and the statistics control registers.
Definition: hwa/v0/hwa.h:1248
HWA Paramset Config for Output Formatter/Destination block.
Definition: hwa/v0/hwa.h:1184
int32_t HWA_readRam(HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx)
Function to read the HWA 2D statistics output RAM, including HWA_RAM_TYPE_2DSTAT_ITER_VAL,...
int32_t HWA_controlPeripheralSuspendMode(HWA_Handle handle, uint8_t flagEnDis)
Function to control the suspend mode of the peripheral when the controlling processor (where this dri...
int32_t HWA_readInterfChirpCountReg(HWA_Handle handle, uint16_t *numInterfSamplesChirp)
Function to read the number of samples that exceeded the threshold in a chirp.
void * HWA_Handle
A handle that is returned from a HWA_open() call.
Definition: hwa/v0/hwa.h:732
HWA Statistics from the STATISTICS block.
Definition: hwa/v0/hwa.h:1729
int32_t HWA_setSourceAddress(HWA_Handle handle, uint16_t paramIdx, uint32_t sourceAddress)
Function to set the source address for one paramset.
void HWA_deinit(void)
Function to deinitialize the HWA module.
int32_t HWA_readStatsReg(HWA_Handle handle, HWA_Stats *pStats, uint8_t numIter)
Function to read the 4 sets of 'MAX' statistics register.
HWA driver internal Config.
Definition: hwa/v0/hwa.h:1864
HWA H/W Parameters.
Definition: hwa/v0/hwa.h:756
int32_t HWA_readIntfAccReg(HWA_Handle handle, uint64_t *accBuf, uint8_t type, uint8_t startIdx, uint8_t size)
Function to read the interference threshold MAG or MAGDIFF Accumulator register.
HWA_Object * gHwaObjectPtr[]
Externally defined driver object pointer.
int32_t HWA_softwareResetAccumulators(HWA_Handle handle, uint8_t accumulatortype)
Function for sofware to reset the DC accumulators or interference statistics accumulators.