Macros that define values for the various source select of threshold in pre-processing block.
◆ HWA_INTERFMITIGATION_PATH_ZEROOUT
#define HWA_INTERFMITIGATION_PATH_ZEROOUT ((uint8_t)0U) /** select the zero-out path in the interference mitigation module */ |
◆ HWA_INTERFMITIGATION_PATH_WINDOWZEROOUT
#define HWA_INTERFMITIGATION_PATH_WINDOWZEROOUT ((uint8_t)1U) /** select the windowed zero-out path in the interference mitigation module */ |
◆ HWA_INTERFMITIGATION_PATH_LINEARINTERPOLATION
#define HWA_INTERFMITIGATION_PATH_LINEARINTERPOLATION ((uint8_t)2U) /** select the linear interpolation path path in the interference mitigation module */ |
◆ HWA_INTERFMITIGATION_PATH_UNUSED
#define HWA_INTERFMITIGATION_PATH_UNUSED ((uint8_t)3U) /** un-used mode in the interference mitigation module */ |