Macros that define values for interpolation property of the FFT window to achieve larger FFT size using stitching.
Macros | |
#define | HWA_FFT_WINDOW_INTERPOLATE_MODE_NONE ((uint8_t)0U) |
#define | HWA_FFT_WINDOW_INTERPOLATE_MODE_4K ((uint8_t)2U) |
#define | HWA_FFT_WINDOW_INTERPOLATE_MODE_8K ((uint8_t)1U) |
#define HWA_FFT_WINDOW_INTERPOLATE_MODE_NONE ((uint8_t)0U) |
no window interpolation is enabled
#define HWA_FFT_WINDOW_INTERPOLATE_MODE_4K ((uint8_t)2U) |
window interpolation to achieve 4K FFT
#define HWA_FFT_WINDOW_INTERPOLATE_MODE_8K ((uint8_t)1U) |
window interpolation to achieve 8K FFT