AM273x MCU+ SDK  08.02.00

Introduction

Macros that define values for the various source select of threshold in pre-processing block.

Macros

#define HWA_INTERFTHRESH_SELECT_SW
 
#define HWA_INTERFTHRESH_SELECT_EST_AVERAGE
 
#define HWA_INTERFTHRESH_SELECT_EST_INDIVIDUAL
 

Macro Definition Documentation

◆ HWA_INTERFTHRESH_SELECT_SW

#define HWA_INTERFTHRESH_SELECT_SW
Value:
((uint8_t)0U)

◆ HWA_INTERFTHRESH_SELECT_EST_AVERAGE

#define HWA_INTERFTHRESH_SELECT_EST_AVERAGE
Value:
((uint8_t)1U)

◆ HWA_INTERFTHRESH_SELECT_EST_INDIVIDUAL

#define HWA_INTERFTHRESH_SELECT_EST_INDIVIDUAL
Value:
((uint8_t)2U)