Macros that define values for different type of accumulator registers of HWA_readAccumulatorReg() function.
Macros | |
#define | HWA_INTERFERENCE_THRESHOLD_TYPE_MAG ((uint8_t)0U) |
#define | HWA_INTERFERENCE_THRESHOLD_TYPE_MAGDIFF ((uint8_t)1U) |
#define HWA_INTERFERENCE_THRESHOLD_TYPE_MAG ((uint8_t)0U) |
interference mag threshold register
#define HWA_INTERFERENCE_THRESHOLD_TYPE_MAGDIFF ((uint8_t)1U) |
interference magdiff threshold register