Secure Debug User Guide

Note

This document is only applicable to High Security (HS) devices.

Introduction

On K3 High Security - Security Enforced (HS-SE) devices, the JTAG port is closed by default. The below table shows the default state of the JTAG on various device types.

Table 4 JTAG Default state on various device types
Device Type Variant M3 JTAG State Other cores JTAG State
General Purpose (GP) NA Open Open
High Security (HS) Field Securable (FS) Closed Open
High Security (HS) Security Enforced (SE) Closed Closed

The JTAG port for M3 core running System Firmware always remains closed on HS-FS or HS-SE devices. Software cannot open the JTAG port for the M3 core. If required, the user can open the JTAG port and debug the remaining cores on the device. Opening the JTAG port when System Firmware is running requires

  1. A signed X509 certificate authorizing the debug. - This is a distinct certificate from the X509 certificates used for secure boot.
  2. Sending the debug certificate to System Firmware to process and open the debug ports.

This document describes both these steps. It also describes how the debug can be controlled via board configuration.

Note

Please note that all steps in this document require JTAG connectivity to be enabled in efuses. Otherwise the steps in this document do not have any effect.

Creating a debug certificate

X509 Configuration Template

[ req ]
distinguished_name = req_distinguished_name
x509_extensions = v3_ca
prompt = no

dirstring_type = nobmp

# This information will be filled by the end user.
# The current data is only a place holder.
# System firmware does not make decisions based
# on the contents of this distinguished name block.
[ req_distinguished_name ]
C = oR
ST = rx
L = gQE843yQV0sag
O = dqhGYAQ2Y4gFfCq0t1yABCYxex9eAxt71f
OU = a87RB35W
CN = x0FSqGTPWbGpuiV
emailAddress = kFp5uGcgWXxcfxi@vsHs9C9qQWGrBs.com

[ v3_ca ]
basicConstraints = CA:true
1.3.6.1.4.1.294.1.3=ASN1:SEQUENCE:swrv
1.3.6.1.4.1.294.1.8=ASN1:SEQUENCE:debug

[ swrv ]
# Replace PUT-SWRV with actual SWREV SYSFW value
swrv = INTEGER:PUT-SWRV

[ debug ]
# Replace PUT-DEVICE-UID with actual device UID value
debugUID = FORMAT:HEX,OCT:PUT-DEVICE-UID
# Replace PUT-DBG-TYPE with actual debug type value
debugType = INTEGER:PUT-DBG-TYPE
# Replace PUT-NONSEC-DBG with actual non secure debug cores value
coreDbgEn = INTEGER:PUT-NONSEC-DBG
# Replace PUT-SEC-DBG with actual secure debug cores value
coreDbgSecEn = INTEGER:PUT-SEC-DBG

This X509 config can then be signed with SMPK (private) or BMPK (private) by using the command below:

$ openssl req -new -x509 -key custMpk.pem -nodes -outform der -out debug_unlock_cert.der -config signing_config.txt -sha512

Note

The data in the req_distinguished_name section is random to indicate the following:

  1. System Firmware does not process the information in the section.
  2. The data in this section needs to be updated by the user to reflect their company name, location, email address, etc.

Populating the fields in the certificate

The X509 certificate format is described in Introduction.

System Firmware expects two X509 extensions in the debug unlock certificate.

  1. System Firmware Debug Extension - Mandatory
  2. System Firmware Software Revision Extension - Mandatory

Below are the steps to populate the X509 extensions:

Debug Certificate Revision

If you have specified a non-zero debug certificate revision in the Secure Debug Unlock, you must populate the System Firmware Software Revision Extension in the certificate. Choose a version number equal to or higher than minimum specified version.

Debug Extension

  1. Populate the SoC UID in the extension. SoC UID can be obtained in multiple ways.

    If the board configuration allows a wild card jtag unlock i.e. skipping the SoC UID match, you can set the SoC UID to a 256 bit all zeros string. See example below.

    debugUID = FORMAT:HEX,OCT:0000000000000000000000000000000000000000000000000000000000000000
    
  2. The debugType field is a combination field. It contains both the level of debug to be allowed at SoC level and a reserved field. Both fields are 16 bits wide.

    • Select debug privilege level for the table Debug Levels. Encode this as a 16 bit integer.

    • Set the reserved field as zero. Encode also as a 16 bit integer.

      Combine both of them as follows.

      debugType = INTEGER:0xPPPPQQQQ
      

      where PPPP is the reserved field and QQQQ is the debug privilege level.

    As an example, enabling full debug i.e. DEBUG_FULL in Debug Levels

    debugType = INTEGER:0x00000004
    
  3. The coreDbgEn lists the IDs of processors for which non-secure debug is enabled. The processor IDs can be obtained from the SoC specific information in this documentation. Processor IDs are encoded as a string of hexadecimal values. Each processor ID takes a byte.

    E.g. For AM65x, the processor IDs are listed in AM65x Processor Descriptions. If non-secure debug needs to be enabled for the following four cores on AM65x,

    Processor ID Processor Name Location in SoC
    0x20 A53_CL0_C0 COMPUTE_CLUSTER_MSMC0: (Cluster 0 Processor 0)
    0x21 A53_CL0_C1 COMPUTE_CLUSTER_MSMC0: (Cluster 0 Processor 1)
    0x01 R5_CL0_C0 MCU_SEC_MMR0: (Cluster 0 Processor 0)
    0x02 R5_CL0_C1 MCU_SEC_MMR0: (Cluster 0 Processor 1)

    the coreDbgEn field is populated by concatenating the processor IDs.

    coreDbgEn = INTEGER:0x20210102
    

Note

The SoC reset enables both invasive and non-invasive debug for all non secure cores, so the non secure cores not listed in coreDbgEn also will be open for debug, in a case where debugType is set as one of DEBUG_PUBLIC, DEBUG_PUBLIC_USER, DEBUG_FULL, or DEBUG_SECURE_USER.

  1. The coreDbgSecEn lists the IDs of processors for which secure debug is enabled. The processor IDs can be obtained from the SoC specific information in this documentation. Processor IDs are encoded as a string of hexadecimal values. Each processor ID takes a byte.

    E.g. For AM65x, the processor IDs are listed in AM65x Processor Descriptions If secure debug needs to be enabled for the following two cores on AM65x,

    Processor ID Processor Name Location in SoC
    0x22 A53_CL1_C0 COMPUTE_CLUSTER_MSMC0: (Cluster 1 Processor 0)
    0x23 A53_CL1_C1 COMPUTE_CLUSTER_MSMC0: (Cluster 1 Processor 1)

    the coreSecDbgEn field is populated by concatenating the processor IDs.

    coreDbgSecEn = INTEGER:0x2223
    

Note

In case there is no debug unlock needed for any of the secure cores / non-secure cores, the core id in the corresponding debug extension should be set to (0xFF) to indicate invalid value.

E.g. To create a certificate to enable only non-secure debug for R5 cores, the debug cert extension for the list of secure and non-secure debug cores should be: .. code:

coreDbgEn = INTEGER:0x0102
coreDbgSecEn = INTEGER:0xFF

Certificate validation done by System Firmware

First, System Firmware expects a certificate signed with an active customer key to unlock the debug access to the non-M3 cores.

The active customer key is:

  1. SMPK if key revision is set to 1 in the efuses
  2. BMPK if key revision is set to 2 in the efuses

Then, the signature of the certificate is verified, and the hash of the public key in the certificate is compared against the hash of the public key in the efuses.

Note

System Firmware proceeds to the next steps only if the signature is verified and the public key hashes match.

Next, System Firmware looks for the System Firmware Debug Extension and System Firmware Software Revision Extension in the X509 certificate.

Warning

If any one of the two X509 extensions is not present, further processing does not happen.

Note

The remaining X509 extensions are ignored by System Firmware when processing the debug certificate.

Afterwards, System Firmware validates the information passed in the System Firmware Debug Extension and System Firmware Software Revision Extension by doing the following:

  1. The certificate revision of the debug certificate must be greater than or equal to the value specified by the min_cert_rev field in Secure Debug Unlock.
  2. The UID passed in the debug extension is checked against the SoC UID. The UIDs must match unless otherwise specified in the board configuration. See the field allow_wildcard_unlock in Secure Debug Unlock.
  3. System Firmware checks that the values specified for debug_priv_level are valid.
  4. System Firmware verifies that the processor IDs specified in the fields coreDbgEn and coreDbgSecEn are valid, and that the cores in coreDbgSecEn actually support secure debug.

Note

coreDbgSecEn lists which cores need to have secure level debug enabled. coreDbgEn lists which cores need to have non-secure level debug enabled.

Once these checks pass, System Firmware performs the actual debug unlock operation.

Sending debug certificate to System Firmware

Using TISCI API

The debug unlock certificate can be supplied to System Firmware via the TISCI_MSG_OPEN_DEBUG_FWLS - Open Debug Firewalls message. The debug unlock certificate must first be placed in memory. The physical address of the certificate is passed as a part of the TISCI message. System Firmware validates the certificate and its contents. If the checks pass, System Firmware performs debug unlock.

This procedure can be used when if JTAG debugger is unable to supply the unlock certificate over the JTAG interface.

Over the JTAG interface

The debug unlock certificate can be provided to System Firmware over the JTAG interface. Even though the JTAG access to the cores on the device is locked, the host PC can read and write to the Secure Access Point (Sec-AP) via the JTAG interface. The debug unlock certificate must be supplied to System Firmware via Sec-AP for processing. System Firmware processes the certificate, unlocks the JTAG and reports the JTAG unlock status. At this point, the host PC can debug the unlocked cores in the same manner as a GP device.

The protocol for communication via the Sec-AP is described in Secure AP Command Interface. This data transfer protocol is also supported in TI Code Composer Studio(CCS). We will describe how to use CCS to unlock the JTAG. The required CCS version is CCS 9.3 or later. Normally it would suffice to have a version of CCS that supports the device you are using.

  1. Create a target configuration file for the HS EVM in CCS and launch the target configuration file. This will create a file ccBoard0.dat which we will use in later steps. You will not be able to connect to any cores on the device in this step.

  2. The file ccBoard0.dat is typically found in the following directories.

    • on Linux, ~/.ti/<ccs_version>/0/0/BrdDat/ccBoard0.dat
    • on Windows, C:\Users\<user>\AppData\Local\Texas Instruments\CCS\<ccs_version>\0\0\BrdDat\ccBoard0.dat
  3. Find the “uscif” folder in CCS installation. This is typically in the following path <ccs install>/ccs/ccs_base/common/uscif. This folder will contain the dbgauth executable (dbgauth.exe on windows).

  4. Verify K3 support by running

    $ ./dbgauth --help
    ...
        --mode 3 = SUPPORTED TARGETS: All Keystone 3 devices
    ...
    

    The output must include the above description for “mode 3”. Older versions of EMUPACK included AM65x as the supported targets for mode 3.

Performing JTAG unlock

To unlock the JTAG, use the unlock command of dbgauth tool. We are assuming that ccs version is ccs1010.

$ cd /opt/ti/ccs1010/ccs/ccs_base/common/uscif || exit 1

$ ./dbgauth -c ~/.ti/ccs1010/0/0/BrdDat/ccBoard0.dat \
        -x xds110 \
        -s cs_dap_0 \
        -o unlock \
        -m 3 \
        -f ~/debug_unlock_cert.der
Using board config file:
/home/user/.ti/ccs1010/0/0/BrdDat/ccBoard0.dat
Successfully opened certificate file /home/user/debug_unlock_cert.der
Read 1509 bytes from certificate file /home/user/debug_unlock_cert.der
The target device is unlocked.

Please read the help of dbgauth for command line options.

  1. The argument to -x flag depends on the debugger used.

  2. The argument to -s flag depends on the board. This can be determined from the ccBoard0.dat file. Open ccBoard0.data with a text editor and look for similar line in the file. The identifier at the start of the line e.g. cs_dap_0 indicates the name to be used as argument.

    ...
    @ cs_dap_0 family=cs_dap irbits=4 drbits=1 subpaths=15 identify=0 revision=Power-AP systemresetwhileconnected=1
    ...
    

Retrieving SoC UID

Retrieving the SoC UID over JTAG

To retrieve the SoC UID, use the getuid command of dbgauth tool. We are assuming that ccs version is ccs1010.

Note

The commands below are shown for Linux. They need to be modified according to path name conventions of other operating systems.

$ cd /opt/ti/ccs1010/ccs/ccs_base/common/uscif || exit 1

$ ./dbgauth -c ~/.ti/ccs1010/0/0/BrdDat/ccBoard0.dat \
        -x xds110 \
        -s cs_dap_0 \
        -o getuid \
        -m 3
Using board config file:
/home/user/.ti/ccs1010/0/0/BrdDat/ccBoard0.dat

UID = c89491b8edad0fb3a5f201ec4caff17bcde0ed5ac845b17da14e0749da22d4cb

The retrieved UID can be populated into the debug certificate in the below manner.

debugUID = FORMAT:HEX,OCT:c89491b8edad0fb3a5f201ec4caff17bcde0ed5ac845b17da14e0749da22d4cb

Retrieving the SoC UID over UART

When the device is in UART boot mode, ROM prints the SoC information including the SoC ID on the boot UART. The last 32 bytes i.e. 64 characters before the start of the UART boot character ‘CC’ contain the SoC ID.

02000000011a00006a37657300000000
00000000485353450200010002000100
02a6000001000200cffc17b20bcbf96a
8c712e8d732b48c3e09ac6c0951013ce
a93e069d2ccdac95420cca9c5f637a80
0bb88ba99d3a8b1d92075c67bcc047d2
15de4a0d4ee20fd61f6002b07cd9b0b7
c47d9ca8d1aae57b8e8784a12f636b2b
760d7d98a18f189760dfd0f23e2b0cb1
0ec7edc7c6edac3d9bdfefe0eddc3fff
7fe9ad875195527dc89491b8edad0fb3
a5f201ec4caff17bcde0ed5ac845b17d
a14e0749da22d4cb
CCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCC

The above shows the UART output formatted to 32 characters per line. The characters corresponding to SoC data are

                c89491b8edad0fb3
a5f201ec4caff17bcde0ed5ac845b17d
a14e0749da22d4cb

Retrieving the SoC UID via TISCI

The TISCI_MSG_GET_SOC_UID API can be used to retrieve the SoC UID to print for reference:

SOC_UID[0] = 0xB89194C8
SOC_UID[1] = 0xB30FADED
SOC_UID[2] = 0xEC01F2A5
SOC_UID[3] = 0x7BF1AF4C
SOC_UID[4] = 0x5AEDE0CD
SOC_UID[5] = 0x7DB145C8
SOC_UID[6] = 0x49074EA1
SOC_UID[7] = 0xCBD422DA

Please note that the data is formatted in little endian fashion and bytes inside individual words need to be reordered before populating the debugUID field in the certificate. Alternative is to cast the response payload to a byte array before printing to view the values in byte order.

Controlling Debug via Board Configuration

Security board configuration allows the user to control the JTAG unlock process. See Secure Debug Unlock for the data structure definition.

  1. By setting allow_jtag_unlock to 0, runtime JTAG unlock through System Firmware can be prevented. The JTAG cannot be unlocked using the TISCI API or through the Sec-AP once System Firmware is running.

    Warning

    Please note that JTAG connection for R5 can still be unlocked by including the ROM debug X509 extension in the R5 boot loader X509 certificate.

    Note

    The rest of this section only applies in allow_jtag_unlock is set to 0x5A.

  2. Setting allow_wildcard_unlock skips matching the UID in the debug unlock certificate with the SoC UID. All the remaining checks should pass. This option allows using a single debug unlock certificate across multiple devices sharing the same root of trust keys (SMPK/BMPK).

    Warning

    While wildcard unlock is convenient during development, it must not be used during production. Please avoid creating a wildcard debug unlock certificate with production keys.

  3. Use min_cert_rev to prevent older debug unlock certificates from being used. Set this to 0 in development and increment it before production.

  4. While System Firmware allows debug unlock to be performed by one of the hosts on the device through a TISCI message, this path can be disabled as well. Set the jtag_unlock_hosts array to all zeroes to prevent jtag unlock using the TISCI message. Alternatively you can limit the hosts that can unlock debug to a specific hosts. Any host can be allowed to unlock the jtag port by using a special host id. Please refer to Secure Debug Unlock.

Note

JTAG unlock can be permanently disabled for all cores by blowing efuse. This can be achieved by calling TISCI_MSG_DISABLE_JTAG_UNLOCK API.