Cryptographic Services¶
Table of Contents
Introduction¶
The Cryptographic services allow tifs client to encrypt/decrypt data blobs using one of AES-ECB, AES-CBC or AES-GCM operations.
Functional Goals¶
Cryptographic Service System provides the following functionality:
- API to encrypt a data blob.
- API to decrypt a data blob.
Design¶
The to-be encrypted/decrypted blob must be preceded by a context. The blob starts immediately after the context blob ends. The context blob contains information like the algorithm to use, key, key size, iv, data length etc.
The response contains calculated tag when the mode is AES-GCM and operation type is ‘encryption’.
The user may use one of the keys in the imported symmetric keyring, that has appropriate rights set to be be used in the CSP API. In order to do so, the user must populate the key id in the context.
The context also contains a revision field that denotes the context version. The revision field has been added to support different variations of the service in the future. Currently, just one version is supported which is version 0.
The structure of the context v0 is given below.
Context Structure¶
struct csp_aes_ctx_v0 {
uint32_t revision;
uint8_t mode;
uint8_t key_size;
uint8_t ctr_width;
uint8_t key_id;
uint64_t data_len;
uint64_t dest_addr;
uint32_t key[8];
uint32_t iv[4];
uint32_t tag[4];
}
| revision | 32-bit magic word - set to 0x0AE50000 |
| mode | AES operation mode (ECB - 0, CBC - 1, GCM - 3) |
| key_size | AES key size (128 bits - 0, 256 bits - 2) |
| ctr_width | Reserved for future use |
| key_id | This should have the key id if a ‘symmetric keyring’ key is to be used for encryption/decryption, otherwise set to 0 |
| data_len | Length of data in bytes |
| dest_addr | 64-bits physical address where encrypted/decrypted blob has to be loaded |
| key | Encryption key if key_id is zero (‘key in the context’ mode), otherwise set to 0 |
| iv | Initialization vector for AES operation. Required for CBC and GCM modes. Not used for ECB mode. |
| tag | Authentication tag as an array of 4 words (16 bytes) for GCM mode encryption operations, set to 0 for non-GCM modes |