Key Writer (Lite)

This guide describes the procedure to be followed to populate customer keys in eFuses of the SoC.

Note

This document must be read alongside OTP Keywriter (Lite) TISCI Description

This service is available only on AM62Lx device.

High Security (HS) Device Sub-types

  1. HS-FS (High Security - Field Securable): Device type before customer keys are programmed (the state in which the device leaves TI factory). In this state, device protects the ROM code, TI keys and certain security peripherals. HS-FS devices do not enforce secure boot process.

    • M3/M4 JTAG port is closed, A53 JTAG port is open
    • DMSC/SMS/SMS-lite Firewalls are closed, SoC Firewalls are open
    • Board configuration need not be signed
    • ROM Boot expects a combined boot image that contains TI signed system-firmware binary. The outer certificate can be created using any private key.
    • System Firmware binary is encrypted by the TI Encryption key (TI MEK), and signed by the TI Private key (TI MPK).
  2. HS-SE (High Security – Security Enforced without customer encryption keys): Device type after only the customer public key hashes are programmed. HS-SE devices enforce secure boot (without encryption).

    • M3/M4, A53 JTAG ports are both closed
    • DMSC/SMS/SMS-lite, SoC Firewalls are both closed
    • Board configuration needs to be signed with active customer private key (SMPK/BMPK)
    • ROM Boot expects a combined boot image that contains TI signed system-firmware binary. The outer certificate must be created using the active customer private key (SMPK/BMPK). The boot image must not be encrypted because HS-SE (converted using keywriter lite) devices don’t have any stored customer encryption key.
    • System Firmware binary is encrypted by the TI Encryption key (TI MEK), and signed by the TI Private key (TI MPK).

HS-FS to HS-SE Conversion

In order to convert a HS-FS device to HS-SE device, one has to program the customer root key (optionally backup key) on the target device, using OTP Keywriter Lite.

Customer key information is put in a structured format to create a binary blob. A list of fields that OTP keywriter Lite supports, can be found here.

../_images/hsfs_to_hsselite_conversion.png

Certain efuse bits have been allocated to store the type of keywriter (either keywriter or keywriter lite) on devices.

When keywriter lite is utilized, it checks these bits to verify that they are either empty or contain the state corresponding to keywriter lite. If any other value is detected, keywriter lite becomes inoperable.

Upon the initial execution of keywriter lite on a device, the keywriter lite state is programmed into the efuse bits, effectively binding the device to the keywriter lite type. This ensures that the device is permanently associated with keywriter lite, preventing any other keywriter type from being used.

Introduction

The keywriter lite service is used for programming fields that serve different purposes. Following is a list of supported fields:

Table 6 Supported OTP fields
Field Description Notes
SMPKH Secondary Manufacturer Public Key Hash SMPK is 4096-bit customer RSA signing key
BMPKH Backup Manufacturer Public Key Hash BMPK is 4096-bit customer RSA signing key
MPK Options SMPK/BMPK options (Reserved for future use) 10 bit value (split into 2 parts)
KEYCNT Key count 2 if BMPK, SMPK are used, 1 if SMPK is used, 0 if none
KEYREV Key revision Can have a maximum value = key count
MSV Model specific value 20 bit value with 12 bit BCH code
SWREV-BOARDCONFIG Secure Board Configuration software revision 64 bit value
SWREV-SBL SBL software revision 48 bit value
SWREV-SYSFW Firmware software revision 48 bit value
JTAG DISABLE JTAG unlock disable 4 bit value
EFUSE BOOT MODE efuse boot modes 25 bit value
EXTENDED OTP Extended OTP array 1024 bit extended otp array

Programming Modes

The keywriter (lite) service functions in different programming modes each identified by a unique number known as the command id. Each mode is dedicated for programming a specific field or a set of fields. The programming modes offer the flexibility to selectively program just one field or a group of fields or all fields at once. The structure of binary data blob depends on the programming mode. The various programming modes supported by keywriter lite are listed below:

Table 7 Keywriter Lite Programming Modes
Programming Mode Command ID Purpose
Oneshot mode 0 Program all supported fields at once.
Multishot mode 1 Program a subset of supported fields at once.
SMPKH mode 2 Program just SMPKH.
BMPKH mode 3 Program just BMPKH.
Key count mode 4 Program just key count.
key revision mode 5 Program just key revision.
SBL SWREV mode 6 Program just SBL swrev.
SYSFW SWREV mode 7 Program just SYSFW swrev.
BRDCFG SWREV mode 8 Program just BRDCFG swrev.
MSV mode 9 Program just MSV.
JTAG mode 10 Program just JTAG unlock disable.
Boot mode mode 11 Program just efuse boot modes.
Extended OTP mode 12 Program just extended otp.

The programming mode must be selected based on the use case. For example, if someone wants to program just SMPKH, ‘SMPKH mode’ must be use; if someone wants to program SMPKH, key-count and key-revision at once (minimum programming needed for device conversion), ‘multi-shot mode’ must be used.

Keywriter Lite blob

Field data is provided to keywriter lite service through a structured binary blob. The structure of the blob depends on the selected programming mode. The general structure of the blob is shown below:

../_images/kwlite_blob_structure.png

Structure of header

The structure of header is given below:

struct keywriter_lite_header {
    uint16_t magic;
    uint16_t size;
    uint8_t abi_major;
    uint8_t abi_minor;
    uint16_t reserved0;
    uint32_t cmd_id;
    uint32_t reserved1[2];
} __attribute__((packed));
  1. magic: A magic number with value 0x9012U
  2. size: size of the payload section in bytes
  3. abi_major: abi major version number - 0x0
  4. abi_minor: abi minor version number - 0x1
  5. reserved0: reserved for future use, set to zero
  6. cmd_id: command id for the programming mode to be used
  7. reserved1: reserved for future use, set to zero

Payload substructures

The payload is made up of field specific substructures. For single-shot and multi-shot programming modes, the blob must have all the substructures packed in a specific order (more on this below.) For the remaining modes, the blob must have just the corresponding substructure.

MPK Options substructure:

struct mpk_opts {
    uint32_t field_header;
    uint32_t action_flags;
    uint16_t options;
    uint8_t resv_field[2];
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x4A7EU
  2. action_flags: Collection of flags to control the programming
  3. options: Reserved for future use, set to zero
  4. resv_field: Reserved for future use, set to zero
  5. reserved: Reserved for future use, set to zero

SMPKH/BMPKH substructure:

struct mpkh {
    uint32_t field_header;
    uint32_t action_flags;
    uint8_t mpkh[64];
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x1234U/0x9FFCU (SMPKH/BMPKH)
  2. action_flags: Collection of flags to control the programming, see faq section for more information
  3. mpkh: MPKH value
  4. reserved: Reserved for future use - set to zero.

Key Count substructure:

struct key_cnt {
    uint32_t field_header;
    uint32_t action_flags;
    uint32_t count;
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x5678U
  2. action_flags: Collection of flags to control the programming
  3. count: The key count value encoded in bit-position format.
  4. reserved: Reserved for future use - set to zero.

Key Revision substructure:

struct key_rev {
    uint32_t field_header;
    uint32_t action_flags;
    uint32_t revision;
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x62C8U
  2. action_flags: Collection of flags to control the programming
  3. revision: The key revision value encoded in bit-position format.
  4. reserved: Reserved for future use - set to zero.

SBL SWREV substructure:

struct sbl_revision {
    uint32_t field_header;
    uint32_t action_flags;
    uint64_t revision;
    uint32_t reserved[3];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x8BADU
  2. action_flags: Collection of flags to control the programming
  3. revision: The SBL software revision value encoded in bit-position format.
  4. reserved: Reserved for future use - set to zero.

SYSFW SWREV substructure:

struct sysfw_revision {
    uint32_t field_header;
    uint32_t action_flags;
    uint64_t revision;
    uint32_t reserved[3];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x45A9U
  2. action_flags: Collection of flags to control the programming
  3. revision: The SYSFW software revision value encoded in bit-position format.
  4. reserved: Reserved for future use - set to zero.

BRDCFG SWREV substructure:

struct brdcfg_revision {
    uint32_t field_header;
    uint32_t action_flags;
    uint64_t revision;
    uint32_t reserved[4];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x98DCU
  2. action_flags: Collection of flags to control the programming
  3. revision: The BRDCFG software revision value encoded in bit-position format.
  4. reserved: Reserved for future use - set to zero.

MSV substructure:

struct msv {
    uint32_t field_header;
    uint32_t action_flags;
    uint32_t msv;
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x1337U
  2. action_flags: Collection of flags to control the programming
  3. msv: The 20-bit MSV value.
  4. reserved: Reserved for future use - set to zero.

JTAG Disable substructure:

struct jtag_disable {
    uint32_t field_header;
    uint32_t action_flags;
    uint32_t jtag;
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0x7421U
  2. action_flags: Collection of flags to control the programming
  3. jtag: The 4-bit jtag unlock disable value.
  4. reserved: Reserved for future use - set to zero.

Boot Mode substructure:

struct boot_mode {
    uint32_t field_header;
    uint32_t action_flags;
    uint32_t fuse_id;
    uint32_t boot_mode;
    uint32_t reserved[2];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0xA1B2U
  2. action_flags: Collection of flags to control the programming
  3. fuse_id: The index of the fuse to program currently accepts only 1,2.
  4. boot_mode: The 25-bit boot mode value to program.
  5. reserved: Reserved for future use - set to zero.

Ext OTP substructure:

struct ext_otp {
    uint32_t field_header;
    uint32_t action_flags;
    uint16_t size;
    uint16_t index;
    uint8_t wprp[16];
    uint8_t otp[128];
    uint32_t reserved[4];
} __attribute__((packed));
  1. field_header: The lower 16-bits contain a magic number with value 0xD0E5U
  2. action_flags: Collection of flags to control the programming
  3. size: The number of bits to program.
  4. index: The index in the 1024-bits space to start programming from.
  5. wprp: Read protect/write protect array.
  6. otp: The 1024 bits extended otp data.
  7. reserved: Reserved for future use - set to zero.

Structure of payload

For single-shot or multi-shot programming mode the payload contains all the substructures. For other programming modes the payload contains just the corresponding substructure.

Payload structure for single-shot/multi-shot mode:

struct keywriter_lite_payload {
    struct mpk_opts mpkOptions;
    struct mpkh smpkh;
    struct mpkh bmpkh;
    struct key_cnt keyCount;
    struct key_rev keyRevision;
    struct sbl_revision sblRev;
    struct sysfw_revision sysfwRev;
    struct brdcfg_revision brdcfgRev;
    struct msv msvVal;
    struct jtag_disable jtagDisable;
    struct boot_mode bootMode;
    struct ext_otp extOtp;
} __attribute__((unused));

While using single-shot programming mode, all fields must be enabled. While using multi-shot programming mode, only the fields that need to be programmed must be enabled.

Payload structure for smpkh mode:

struct keywriter_lite_payload {
    struct mpk_opts mpkOptions;
    struct mpkh smpkh;
} __attribute__((unused));

Payload structure for bmpkh mode:

struct keywriter_lite_payload {
    struct mpk_opts mpkOptions;
    struct mpkh bmpkh;
} __attribute__((unused));

Payload structure for key count mode:

struct keywriter_lite_payload {
    struct key_cnt keyCount;
} __attribute__((unused));

Payload structure for key revision mode:

struct keywriter_lite_payload {
    struct key_rev keyRevision;
} __attribute__((unused));

Payload structure for sbl revision mode:

struct keywriter_lite_payload {
    struct sbl_revision sblRev;
} __attribute__((unused));

Payload structure for sysfw revision mode:

struct keywriter_lite_payload {
    struct sysfw_revision sysfwRev;
} __attribute__((unused));

Payload structure for boardcfg revision mode:

struct keywriter_lite_payload {
    struct brdcfg_revision brdcfgRev;
} __attribute__((unused));

Payload structure for msv mode:

struct keywriter_lite_payload {
    struct msv msvVal;
} __attribute__((unused));

Payload structure for jtag unlock disable mode:

struct keywriter_lite_payload {
    struct jtag_disable jtagDisable;
} __attribute__((unused));

Payload structure for ‘boot mode’ mode:

struct keywriter_lite_payload {
    struct boot_mode bootMode;
} __attribute__((unused));

Payload structure for extended otp mode:

struct keywriter_lite_payload {
    struct ext_otp extOtp;
} __attribute__((unused));

Structure of Checksum

struct checksum {
    uint8_t hash[64];
} __attribute__((packed));
  1. hash: SHA2-512 hash of the keywriter-lite header and keywriter-lite payload sections combined.

Procedure

The following figure illustrates the procedure to be followed to generate the binary blob for key writing.

../_images/kwlite_blob_creation_procedure.png

FAQs

  1. What happens when one or more unsupported fields are marked as enabled in a single-shot/multi-shot blob?

The unsupported fields are ignored by TIFS. In case of single-shot mode, if any of supported fields are disabled, the request would be NACKed. In case of multi-shot mode, if none of the supported fields are enabled, the request would be NACKed.

  1. What is the purpose of the action_flags field present in all substructures?

The action_flags field is a 32-bit value (8 hexadecimal digits) that controls how each field is programmed. It is divided into 4 bytes, each with a specific function:

action_flags (8 Hex) : <wp> <rp> <override> <active/inactive>

Each byte can be enabled by setting it to 0x5A and disabled by setting it to 0xA5. All other values are invalid. The functions of each byte are:

  • Write Protect (most significant byte):
    When enabled (0x5AA5A5A5U), prevents any future writes to this field.
  • Read Protect:
    When enabled (0xA55AA5A5U), prevents any future reads of this field. This provides security by making the field value unreadable after programming.
  • Override:
    When enabled (0xA5A55AA5U), allows programming fields by overriding their current value. For example, to change a revision value, override must be enabled. If the efuse rows corresponding to the key are not write protected, then enabling the override flag would attempt to program the efuse rows. Depending on the value, efuse programming may succeed or fail. For example, efuse row has data 0x11 (no write protect), and override is enabled. If the new value is 0x33, then it will be programmed. In case the new value is 0x22, it will fail since there would be an attempt to reset the bits at index 0 and 4.
  • Active/Inactive or Enable/Disable (least significant byte):
    When enabled (0xA5A5A55AU), indicates that this field should be programmed with the provided input value. This essentially controls whether the field is included in the current programming operation. Disabling this field would skip programming the field.

The usage of the active/inactive byte depends on the programming mode:

  • In single-shot mode, all fields must have the active byte enabled.
  • In multi-shot mode, only the fields you want to program should have the active byte enabled.
  • In specific field modes (like SMPKH mode, key count mode, etc.), the active byte must be enabled for the single field being programmed.

For example, to program a field with write protection enabled and make it active for programming, you would use: 0x5AA5A55AU.