HWA Paramset Config for pre-processing block.
HWA paramset config parameters for the preprocessing block inside HWA_ParamConfig which is used with the HWA_ConfigParamSet() call.
Data Fields | |
uint8_t | dcEstResetMode |
uint8_t | dcSubEnable |
uint8_t | dcSubSelect |
struct { | |
uint8_t thresholdEnable | |
uint8_t thresholdMode | |
uint8_t thresholdSelect | |
} | interfLocalize |
struct { | |
uint8_t resetMode | |
} | interfStat |
uint8_t HWA_PreProcessing::dcEstResetMode |
controls the reset behavior for all 12 accumulators, see HWA_DCEST_INTERFSUM_RESET_MODE macros for correct values. set into HWA_DCEST_INTERFSUM_RESET_MODE_NOUPDATE to bybass DC estimation. sets the bits DCEST_RESET_MODE in register PREPROC in paramset
uint8_t HWA_PreProcessing::dcSubEnable |
enable/bypass DC subtraction, see HWA_FEATURE_BIT macros for correct values. set into HWA_FEATURE_BIT_DISABLE to disable the DC subtraction. sets the bits DCSUB_EN of the register PREPROC in paramset
uint8_t HWA_PreProcessing::dcSubSelect |
see HWA_DCSUB_SELECT macros for the correct values sets bits DCSUB_SELECT of the register PREPROC in paramset
uint8_t HWA_PreProcessing::thresholdEnable |
enable/disable interference marking out, see HWA_FEATURE_BIT macros for correct values if set into HWA_FEATURE_BIT_DISABLE to disable the interference localization. sets the bits INTERFTHRESH_EN of the register PREPROC in paramset
uint8_t HWA_PreProcessing::thresholdMode |
specifies interference threshold mode, see HWA_INTERFERENCE_THRESH_MODE macros for the correct values sets the bits INTERFTHRESH_MODE of the register PREPROC in paramset
uint8_t HWA_PreProcessing::thresholdSelect |
select the source of the threshold, see HWA_INTERFERENCE_THRESH_SELECT macros for the correct values sets bits INTERFTHRESH_SELECT of the register PREPROC in paramset
struct { ... } HWA_PreProcessing::interfLocalize |
uint8_t HWA_PreProcessing::resetMode |
control reset behavior for all mag sum and magdiff sum accumulators, if it is set to HWA_DCEST_INTERFSUM_RESET_MODE_NOUPDATE, it is bypassed. see HWA_DCEST_INTERFSUM_RESET_MODE macros for the correct values sets the INTERFSUM_MAG_RESET bits of the register PREPROC in paramset
struct { ... } HWA_PreProcessing::interfStat |