Select the source of interference threshold 0 : User-defined threshold via INTERFTHRESH_MAG_SW and INTERFTHRESH_MAGDIFF_SW 1 : Single threshold based on built-in interference statistics outputs using sum value across collected interference statistics 2 : Threshold based on built-in interference statistics outputs, with each statistic being used for corresponding iteration (RX channel)
◆ HWA_INTERFERENCE_THRESH_SELECT_USER_DEFINED
#define HWA_INTERFERENCE_THRESH_SELECT_USER_DEFINED ((uint8_t)0U) |
◆ HWA_INTERFERENCE_THRESH_SELECT_BUILTIN_SUM_STATS
#define HWA_INTERFERENCE_THRESH_SELECT_BUILTIN_SUM_STATS ((uint8_t)1U) |
◆ HWA_INTERFERENCE_THRESH_SELECT_BUILTIN
#define HWA_INTERFERENCE_THRESH_SELECT_BUILTIN ((uint8_t)2U) |