HWA driver interface for HWA2.0.
Go to the source code of this file.
Data Structures | |
struct | HWA_Attrs |
HWA H/W Parameters. More... | |
struct | HWA_RAMAttrs |
HWA RAM Parameters. More... | |
struct | HWA_SrcDMAConfig |
Source trigger DMA parameters. More... | |
struct | HWA_CommonConfig |
HWA Common Config. More... | |
struct | HWA_SourceConfig |
HWA Paramset Config for Input Formatter/Source block. More... | |
struct | HWA_DestConfig |
HWA Paramset Config for Output Formatter/Destination block. More... | |
struct | HWA_AccelModeFFT |
HWA Paramset Config for FFT block. More... | |
struct | HWA_AccelModeCompress |
HWA Paramset Config for Compression/Decompression block. More... | |
struct | HWA_ComplexMultiply |
HWA Paramset Config for ComplexMultiply block. More... | |
struct | HWA_AccelModeCFAR |
HWA Paramset Config for CFAR block. More... | |
struct | HWA_ParamConfig |
HWA Paramset Config. More... | |
struct | HWA_InterruptConfig |
HWA Interrupt Config. More... | |
struct | HWA_Stats |
HWA Statistics from the STATISTICS block. More... | |
struct | HWA_DebugStats |
HWA Debug statistics. More... | |
struct | HWA_MemInfo |
HWA Local memory Information. More... | |
struct | HWA_InterruptPriority |
HWA interrupt priority for HWA background thread done, ALT thread done, paramset done interrupt 1 and paramset done 2 interrupt. More... | |
struct | HWA_OpenConfig |
HWA configuration structure, which describes the configuration information, needed for hwa handle open. More... | |
struct | HWA_InterruptCtx |
HWA Interrupt context structure for paramset done interrupt. More... | |
struct | HWA_DoneInterruptCtx |
HWA Interrupt context structure for done interrupt. More... | |
struct | HWA_Object |
HWA driver internal Config. More... | |
Macros | |
#define | HWA_RAM_WINDOW_SIZE_IN_BYTES 1024*4 |
#define | HWADRV_ADDR_TRANSLATE_CPU_TO_HWA(x) (uint32_t)((uint32_t)(x) & 0x000FFFFFU) |
transfer the CPU address to HWA address More... | |
#define | HWA_ERRNO_BASE (-2800) |
HWA driver error base. More... | |
#define | HWA_EINVAL (HWA_ERRNO_BASE-1) |
Error Code: Invalid argument. More... | |
#define | HWA_ENOINIT (HWA_ERRNO_BASE-2) |
Error Code: Operation cannot be done as HWA_init is not done. More... | |
#define | HWA_EOUTOFRANGE (HWA_ERRNO_BASE-3) |
Error Code: input argument out of range. More... | |
#define | HWA_EOUTOFMEM (HWA_ERRNO_BASE-4) |
Error Code: out of memory. More... | |
#define | HWA_ENOTSUPP (HWA_ERRNO_BASE-5) |
Error Code: feature not supported. More... | |
#define | HWA_EINUSE (HWA_ERRNO_BASE-6) |
Error Code: channel or resource in use. More... | |
#define | HWA_ENOTALIGNED (HWA_ERRNO_BASE-7) |
Error Code: address is not aligned to the expected boundary. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_PARAMSET (HWA_ERRNO_BASE-8) |
Error Code: Invalid argument: paramset Start/Stop Idx and numLoops in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_PARAMSET_ALT (HWA_ERRNO_BASE-9) |
Error Code: Invalid argument: paramset Start/Stop Idx and numLoops for context switching in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_FFTCONFIG (HWA_ERRNO_BASE-10) |
Error Code: Invalid argument: for FFT config in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_DCEST (HWA_ERRNO_BASE-11) |
Error Code: Invalid argument: for DC estimation in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_CFAR (HWA_ERRNO_BASE-12) |
Error Code: Invalid argument: for CFAR config in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_INTERFERENCE (HWA_ERRNO_BASE-13) |
Error Code: Invalid argument: for interference localization/mitigation in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_COMPLEXMULT (HWA_ERRNO_BASE-14) |
Error Code: Invalid argument: for complex multiply in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_CHANCOMB (HWA_ERRNO_BASE-15) |
Error Code: Invalid argument: for channel combine in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_ZEROINSERT (HWA_ERRNO_BASE-16) |
Error Code: Invalid argument: for zero insert in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_ADVSTAT (HWA_ERRNO_BASE-17) |
Error Code: Invalid argument: for advanced statistics in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_COMPRESS (HWA_ERRNO_BASE-18) |
Error Code: Invalid argument: for compress/decompression in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_LOCALMAXIMUM (HWA_ERRNO_BASE-19) |
Error Code: Invalid argument: for local maximum in common register. More... | |
#define | HWA_EINVAL_PARAMSET_GENERALCONFIG (HWA_ERRNO_BASE - 20) |
Error Code: Invalid argument: general config in paramset More... | |
#define | HWA_EINVAL_PARAMSET_SOURCE (HWA_ERRNO_BASE - 21) |
Error Code: Invalid argument: source(input formatter) in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_DEST (HWA_ERRNO_BASE - 22) |
Error Code: Invalid argument: destination(output formatter) in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_SRCDST_ADDRESS (HWA_ERRNO_BASE - 23) |
Error Code: Invalid argument: src and dst address in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_GENERALCONFIG (HWA_ERRNO_BASE - 24) |
Error Code: Invalid argument: FFT mode: general config in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_SIZE (HWA_ERRNO_BASE - 25) |
Error Code: Invalid argument: FFT mode: FFT size in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_POSTPROC (HWA_ERRNO_BASE - 26) |
Error Code: Invalid argument: FFT mode: post processing in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_PREPROC (HWA_ERRNO_BASE - 27) |
Error Code: Invalid argument: FFT mode: pre-processing in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_INTERF (HWA_ERRNO_BASE - 28) |
Error Code: Invalid argument: FFT mode: pre-processing interference localization/statistics/mitigation in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_COMPLEXMULT (HWA_ERRNO_BASE - 29) |
Error Code: Invalid argument: FFT mode: pre-processing complex multiply block in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_CFARMODE_GENERALCONFIG (HWA_ERRNO_BASE - 30) |
Error Code: Invalid argument: CFAR mode: general configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_CFARMODE_OSCONFIG (HWA_ERRNO_BASE - 31) |
Error Code: Invalid argument: CFAR mode: CFAR-OS configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_CFARMODE_CACONFIG (HWA_ERRNO_BASE - 32) |
Error Code: Invalid argument: CFAR mode: CFAR-CA configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_COMPRESSMODE (HWA_ERRNO_BASE - 33) |
Error Code: Invalid argument: compress/decompress mode: compress/decompress configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_LOCALMAXMODE (HWA_ERRNO_BASE - 34) |
Error Code: Invalid argument: local maxima mode: local maxima configuration in paramset. More... | |
#define | HWA_PARAMSET_POLLINGNOTALLOWED (HWA_ERRNO_BASE - 35) |
Error Code: if paramset interrupt is enabled, polling should be disabled. More... | |
#define | HWA_NUM_RXCHANNELS (12U) |
Number of RX channels in pre-processing block. More... | |
#define | HWA_NUM_INTERFMITG_WINARRAY (5U) |
Number of programmable array of window parameters in interference mitigation block. More... | |
#define | HWA_BPMPATTERN_LENGTH_INWORDS (8U) |
The length of BPM Pattern sequence in words. More... | |
#define | HWA_CHANCOMB_LENGTH_INWORDS (8U) |
The length of channel combining vector in words. More... | |
#define | HWA_ZEROINSERT_LENGTH_INWORDS (8U) |
The length of zero insert mask in words. More... | |
#define | HWA_NUM_RAMS (3U) |
The number of RAM types in HWA. More... | |
#define | HWA_MAXNUM_LOOPS (4095U) |
The maximum number of loops in HWA. More... | |
#define | HWA_CMP_K_ARR_LEN (8U) |
The length of EGE compression/decompression K-paramseters array. More... | |
#define | HWA_DONE_INTERRUPT_PRIORITY (1U) |
Default HWA background thread done interrupt priority. More... | |
#define | HWA_PARAMSETDONE_INTERRUPT1_PRIORITY (1U) |
Default HWA background thread done interrupt priority. More... | |
#define | HWA_PARAMSETDONE_INTERRUPT2_PRIORITY (1U) |
Default HWA paramset done interrupt 2 priority. More... | |
#define | HWA_FEATURE_BIT_ENABLE ((uint8_t)1U) |
#define | HWA_FEATURE_BIT_DISABLE ((uint8_t)0U) |
#define | HWA_SAMPLES_WIDTH_16BIT ((uint8_t)0U) |
#define | HWA_SAMPLES_WIDTH_32BIT ((uint8_t)1U) |
#define | HWA_SAMPLES_FORMAT_COMPLEX ((uint8_t)0U) |
#define | HWA_SAMPLES_FORMAT_REAL ((uint8_t)1U) |
#define | HWA_SAMPLES_UNSIGNED ((uint8_t)0U) |
#define | HWA_SAMPLES_SIGNED ((uint8_t)1U) |
#define | HWA_FFT_WINDOW_NONSYMMETRIC ((uint8_t)0U) |
#define | HWA_FFT_WINDOW_SYMMETRIC ((uint8_t)1U) |
#define | HWA_FFT_WINDOW_INTERPOLATE_MODE_NONE ((uint8_t)0U) |
#define | HWA_FFT_WINDOW_INTERPOLATE_MODE_4K ((uint8_t)1U) |
#define | HWA_FFT_WINDOW_INTERPOLATE_MODE_2K ((uint8_t)2U) |
#define | HWA_FFT_MODE_MAGNITUDE_LOG2_DISABLED ((uint8_t)0U) |
#define | HWA_FFT_MODE_MAGNITUDE_ONLY_ENABLED ((uint8_t)2U) |
#define | HWA_FFT_MODE_MAGNITUDE_LOG2_ENABLED ((uint8_t)3U) |
#define | HWA_FFT_MODE_OUTPUT_DEFAULT ((uint8_t)0U) |
#define | HWA_FFT_MODE_OUTPUT_MAX_STATS ((uint8_t)2U) |
#define | HWA_FFT_MODE_OUTPUT_SUM_STATS ((uint8_t)3U) |
#define | HWA_NOISE_AVG_MODE_CFAR_CA ((uint8_t)0U) |
#define | HWA_NOISE_AVG_MODE_CFAR_CAGO ((uint8_t)1U) |
#define | HWA_NOISE_AVG_MODE_CFAR_CASO ((uint8_t)2U) |
#define | HWA_NOISE_AVG_MODE_CFAR_OS ((uint8_t)3U) |
#define | HWA_TRIG_MODE_IMMEDIATE ((uint8_t)0U) |
#define | HWA_TRIG_MODE_SOFTWARE ((uint8_t)1U) |
#define | HWA_TRIG_MODE_RESERVED1 ((uint8_t)2U) |
#define | HWA_TRIG_MODE_DMA ((uint8_t)3U) |
#define | HWA_TRIG_MODE_HARDWARE ((uint8_t)4U) |
#define | HWA_TRIG_MODE_RESERVED2 ((uint8_t)5U) |
#define | HWA_TRIG_MODE_RESERVED3 ((uint8_t)6U) |
#define | HWA_TRIG_MODE_M4CONTROL ((uint8_t)7U) |
#define | HWA_ACCELMODE_FFT ((uint8_t)0U) |
#define | HWA_ACCELMODE_CFAR ((uint8_t)1U) |
#define | HWA_ACCELMODE_COMPRESS ((uint8_t)2U) |
#define | HWA_ACCELMODE_NONE ((uint8_t)7U) |
#define | HWA_CFAR_OPER_MODE_LOG_INPUT_REAL 0U |
#define | HWA_CFAR_OPER_MODE_LOG_INPUT_COMPLEX 1U |
#define | HWA_CFAR_OPER_MODE_MAG_INPUT_REAL 2U |
#define | HWA_CFAR_OPER_MODE_MAG_INPUT_COMPLEX 3U |
#define | HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_REAL 4U |
#define | HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_COMPLEX 5U |
#define | HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_CUT ((uint8_t)0U) |
#define | HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_DET_FLAG ((uint8_t)1U) |
#define | HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_NEIGHBOR_NOISE_VAL ((uint8_t)2U) |
#define | HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_CUT ((uint8_t)3U) |
#define | HWA_CMP_DCMP_COMPRESS ((uint8_t)0U) |
#define | HWA_CMP_DCMP_DECOMPRESS ((uint8_t)1U) |
#define | HWA_CMP_K_ARR_LEN (8U) |
The length of EGE compression/decompression K-paramseters array. More... | |
#define | HWA_COMPRESS_METHOD_EGE ((uint8_t)0U) |
#define | HWA_COMPRESS_PATHSELECT_BOTHPASSES ((uint8_t)3U) |
#define | HWA_RAM_TYPE_WINDOW_RAM ((uint8_t)0U) |
#define | HWA_RAM_TYPE_INTERNAL_RAM ((uint8_t)1U) |
#define | HWA_ACCUMULATORREG_TYPE_DC ((uint8_t)0U) |
#define | HWA_ACCUMULATORREG_TYPE_INTERF_MAG ((uint8_t)1U) |
#define | HWA_ACCUMULATORREG_TYPE_INTERF_MAGDIFF ((uint8_t)2U) |
#define | HWA_ACCUMULATORREG_TYPE_INTERF ((uint8_t)3U) |
#define | HWA_INTERFERENCE_THRESHOLD_TYPE_MAG ((uint8_t)0U) |
#define | HWA_INTERFERENCE_THRESHOLD_TYPE_MAGDIFF ((uint8_t)1U) |
#define | HWA_PARAMDONE_INTERRUPT_TYPE_CPU ((uint8_t)1U) |
#define | HWA_PARAMDONE_INTERRUPT_TYPE_DMA ((uint8_t)2U) |
#define | HWA_COMMONCONFIG_MASK_NUMLOOPS 0x00000001 |
#define | HWA_COMMONCONFIG_MASK_PARAMSTARTIDX 0x00000002 |
#define | HWA_COMMONCONFIG_MASK_PARAMSTOPIDX 0x00000004 |
#define | HWA_COMMONCONFIG_MASK_FFT1DENABLE 0x00000008 |
#define | HWA_COMMONCONFIG_MASK_BPMRATE 0x00000010 |
#define | HWA_COMMONCONFIG_MASK_BPMPATTERN 0x00000020 |
#define | HWA_COMMONCONFIG_MASK_INTERFERENCETHRESHOLD 0x00000040 |
#define | HWA_COMMONCONFIG_MASK_TWIDDITHERENABLE 0x00000080 |
#define | HWA_COMMONCONFIG_MASK_LFSRSEED 0x00000100 |
#define | HWA_COMMONCONFIG_MASK_FFTSUMDIV 0x00000200 |
#define | HWA_COMMONCONFIG_MASK_CFARTHRESHOLDSCALE 0x00000400 |
#define | HWA_COMMONCONFIG_MASK_I_CMULT_SCALE 0x00001000 |
#define | HWA_COMMONCONFIG_MASK_Q_CMULT_SCALE 0x00002000 |
#define | HWA_COMMONCONFIG_MASK_EGECOMRESS_KPARAM 0x00004000 |
#define | HWA_COMPLEX_MULTIPLY_MODE_DISABLE ((uint8_t)0U) /** 0-disable */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_FREQ_SHIFTER ((uint8_t)1U) /** 1-Freq Shifter mode, see \ref HWA_ComplexMultiply::freqShiftTwiddleIncr */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_SLOW_DFT ((uint8_t)2U) /** 2-slow DFT mode, see \ref HWA_CommonConfig::modeCfg::slowDFT::startFreq */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_FFT_STITCHING ((uint8_t)3U) /** 3-FFT stitching mode, see \ref HWA_CommonConfig::modeCfg::FFTstitching::twiddlePattern and HWA_CommonConfig::modeCfg::FFTstitching::winInterpolateMode */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_MAG_SQUARED ((uint8_t)4U) /** 4-Magnitude Squared mode */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_SCALAR_MULT ((uint8_t)5U) /** 5-Scalar Multiplication mode, see \ref HWA_CommonConfig::modeCfg::scalerMultiply::scaleCmultScaleEn */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT ((uint8_t)6U) /** 6-Vector Multiplication mode, see \ref HWA_CommonConfig::modeCfg::vectorMultiplyMode1::cmultScaleEn and HWA_CommonConfig::modeCfg::vectorMultiplyMode1::ramAddrOffset */ |
#define | HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT_2 ((uint8_t)7U) /** 7-Vector Multiplication mode 2, see \ref HWA_CommonConfig::modeCfg::vectorMultiplyMode2::ramAddrOffset */ |
#define | HWA_FFT_STITCHING_TWID_PATTERN_2K ((uint8_t)0U) /** 2K fft stitching twid factor pattern */ |
#define | HWA_FFT_STITCHING_TWID_PATTERN_4K ((uint8_t)1U) /** 4K fft stitching twid factor pattern */ |
Typedefs | |
typedef void * | HWA_Handle |
A handle that is returned from a HWA_open() call. More... | |
typedef void(* | HWA_ParamDone_IntHandlerFuncPTR) (uint32_t paramSet, void *arg) |
HWA Interrupt callback function after every paramset completion. More... | |
typedef void(* | HWA_Done_IntHandlerFuncPTR) (void *arg) |
HWA Interrupt callback function after all paramsets completion. More... | |
Functions | |
void | HWA_init (void) |
Function to initialize the HWA module. More... | |
void | HWA_deinit (void) |
Function to deinitialize the HWA module. More... | |
HWA_Handle | HWA_open (uint32_t index, HWA_OpenConfig *hwaCfg, int32_t *errCode) |
Function to initialize HWA specified by the particular index value. More... | |
int32_t | HWA_close (HWA_Handle handle) |
Function to close a HWA peripheral specified by the HWA handle. More... | |
int32_t | HWA_reset (HWA_Handle handle) |
Function to reset the internal state machine of the HWA. More... | |
DSSHWACCRegs * | HWA_getCommonCtrlAddr (HWA_Handle handle) |
Function to returns the HWA common control base address. More... | |
DSSHWACCPARAMRegs * | HWA_getParamSetAddr (HWA_Handle handle, uint8_t paramsetIdx) |
Function to returns the HWA paramSet base address. More... | |
int32_t | HWA_configCommon (HWA_Handle handle, HWA_CommonConfig *commonConfig) |
Function to set the common HWA configuration parameters needed for the next operations/iterations/paramsets of HWA. More... | |
int32_t | HWA_configParamSet (HWA_Handle handle, uint8_t paramsetIdx, HWA_ParamConfig *paramConfig, HWA_SrcDMAConfig *dmaConfig) |
Function to set the HWA configuration parameters for a given paramSet. More... | |
int32_t | HWA_getDMAconfig (HWA_Handle handle, uint8_t dmaTriggerSrc, HWA_SrcDMAConfig *dmaConfig) |
Function to get the config to program the DMA for a given DMA Trigger channel. Application should use the returned config to program the DMA so that it can then in turn trigger the paramset. Application should make sure that the channel provided here in dmaTriggerSrc should match the HWA_ParamConfig::dmaTriggerSrc passed to HWA_configParamSet() More... | |
int32_t | HWA_getCfarPeakCntRegAddress (HWA_Handle handle, uint32_t *peakCntAddr) |
Function to get the address of CFAR Peak Count register. More... | |
int32_t | HWA_configRam (HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx) |
Function to set the HWA RAM : HWA_RAM_TYPE_WINDOW_RAM, HWA_RAM_TYPE_VECTORMULTIPLY_RAM, HWA_RAM_TYPE_LUT_FREQ_DEROTATE_RAM or HWA_RAM_TYPE_SHUFFLE_RAM. More... | |
int32_t | HWA_enableParamSetInterrupt (HWA_Handle handle, uint8_t paramsetIdx, HWA_InterruptConfig *intrConfig) |
Function to enable the CPU and/or DMA interrupt after a paramSet completion. The CPU interrupt for every paramset completion may not be supported on all devices - see HWA_Attrs::isConcurrentAccessAllowed. More... | |
int32_t | HWA_enableDoneInterrupt (HWA_Handle handle, HWA_Done_IntHandlerFuncPTR callbackFn, void *callbackArg) |
Function to enable the CPU interrupt after all programmed paramSets have been completed in the background or ALT thread. More... | |
int32_t | HWA_disableParamSetInterrupt (HWA_Handle handle, uint8_t paramsetIdx, uint8_t interruptTypeFlag) |
Function to disable the CPU and/or DMA interrupt after a paramSet completion. More... | |
int32_t | HWA_disableDoneInterrupt (HWA_Handle handle) |
Function to disable the CPU interrupt after all programmed paramSets have been completed. More... | |
int32_t | HWA_enable (HWA_Handle handle, uint8_t flagEnDis) |
Function to enable the state machine of the HWA. This should be called after paramset and RAM have been programmed. More... | |
int32_t | HWA_setSoftwareTrigger (HWA_Handle handle) |
Function to manually trigger the execution of the state machine via software, the software trigger through either FW2HWA_TRIG_0 or FW2HWA_TRIG_1 register if the trigger is set to HWA_TRIG_MODE_SOFTWARE from DSP, trigger is done through FW2HWA_TRIG_0 if the trigger is set to HWA_TRIG_MODE_M4CONTROL from M4, trigger is done through FW2HWA_TRIG_1. More... | |
int32_t | HWA_setDMA2ACCManualTrig (HWA_Handle handle, uint8_t idx) |
Function to manually trigger the execution of the state machine waiting on DMA via software. More... | |
int32_t | HWA_setSourceAddress (HWA_Handle handle, uint16_t paramIdx, uint32_t sourceAddress) |
Function to set the source address for one paramset. More... | |
int32_t | HWA_readStatsReg (HWA_Handle handle, HWA_Stats *pStats, uint8_t numIter) |
Function to read the 4 sets of 'MAX' statistics register. More... | |
int32_t | HWA_readCFARPeakCountReg (HWA_Handle handle, uint8_t *pbuf, uint8_t size) |
Function to read the PEAKCNT register. More... | |
int32_t | HWA_readDebugReg (HWA_Handle handle, HWA_DebugStats *pStats) |
Function to read the debug registers (paramcurr, loopcou, acc_trig_in_stat) More... | |
int32_t | HWA_clearDebugReg (HWA_Handle handle) |
Function to clear the debug registers (acc_trig_in_clr) More... | |
int32_t | HWA_getHWAMemInfo (HWA_Handle handle, HWA_MemInfo *memInfo) |
Function to get HWA processing Memory information including address, size and number of banks. More... | |
int32_t | HWA_getDMAChanIndex (HWA_Handle handle, uint8_t edmaChanId, uint8_t *hwaDestChan) |
Function to get the dma destination index with a given EDMA channel number This function assumes the EDMA channel number is from the first EDMA instance. More... | |
int32_t | HWA_getEDMAChanId (HWA_Handle handle, uint8_t hwaDMAdestChan) |
Function to get the edma EDMA channel number from a given HWA paramset destination channel. This function assumes the EDMA channel number is from the first EDMA instance. More... | |
int32_t | HWA_readDCEstimateReg (HWA_Handle handle, cmplx32ImRe_t *pbuf, uint8_t startIdx, uint8_t size) |
Function to read the DC_EST_I/Q register. More... | |
int32_t | HWA_readIntfAccReg (HWA_Handle handle, uint64_t *accBuf, uint8_t type, uint8_t startIdx, uint8_t size) |
Function to read the interference threshold MAG or MAGDIFF Accumulator register. More... | |
int32_t | HWA_readDCAccReg (HWA_Handle handle, cmplx64ImRe_t *accbuf, uint8_t startIdx, uint8_t size) |
Function to read the DC estimation accumulator register,. More... | |
int32_t | HWA_readInterfChirpCountReg (HWA_Handle handle, uint16_t *numInterfSamplesChirp) |
Function to read the number of samples that exceeded the threshold in a chirp. More... | |
int32_t | HWA_readInterfFrameCountReg (HWA_Handle handle, uint32_t *numInterfSamplesFrame) |
Function to read the number of samples that exceeded the threshold in a frame. More... | |
int32_t | HWA_readInterfThreshReg (HWA_Handle handle, uint32_t *pbuf, uint8_t startIdx, uint8_t size, uint8_t type) |
Function to read the interference statistics INTF_LOC_THRESH_MAG_VAL or INTF_LOC_THRESH_MAG_VAL registers. More... | |
Variables | |
HWA_Attrs | gHwaAttrs [] |
Externally defined driver configuration array. More... | |
HWA_RAMAttrs | gHwaRamCfg [HWA_NUM_RAMS] |
Externally defined driver RAM configuration array. More... | |
HWA_Object | gHwaObject [] |
Externally defined driver object. More... | |
HWA_Object * | gHwaObjectPtr [] |
Externally defined driver object pointer. More... | |
uint32_t | gHwaConfigNum |
Externally defined driver configuration array size. More... | |
#define HWA_RAM_WINDOW_SIZE_IN_BYTES 1024*4 |
Internal or Window RAM size in bytes. See HWA_configRam
#define HWADRV_ADDR_TRANSLATE_CPU_TO_HWA | ( | x | ) | (uint32_t)((uint32_t)(x) & 0x000FFFFFU) |
transfer the CPU address to HWA address
#define HWA_NUM_RXCHANNELS (12U) |
Number of RX channels in pre-processing block.
#define HWA_NUM_INTERFMITG_WINARRAY (5U) |
Number of programmable array of window parameters in interference mitigation block.
#define HWA_BPMPATTERN_LENGTH_INWORDS (8U) |
The length of BPM Pattern sequence in words.
#define HWA_CHANCOMB_LENGTH_INWORDS (8U) |
The length of channel combining vector in words.
#define HWA_ZEROINSERT_LENGTH_INWORDS (8U) |
The length of zero insert mask in words.
#define HWA_NUM_RAMS (3U) |
The number of RAM types in HWA.
#define HWA_MAXNUM_LOOPS (4095U) |
The maximum number of loops in HWA.
|
extern |
Externally defined driver configuration array.
|
extern |
Externally defined driver RAM configuration array.
|
extern |
Externally defined driver object.
|
extern |
Externally defined driver object pointer.
|
extern |
Externally defined driver configuration array size.