xWRL6432 MMWAVE-L-SDK  05.01.00.04

Detailed Description

HWA Paramset Config for FFT block.

HWA paramset config parameters for the FFT block inside HWA_ParamConfig which is used with the HWA_ConfigParamSet() call.

Data Fields

uint8_t fftEn
 
uint8_t fftSize
 
uint16_t butterflyScaling
 
uint8_t interfZeroOutEn
 
uint8_t windowEn
 
uint16_t windowStart
 
uint8_t winSymm
 
uint8_t winInterpolateMode
 
uint8_t magLogEn
 
uint8_t fftOutMode
 

Field Documentation

◆ fftEn

uint8_t HWA_AccelModeFFT::fftEn

1 bit value: See HWA_FEATURE_BIT macros for correct values. Enable/Disable for FFT computation 0 - FFT disabled (Pipelined FFT sub-block bypassed) 1 - FFT enabled (Pipelined FFT sub-block enabled) Sets the FFT_EN bits of PARAM1_0

◆ fftSize

uint8_t HWA_AccelModeFFT::fftSize

4 bit value: Specifies FFT size. Actual FFT size is equal to 2^(fftSize) Supported values are [1..10], which correspond to FFT sizes [2..1024]. The actual FFT size should be equal to or larger than srcAcnt Sets the FFTSIZE bits of PARAM1_6

◆ butterflyScaling

uint16_t HWA_AccelModeFFT::butterflyScaling

10 bit value: 1 bit per butterfly stage. LSB is for last stage and MSB is for the first stage for each bit, 0 - MSB is saturated 1 - convergent rounded at LSB (divide by 2) Number of valid bits in this field depends on the fftSize. Sets the BFLY_SCALING bits of PARAM1_6

◆ interfZeroOutEn

uint8_t HWA_AccelModeFFT::interfZeroOutEn

1 bit value: See HWA_FEATURE_BIT macros for correct values. Enable/Disable for interference zeroing out HWA_COMMONCONFIG::interferenceThreshold field should be set to a valid value if this field is enabled. Sets the INTERF_THRESH_EN bits of PARAM1_6

◆ windowEn

uint8_t HWA_AccelModeFFT::windowEn

1 bit value: See HWA_FEATURE_BIT macros for correct values. Enable/Disable for Windowing operation Sets the WINDOW_EN bits of PARAM1_0

◆ windowStart

uint16_t HWA_AccelModeFFT::windowStart

10 bit value: (0-1023) Specifies the offset from the actual Window RAM base address and represents the starting address of the window function in the Window RAM. A value of 0x0 means the starting address is the first 32-bit word in the Window RAM, 0x1 is the second 32-bit word and so on. Sets the WINDOW_START bits of PARAM1_6

◆ winSymm

uint8_t HWA_AccelModeFFT::winSymm

1 bit value: See HWA_WINDOW_SYMM macros for correct values. Indicates whether the window function is symmetric or not Sets the WINSYMM bits of PARAM1_6

◆ winInterpolateMode

uint8_t HWA_AccelModeFFT::winInterpolateMode

2 bit value: See HWA_FFT_WINDOW_INTERPOLATE_MODE macros for correct values. Configures linear interpolation for the window coefficients, which is relevant for large-size FFT computation (i.e., FFT sizes of 2K, 4K) that is obtained via stitching multiple smaller-size FFTs. (Note: winSymm should be set to 0 when using 4K or 2K mode( Sets the WINDOW_INTERP_FRACTION bits of PARAM1_7

◆ magLogEn

uint8_t HWA_AccelModeFFT::magLogEn

2 bit value: See HWA_FFT_MODE_MAGNITUDE_LOG2 macros for correct values. Enable/Disable for Magnitude and Log2 computation Sets the ABS_EN, LOG2EN bits of PARAM1_0

◆ fftOutMode

uint8_t HWA_AccelModeFFT::fftOutMode

2 bit value: See HWA_FFT_MODE_OUTPUT macros for correct values. Configures the output mode of the FFT Engine path For stats mode, following parameters will be overriden in HWA_DestConfig of that paramset dstAcnt=4095, dstAIdx=dstBIdx=8, dstWidth=1, dstRealComplex=0. Sets the FFT_OUTPUT_MODE bits of PARAM1_0