3.3.4.12. GPIOΒΆ

GPIO Driver Overview

The GPIO Driver enables the GPIO controllers available on the device. The driver configures the GPIO hardware and interfaces and makes them available to the sysfs interface for user space interaction or other device drivers that need to access pins. For example, a MMC/SD driver may need to read a GPIO as in input to determine if a card is present. The H/W GPIO controllers available will vary by SoC and system configuration.

AM65 specifics

AM65 SoCs host DAVINCI GPIO IP.

Current software supports banked GPIO interrupt only. 16 GPIOs form a bank. Each bank can produce an interrupt; this is done to save the number of interrupt lines reaching the CPU. CONFIG_GPIO_DAVINCI=y should be part of the defconfig. Driver source code: drivers/gpio/gpio-davinci.c

Overview

The GPIO controllers allow interaction with GPIO pins for input/output and interrupt generation.

../../../../_images/GPIO_driver_diagram.png

User Layer

The GPIO driver can be used via the sysfs interface in user space or by other drivers that may need to access pins as either input/outputs or interrupts. More information about this driver and GPIO usage in Linux can be found in the kernel documentation:

  • GPIO Interface: Under Kernel directory Documentation/gpio/gpio.txt
  • GPIO Driver: Under Kernel directory Documentation/gpio/driver.txt

sysfs

The sysfs interface is for GPIO is located in the kernel at /sys/class/gpio. More information about this interface can also be found in the kernel sources:

  • GPIO sysfs: Under Kernel directory Documentation/gpio/sysfs.txt

For controlling LEDs and Buttons, the kernel has standard drivers, “leds-gpio” and “gpio_keys”, respectively, that should be used instead of GPIO directly.

Consuming Drivers

The GPIO Driver can also be easily leveraged by other drivers to “consume” a GPIO.

  • GPIO Consumer: Under Kernel directory Documentation/gpio/consumer.txt

For an example of a driver using a GPIO pin, examine this entry in a dts file for how the MMC/SD interface could use a GPIO as a card detect pin Under Kernel directory arch/arm/boot/dts/am335x-bone-common.dtsi line 401


Features

  • Access GPIO from user space as input or output
  • Leverage GPIO from another “consumer” driver

Power Management

GPIO pins to be used to wake the system from low-power sleep states must be configured as a wake source in the device tree. Verify low-power wake capability in the device Technical Reference Manual. Some devices map specific wake capabilities to each GPIO bank.
To configure a GPIO pin as a wake up source, setup a gpio-key instance in the device tree. This will associate a GPIO pin with wake up capability and an interrupt.
For example, look at the gpio_keys: volume_keys@0 node in the device tree LINUX/arch/arm/boot/dts/am335x-evm.dts as a reference. GPIO0_31 is configured as a wake source below:

`` @am33xx_pinmux { ``

pinctrl-names = "default";
pinctrl-0 = <&test_keys>;
...
test_keys: test_keys {
  0x74 (PIN_INPUT_PULLDOWN | MUX_MODE7);  /* gpmc_wpn.gpio0_31 */
};
...
keys: test_keys@0 {
  compatible = "gpio-keys";
  #address-cells = <1>;
  #size-cells = <0>;
  autorepeat;
  test@0 {
    label = "J4-pin21";
    linux,code = <155>;
    gpios = <&gpio0 31 GPIO_ACTIVE_LOW>;
    gpio-key,wakeup;
  };
 };
...

};