3.3.4.11. PWM

Introduction

Linux has support for Enhanced Pulse Width Modulator (ePWM) and Auxiliary Pulse Width Modulator (APWM) modules. APWM is Enhanced Capture (eCAP) module configured in PWM mode. These devices are part of The Pulse-Width Modulation Subsystem (PWMSS)

PWMSS software architecture

../../../../../_images/AM335X_PWM-SS_arch.JPG

Driver Configuration

Procedure to build eHRPWM driver

Device Drivers --->
        <*> Pulse Width Modulation(PWM) Support --->
           <*> eHRPWM PWM support

Procedure to build eCAP driver

Device Drivers --->
        <*> Pulse Width Modulation(PWM) Support --->
           <*> eCAP PWM support

Driver Usage

eCAP

The current release of the driver supports only PWM mode. eCAP can be controlled from the user space through SYSFS interface. SYSFS interface for eCAP is available at

target$ cat /sys/class/pwm/pwmchipN

Where,

‘N’ is the eCAP instance.
Various SYSFS Attributes
2 types of SYSFS attributes are available
  1. Request and Control attributes
  2. Configuration attributes

Note

  • Below examples uses eCAP instance 0 (i = 0).

Type 1 attributes

  • *export* Attribute.

Ask the kernel to export a PWM channel. Writing 0 to the export attribute Acquires the channel and writing 0 to the unexport attribute Frees/Releases the channel. Before performing any operations, device has to be requested first.


Example
  • Request the Device:
target$ echo 0 > /sys/class/pwm/pwmchip0/export
  • free the device:
target$ echo 0 > /sys/class/pwm/pwmchip0/unexport
  • *run* Attribute

Enable/disable the PWM channel

Example
  • Enable the PWM
target$ echo 1 > /sys/class/pwm/pwmchip0/pwm0/enable
  • Disable the PWM
target$ echo 0 > /sys/class/pwm/pwmchip0/pwm0/enable
CAUTION
Before enabling the module, the module needs to be configured using below configuration attributes. Else proper operation is not assured.

Type 2 attributes

i.Setting the Period
Following attributes set the period of the PWM waveform.
  • *period* Attribute

Enter the period in nano seconds value.

Example
if the period is 1 sec , enter
target$ echo 1000000000 > /sys /class/pwm/pwmchip0/pwm0/period
ii.Setting the Duty
Following attributes set the duty of the PWM waveform.
  • *duty_cycle* Attribute

Enter the Duty cycle value in nanoseconds.

target$ echo val > /sys/class/pwm/pwmchip0/pwm0/duty_cycle
iii.Setting the Polarity
  • *Polarity* Attribute.

Setup Signal Polarity

Example
To set the polarity to Active High, Enter
target$ echo 1 > /sys /class/pwm/pwmchip0/pwm0/polarity

Example
To set the polarity to Active Low, Enter
target$ echo 0 > /sys /class/pwm/pwmchip0/pwm0/polarity

Controlling backlight

Following are the 2 procedures to vary brightness of the LCD screen.
i. Setting duty percentage of pwm wave from eCAP sysfs files
target$ echo val > /sys/class/pwm/pwmchip0/pwm0/duty_cycle
‘val’ can range from 0 to 100.
ii. Setting brightness from backlight sysfs files
target$ echo val > /sys/class/backlight/backlight.8/brightness

‘val’ can range from 0 to 8.